English

100G CFP vs QSFP28: When to Use Each?

Updated on Mar 1, 2022 by
10.6k

100G Optical Transceiver

Nowadays, the development momentum of optical modules is unstoppable, among which the 100G optical modules take up most of the market share, such as 100G CFP and QSFP28. Then 100G CFP vs QSFP28, what are the differences and how to choose? This article will give a detailed introduction to CFP and QSFP28 with their specific applications involved.

 

100G CFP vs QSFP28: How to Choose?

For the differences between 100G CFP and 100G QSFP28, this article will have an introduction to them in these aspects definition, power consumption, port density, cost, and application.

CFP vs QSFP28 Round 1: Definition

CFP is a multi-source agreement (MSA) to define the form factor of the optical transceivers for high-speed digital signal transmission. The electrical connection of a CFP uses 10x 10 Gbit/s lanes in each direction (RX, TX). While, the optical connection can support both 10x 10 Gbit/s and 4x 25 Gbit/s variants of 100 Gbit/s. 100G CFP modules offer connectivity options for a wide range of service provider transport, data center networking, and enterprise core aggregation applications.

Figure 1: 100G CFP

QSFP28 transceiver module integrates 4 transmit and 4 receive channels. “28” means each lane carries up to 28G data rate. QSFP28 can do 4x 25G breakout connection, or 1x 100G connection depending on the transceiver used. For example, you can use 100G QSFP28 to 4 SFP28 DAC cables to realize 4x 25G breakout connection and LC-interface based QSFP28 with a single mode fiber (or MTP/MPO-interface based QSFP28 transceiver with a 12-fiber MTP/MPO patch cable) to get 1x 100G connection directly.

Figure 2: CFP vs QSFP28

CFP vs QSFP28 Round 2: Power Consumption

Considering the budget, network configuration, and overall bandwidth capabilities, power consumption plays an important role in transceiver hardware decisions. The power consumption of QSFP28 optical module is usually lower than 3.5W, while the power consumption of other 100G optical modules is 6W to 24W.

CFP vs QSFP28 Round 3: Port Density

The size of QSFP28 is the smallest 100G transceiver on the market. CFP4 is only a quarter of the width of the first generation of CFP. But it is still about 66% larger than QSFP28 in packaging form. This difference in size indicates that QSFP28 is much more efficient in port utilization than CFP.

CFP vs QSFP28 Round 4: Cost

Considering the power consumption and the port density, it will cost less to use QSFP28 in the system. Also, QSFP28 is less expensive than CFP.

CFP vs QSFP28 Round 5: Application

CFP, one of the recommended 100G optical modules, is mainly applied in metro networks and long-distance transmission (normally over 10km).

As shown in the following picture, to achieve high cabling density and long-distance transmission with CFP transceiver, the architecture mixed a 16-channel dual fiber DWDM Mux Demux by adding MTP harness cable and WDM SFP+ OEO converter to transfer the regular SR wavelength to DWDM wavelengths. Thus, a long-distance DWDM network with 100G CFP module is achieved.

Figure 3: 100G CFP Application

There are many QSFP28 products on the market, which are mainly divided into the following four applications according to the transmission distance:

  • Copper DAC Used Inside Racks Within 5m

QSFP28 DAC cables are ideal to use in short-range connections within 5m. They can offer a complete cable assembly in a cost-effective manner.

  • QSFP28 AOC/SR4 Transceiver for 5-100m

QSFP28 AOC is the best fit for 3-20m, and QSFP28 SR4 transceiver with 12-fiber MTP OM3/OM4 cable can support a transmission distance of up to 100m.

  • QSFP28 PSM4/CWDM4/CLR4 Transceiver for 100m-2km

For 100m to 2km, QSFP28 PSM4/CWDM4/CLR4 transceivers can offer cost-effective solutions. They can support up to 500m over 12-fiber MTP single mode fiber and 2km over duplex LC single mode fiber respectively.

  • QSFP28 LR4/ER4/ZR4 Transceiver for Long Span

For long-span 100GbE deployment, such as connectivity between two buildings (mostly up to 10km), QSFP28-100G-LR4 with duplex LC single mode fiber is the preferred option defined by IEEE. For longer distances (up to 40km and 80km), 100G QSFP28 ER4/ZR4 transceivers are better.

As for 100G CFP vs QSFP28, which to use for your network construction? Actually, it depends on two main aspects: the port type of your hardware device and application scenarios. CFP modules have a much larger size than QSFP28 modules. 100G QSFP28 appears to be mainstream and is mostly used in shorter distances (0-10km) between switches or sometimes in long distances (up to 40/80km) with QSFP28 ER4/ZR4. While 100G CFP can also be used for short distances, it is more commonly employed in metropolitan area networks (MANs) and long-haul WDM transmissions.

 

Related Information

A Comprehensive Understanding of CFP Transceiver Modules

100G QSFP28 Optical Transceiver Comparison

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.9k