English

10G Ethernet Cabling Solutions

Updated on Jan 11, 2022 by
4.6k

The dramatic growth in business data throughput has led to increased demand and use for high-performing interconnects, storage devices, and servers. The result is an increased expansion of higher-speed Ethernet solutions, specifically 10 Gigabit Ethernet. This article explains what 10G Ethernet is in detail and introduces 10GbE cabling solutions and several application cases for your reference.

10G cables

 

10G Ethernet Overview

10 Gigabit Ethernet (or 10GbE) is a telecommunication technology that offers data speeds up to 10 billion bits per second. It was first defined by the IEEE 802.3ae-2002 standard. 10GbE works only in full-duplex mode, which enables the transmission of data in both directions simultaneously on the same signal carrier.

10GbE technology is applicable to all kinds of network structures. It can reduce the complexity of the network, and also meet the needs of backbone network large-capacity transmission, solving the "bottleneck" problem of network transmission.

When talking about cabling solutions for 10GbE networks, two broad categories of copper and optical fiber will be considered as a result. The following content introduces the two major 10GbE cabling solutions and several application cases involving 10G switches and modules for your consideration.

 

10G Ethernet Cabling Solutions

Fiber Optic Cabling

Generally, fiber optic cables can be divided into single-mode fiber (SMF) and multi-mode fiber (MMF). Both SMF and MMF systems can be used with 10GbE. MMF cabling supports distances of up to 300m, depending on the transceivers used and transmission speed. Compared with MMF, SMF cabling features lower modal dispersion and supports distances of up to 40km depending on transceivers, transmission speed, and buffer credits for allocated switches.

Case 1: Connect two 10G SFP+ switches using fiber optic cable and two 10G SFP+ modules.

fiber optic cables

As an alternative, a 10G SFP+ AOC (Active Optical Cable) seems to be a more cost-effective choice. It is a fixed assembly that is purchased at a given length yet without sacrificing its transmission speed and distance. SFP+ AOC provides high performance in 10GbE network applications by using an enhanced SFP+ connector to send 10Gbps data through a pair of transmitters and receivers over a fiber optic cable.

Case 2: Connect two 10G SFP+ switches using 10G SFP+ AOC cable.

10G SFP+ AOC

Copper Cabling

Currently, 10GBASE-T is the common technology that enables 10GbE operations over twisted-pair copper cabling systems. Cables must be certified to at least 500MHz to ensure 10GBASE-T compliance. Cat6a cables can deliver 10G performance up to 500 MHz and at a distance of up to 100m, which offers relatively great flexibility in network design due to its 100-meter reach capability. Cat6 cables are able to work in 10GBASE-T deployments too, but with a distance limitation of up to 55m.

To build a 10G copper network, there are generally two cabling solutions: 10GBASE-T switch with Cat6/6a cable, or 10G SFP+ switch with 10GBASE-T SFP+ transceiver.

Case 3: Connect two 10GBASE-T switches using a Cat6 cable.

cat6 cable

Another option is to use a 10G SFP+ DAC (Direct Attach Cable). Same as the AOC cable, the connector fits into the same form factor connector and housing as fiber optic cables with SFP+ connectors. DAC cable is widely used in today’s 10GbE network interconnection. However, from a structured cabling viewpoint, it has a limited distance of up to 10m. It is a low-cost alternative to traditional twisted-pair copper cabling in data center deployments.

Case 4: Connect two 10G SFP+ switches using a 10G SFP+ DAC cable.

10G SFP+ DAC

 

Summary

Since 10 Gigabit Ethernet is only compatible with a specific type of 10g cables, it is important to choose fiber or copper cables accordingly. It has no doubt that your 10GbE cabling may require 10-gigabit transceivers, 10-gigabit switches, etc. And for all these devices you can look up on our website FS.com for more details. Hope the above introduction and application cases can be a good reference for your 10G Ethernet deployment.

Related Articles:

Structured Cabling: Backbone Cabling vs Horizontal Cabling

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k