English

25G/50G/100G Technology and Trend

Updated on Mar 10, 2020 by
8.8k

10G and 40G technologies have matured and occupied a large market during the past decade. In recent years, 25G/50G/100G technologies have gained attention and are becoming prominent in future network deployments. New Ethernet technologies are created to meet market demands and developments, not just for faster speeds. This post will introduce some key 25G/50G/100G technologies to learn the considerations behind.

 

25G Technology

Aimed at cloud data centers, 25G standard was officially approved in 2016, several years later than 10G, 40G, 100G standards. The biggest benefit of 25G is its SerDes technology, which converts serial data to parallel interfaces and vice versa. This reduces the need for many I/O pins and connections.

SerDes lanes.png

Figure 1: SerDes Lanes in Different Gigabit Ethernet

Most switches run SerDes with a clock rate of around 10Ghz, supporting a 10Gb transfer rate. In recent years, SerDes technology has advanced to 25GHz. This development results in the differences in efficiency and costs of 10G/40G and 25G deployment. Leveraging 25GHz SerDes lane, 25G supports a single lane at 25Gbps, which is 2.5 times the bandwidth performance of 10G using a 10GHz lane. When moving from 10G to 25G, rewiring is unnecessary as 25G switches can use the same LC fibers as 10G. Moreover, 25G is capable of providing 4 times the switch port density of 40G which requires 4 10GHz lanes. Thus the migration path 10G-40G-100G is inevitably cost-prohibitive while less scalable and efficient.

25 vs 40.pngFigure 2: 25G Technology vs 40G Technology

 

50G Technology

25G stimulates the anticipation of higher transmission rates in the industry, thus 50G standard was launched in 2018 with the same architecture as 400G/200G standard to serve as the next high-speed solution for connecting servers and data centers. 50G deployment can reuse the 25G devices in the existing 100G network so as to reduce the cost. For this reason, the cost of 50G can be half of 40G, but the performance may increase by 25%. While the most important technology for achieving the high performance of 50G is PAM4 (four-level pulse amplitude modulation).

100 switch to 50G server.png

Figure 3: 100G Switch to 50G Server Connection

50G reaches 53.125 Gbit/s after FEC encoding, which cannot be transmitted over an electrical interface while maintaining signal integrity, thus PAM4 is adopted to map pairs of bits into a single symbol, making an overall baud rate of 26.5625 Gbaud for 50 Gbit/s per lane. PAM4 is widely used in high-speed signal interconnection, offering higher transmission efficiency at a lower cost compared with earlier non-return-to-zero (NRZ). PAM4 at 50 Gbaud provides a path to 100G via a 1*2*50 Gbaud architecture that requires only one single laser but achieves a ten-fold increase in transmission rate from 10G to 100G.

50GBase-LR.png

Figure 4:  50GBASE-LR PMD Architecture Using PAM4

 

100G Technology

Catering to the demands of high-speed and long-reach transmission, the first 100G standard was approved in 2010 and tremendous changes were made in later years. 100G is replacing 40G in data centers because of improved standards, unified technical solutions, and the development of the industry. This is mainly due to the higher transmission rate and longer distance made possible by the use of DWDM technology.

 

Physical Medium Device (PMD) 40 Gige 100 Gige

Multimode optical fiber 

< 100 m with OM3 fiber

40GBase-SR4:

Ribbon fibers 

850 nm 

4 × 10 Gbps

100GBase-SR10 

Ribbon fibers 

850 nm 

10 × 10 Gbps

Single mode optical fiber 

> 10 km

40GBase-LR4:

CWDM 20nm (Channel spacing) 

1310 nm 

4 Wavelengths × 10 Gbps

100GBase-LR4: 

LAN-WDM 4.5 nm 

1310 nm 

4 Wavelengths × 25 Gbps

Single mode optical fiber 

> 40 km

 

100Gbase-ER4: 

LAN-WDM 4.5 nm 

1310 nm 

4 Wavelengths × 25 Gbps

Single mode optical fiber, 

not standardized

 

not standardized 

Channel spacing 8 nm 

1550 nm 

10 Wavelengths × 10 Gbps

Table 1: 100G vs 40G

 

100G DWDM technology enables high capacity transmission over a single wavelength across longer distances and it is especially used for high-speed optical communications. Coherent CFP/CFP2/CFP4 DWDM optical transceivers are for 100G MAN (Metropolitan Area Network) or DCI (Data Center Interconnection ) up to 80 km or a long-haul link more than 1000 km, transporting multiple 10G/40G/100G services to satisfy the increasing demand for high bandwidths. In addition, using 100G DWDM transponder/muxponder can avoid the redesign of network architecture while achieving transport capability and smooth transition among 10G, 40G, 100G, as it multiplexes multiprotocol and multi-rate services.

100G transmission.pngFigure 5: 100G Transmission with DWDM Transponder/Muxponder

 

Relation Among 25G/50G/100G

25G/50G/100G all have wide applications in cloud data centers now, and integrating them can achieve the 10G-25G-50G-100G network upgrade. While before the emergence of 25G and 50G, the traditional migration path is 10G-40G-100G, which is more costly but less efficient. By contrast, upgrading from 25G to 100G can be a more cost-effective solution. Based on 25G, this migration path can be achieved by 4x25G or 2x50G SerDes lanes leveraging new leaf and spine architectures. It improves efficiency and performance, saving money on both initial costs and ongoing expenses by using existing cables. On the whole, the 25G-50G-100G migration path is cheaper and makes full use of switch ports. It also prepares for future upgrades to 200G and 400G.

Read this article for more about the comparison of 10G-40G-100G and 10G-25G-100G migration paths: 10G-25G-100G Network Upgrade: An Inevitable Roadmap for Future Data Centers.

25G-100G leaf-spine.png

Figure 6: 25G-100G Leaf-Spine Architecture

 

Conclusion

These emerging 25G/50G/100G technologies have well adapted to the diverse needs of the market and led the trend of the industry in turn. It is well received that 25G/50G/100G each have their advantages in cost and performance for adopting more advanced technologies compared with 10G and 40G. While the demands never stop, thus the development of technologies will never stop moving forward either. Network managers are always looking for a balance between speed and reuse technology to find a cost-effective solution. Let’s wait and see what will happen in the future.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k