English

An Overview of Available PDU Types in the Market

Updated on May 20, 2020 by
5.9k

The PDUs (Power Distribution Units) with some basic functions were sufficient for most power distribution needs back when the data centers were called data rooms. Witnessing the constant update of power systems, many IT designers are seeking new PDU solutions with more functions that will meet the demands of modern data centers. A variety of PDUs in the market are available to satisfy various needs. This article will help you to classify the PDU types based on their functions, power phases, and installation methods.

According to Functions: Basic vs Intelligent PDU

Basic PDU

As a dependable, space-saving, user-friendly, and cost-effective solution, a basic PDU provides reliable unfiltered power distribution from a UPS (Uninterrupted Power Supply) system, generator, or utility source to multiple devices like equipment racks, wiring closets, server rooms, etc. Adopting basic PDUs will benefit the original UPS system with more outlets, which essentially converts a single high-amperage UPS outlet to multiple low-amperage PDU outlets. However, these basic PDUs are unable to surge suppression or line filtering that could interrupt the flow of power to connected equipment in order to ensure the availability of the power.

Intelligent PDU

Aside from the basic powering functionalities, an intelligent power distribution unit (iPDU) provides a variety of functions like real-time power monitoring, environmental monitoring, and data center infrastructure integration, etc., which help to increase the efficiencies of data centers. Adopting intelligent PDUs will enable the network architects to design smarter IT infrastructures. Here is the division of the intelligent PDUs covering the common types in the market.


  • Metered Power Distribution Unit is designed to provide network-grade power distribution with a digital LCD meter for real-time load monitoring. Metered PDU can locally monitor load level and avoid potential overloads with a built-in digital current meter while offering reliable power distribution from any protected UPS, generator or mains input power source.

  • Monitored Power Distribution Unit is similar to the metered PDU, which displays load levels in real-time, allowing additional equipment to be connected safely. Monitored PDU has the capabilities of remotely monitoring single-phase or three-phase voltage, frequency, and load levels in real-time via a built-in network connection.

  • Switched PDU possesses the same monitoring features with the previous types but further provides the control of powering on/off switches to specific outlets, which enables the users to control the individual outlets for the rebooting of locked equipment. The unused PDU outlets can be locked off electronically in order to prevent the connection of unauthorized hardware. Remote users can switch each of the PDU outlets on or off via SNMP, Web, or telnet.

  • Switched Metered-by-Outlet PDU combines all the capabilities of switched PDUs and metered outlet PDUs, will create power sequencing delays that minimize the risk of inrush currents, reduce the risk of unauthorized access to devices, and save the costs and environmental footprint by powering off devices that are not being used.

  • Automatic Transfer Switch (ATS) PDU is invented to help users provide redundant power to the IT equipment that is not designed with redundant power supplies. The working principle is: to eliminate equipment downtime by automatically switching to a secondary power source if the primary source fails or requires maintenance. The dual AC inputs can be connected to two utility sources, two generator sources, two UPS sources, or any combination. The primary input plugs into the primary UPS system, which must be an on-line UPS system while the secondary input plugs into the secondary UPS system. Power designs with ATS PDUs are normally applied in a wide variety of advanced and redundant-power networking applications in data centers.

  • Maintenance Bypass (MBP) PDU allows the seamless transfer of an electrical load from UPS power to utility power for uninterrupted operation of connected equipment when performing maintenance, replacing batteries, or installing a new UPS. The UPS draws input power from the MBP through a dedicated receptacle that is separate from the outlets for connected devices. When the switch on the front of the MBP is turned from Normal to Bypass, or from Bypass to Normal, the power supplied to connected devices will move from one input power source to another. Power designs with MBP PDUs are normally used in data centers or some other locations where uptime is or crucial.

Differences Between Basic and Intelligent PDUs

The most distinctive difference between basic and intelligent PDUs is their functions. Basic PDUs are reliable power distribution devices, like the larger version of power strips sharing some basic characteristics. Conversely, intelligent PDUs with various functions have performance advantages for connecting the real-time data for wiser decisions, maximizing the uptime for higher performance, reducing energy consumption and operation costs for better budget, and reducing carbon footprints by providing optimal control over AC, heat, and humidity for green data centers.

Due to the abovementioned function diversity, intelligent PDUs are significantly more expensive to purchase and implement than their basic counterparts. However, the operating costs may be saved on the condition that they are designed for smarter data center management.

Basic vs Intelligent

Furthermore, the differences in their functions will also affect the applications of these two categories of PDUs. For some small-scale and simple application scenarios, there is no need to be equipped with intelligent PDUs. Basic PDUs may offer a cost-effective solution to this target audience. If rigorous monitoring of the power is critical in most of the high-density cabling systems, picking intelligent PDUs will be optimal.

According to Power Phases: Single-phase vs Three-phase PDU

The differences between a single-phase PDU and a three-phase PDU are mainly in three factors—power, organization, and application.

Single-phase power systems distribute up to 120V of alternating current. It is calculated as volts multiple amps and is described as volt-amps or VA. A 120V, 20A circuit has an apparent power of 2400VA or 2.4kVA. A 208V, 20A circuit has an apparent power of 4160VA or 4.2kVA. Thus one 208V circuit provides almost twice as much power as one 120V circuit assuming the current (amperage) remains the same. With three 208V circuits, a substantial amount of power can then be deployed in one three-phase PDU.

Three-phase cable of PDUs is larger in size than the cable of single-phase PDUs. However, when required to provide the same amount of apparent power, adopting multiple single-phase PDUs may occupy a bigger space than choosing one three-phase PDU. Therefore, deploying three-phase PDUs will help to create a neat cabling organization.

Single-phase PDUs that are used in a single-phase power system are mostly found in residential settings that have small workloads instead of large-scale data centers. If you are operating a large data center that is carrying heavy workloads, a three-phase power distribution system is evidently more suitable.

According to Installation Methods: Horizontal vs Vertical PDU

Horizontal PDUs are installed in the rack and take up one or two rack spaces (1U-2U). Due to their smaller size, horizontal PDUs have fewer outlets. Whereas the vertical PDUs features a bigger outlook that can have up to 40 outlets. They fit on the upright rails of a rack enclosure without taking horizontal mounting space away from other equipment.

PDU Installation

For a high-density data center, an inch of land values an inch of gold. Obviously, the vertical PDUs provide a space-saving solution and tend to become nearly ubiquitous in today's data centers. Horizontal PDUs still provide effective choices: If the power loads are lower, or in order to protect the power through in-row UPS equipment, some may already be distributed from the U-space of the cabinet. In this situation, a series of horizontal PDUs is fit for this situation. In addition, the rear of the cabinet is off-limits in most cases, so to clear space for airflow, cable management must be as well-ordered as a circuit board. In this situation, moving the rack PDU out of the vertical cabling space and into the horizontal space will create a place for cable management.

Brief Summary

The IT architects are dedicated to deploying rack PDUs that are capable of supplying multiple circuits, higher voltages, and higher currents to accommodate the increased power distribution demands. Various types of PDUs have been introduced in this article, which may help you to determine your choices based on your needs. If you are considering purchasing some rack PDUs for your data centers, PDU Buying Guide may further give you some inspiration.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.7k