English

Best 10Gb Switches of 2023

Updated on Jan 20, 2023 by
7.7k

With all the different brands and types of 10Gb switches on the market, picking up the best 10G network switches for your unique needs can be somewhat confusing. That's where this article comes in handy. Before you buy any 10Gb switch, learn about its key features, such as speed and the number of ports. This article explains how to choose the best 10Gb switches and provides a comprehensive guide to FS 10Gb switches to help you choose the one that suits your needs the best.

 

     " Also check - FS 10Gb switches

 

How to Choose the Best 10Gb Switches?

You should take into consideration a number of key features of 10Gb switches, including speed, energy efficiency, switch ports, and switch functions, before making a choice. Now we will walk you through four key features that play an important role in the quality and performance of 10Gb switches.

 

     " Also check - How to Deploy 10G Switches in Spine-leaf Architecture?

 

Speed

A steady speed is what buyers are looking for in a 10G switch. If you have a shaky connection and your web speed slacks, you may want to check if the switch you've purchased can ensure a decent and steady speed. But speed is influenced by Ethernet, which means the switch itself cannot completely change or slow down your network speed. To err on the safe side, you do need to do a speed test on the 10Gb switch you're going to choose.

Energy Efficiency

This is a vital factor needed to be considered as you will keep the switch on for extended periods of time. Some 10G switches are configured with independent overload and short circuit protection, while others have LED indicators to show power status. These can help you keep on top of energy efficiency. Actually, specific power consumption largely depends on how heavily you deal with the data. Thus, you can choose a 10G switch that fits your needs with relatively low power consumption and high energy efficiency.

Switch Ports

Make sure that you get a 10Gb switch with a proper number of ports, neither less nor more than you have to use. The quantity of ports doesn’t ensure mean better performance. The number of 10G ports often comes with 8, 12, 24, or 48. Furthermore, the 8-port and 12-port 10Gb switches are commonly used for homes or small businesses. 24-port and 48-port 10G switches are mainly deployed in data centers or large enterprise networks. If you need a 10G network switch for home use where you need to connect it to 3-4 devices, buying a switch with 24 ports will be a waste.

Switch Functions

This factor means the highlight of 10G network switches of different types. 10G switches support some common features such as MLAG, IPv4/IPv6, VXLAN, NVGRE, SNMP, MSTP, etc. Those functions ensure that they can fit in both traditional and fully virtualized data centers. Some advanced security features such as Storm Control and IGMP Snooping are also available. They can monitor broadcast, multicast, or unknown unicast traffic to save bandwidth in the network. Thus, you should figure out all the functions a 10G switch has to offer.

A Comprehensive Guide to FS 10Gb Switches

Here we provide a comprehensive guide to FS 10Gb switches to help you choose the one that suits your needs the best.

Best FS 10Gb Switches in Price

FS S3900 series 10Gb switches offer the best value for money. FS S3900 10G switches are Gigabit Ethernet Layer 2/3 switches, which usually have 24 or 48 1G downlink ports and 4 10G uplinks for stacking. Besides, S3900 10G switches also support a variety of functions, such as advanced QoS, 1+1 redundant power supply, Dual Fans, etc, making them ideal for SMB, enterprise, campus, and branch office networks.

 

     " Also check - Deep Dive into FS S3900 Series Enterprise Switches

 

Best FS 10Gb Switches in Switch Ports

In terms of the number of switch ports, FS S5850-48S6Q and S5800-48T4S 10Gb switches definitely top the list. FS S5850-48S6Q 10Gb switches is a high-performance Layer 3 Leaf switch with 48x 10Gb SFP+ access ports and 6x 40Gb QSFP+ ports. They deliver rich layer 2 and layer 3 features with wire speed performance up to a maximum performance of 1.44 Tbps.

 

     " Also check - FS S5850 Series Switch FAQs

 

FS S5800-48T4S 10Gb switches come with 48x 10/100/1000BASE-T RJ45 access ports and 4x 10Gb uplink ports, delivering non-blocking forwarding of 176Gbps combined with feature-rich L2 and L3 switching. They provide a powerful Layer 3 routing solution for next-generation enterprises, data centers, and Metro networks.

Best FS 10Gb Switches in Switch Functions

FS S5860-20SQ 10Gb switch certainly lives up to its name as the best FS 10Gb switch in the aspect of switch functions. The switch adopts cutting-edge Broadcom chips to deliver 760 Gbps switching capacity and 565 Mpps forwarding rate. It supports a wide variety of functions, such as QoS, IGMP Snooping, Link Aggregation, IPv6, L3 Static Routing, RIP, OSPF, etc. FS S5860-20SQ 10Gb switches are ideal for large-scale campus network aggregations, and small and medium-sized network cores, to meet the needs of high-speed, safe, intelligent networks.

Note: S5860-20SQ now supports AC or DC power supply.

 

     " Also check - Create High-Performance Enterprise Networks with FS S5860 Series Switches

 

Final Thoughts

Although we've looked into how to choose the best 10Gb switches, the reality is that there are so many options out there that it’s hardly possible to narrow them down. Each has its own merits and downsides. In a word, you'd better shop around and purchase a 10G network switch based on your own needs and requirements.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k