English

Centralized Split vs Distributed Split in PON Based FTTH Networks

Updated on Dec 10, 2021 by
27.0k

FS PLC splitter

Passive optical network (PON) based FTTH access network is a point-to-multipoint, fiber to the premises network architecture in which passive optical splitters are used to enable a single optical fiber to serve multiple premises. The optical fiber splitter can be placed in different locations of the PON based FTTH network, which involves using centralized (single-stage) or distributed (multi-stage) split architecture in the distribution portion of the FTTH network. In fact, both methods have their own advantages and disadvantages. Then which one should you deploy? A comparison between centralized split and distributed split will be explored in this article.

Centralized Split Architecture Overview

A centralized split approach generally uses a combined split ratio of 1:64 with a 1:2 splitter in the central office, and a 1:32 in a cabinet. These single-stage optical splitters can be placed at several locations in the network or housed at a central location. But in most cases, the centralized optical splitters are placed in the outside plant (OSP) to reduce the amount of overall fiber required. The OLT (Optical Line Terminal) active port in the central office (CO) will be connected/spliced to a fiber leaving the CO. This fiber passes through different closures to reach the input port of the fiber splitter, normally placed in a cabinet. The output port of this fiber splitter goes to the FTTH distribution network, reaching the homes of potential customers through different closures and indoor/outdoor terminal boxes known as ONT (Optical Network Terminal). Thus, the PON network connects one OLT port to 32 ONTs in this centralized split topology.

Centralized Splitting vs Distributed Splitting in PON 1

Figure 1: Centralized split

Distributed Split Architecture Overview

Unlike centralized split topology, a distributed split architecture has no fiber splitters in the central office. The OLT port is connected/spliced directly to an outside plant fiber. The first level of splitting (1:4 or 1:8) is installed in a closure, not far from the central office. The input of this first level fiber optic splitter is connected with the OLT fiber coming from the central office. The second level of fiber splitters (1:16 or 1:8) resides in terminal boxes, very close to the customer premises with each splitter covering 8 to 16 homes. The inputs of these PON splitters are the fibers coming from the outputs of the first level splitters described above.

Distributed splitting in PON

Figure 2: Distributed split

Centralized Splitt vs Distributed Split in FTTH-PON Network

From the introduction of centralized split and distributed split networks above, it’s known that in centralized splitting networks, all PON splitters are located in one closure, which will maximize OLT utilization and provide a single point of access for troubleshooting. But since optical splitters must be terminated to the customer either through individual splices or connectors, the cost of distribution cables will be very high.

In terms of distributed splitting methods, the PON splitters are located in two or more different closures, which will minimize the amount of optical fibers that needs to be deployed to provide service. But it may create inefficient use of OLT PON ports and may increase the testing and turn-up time of customers.

 

In optical networking, the advantages and disadvantages of centralized split and distributed split networks are summarized in the table below:
FTTH Splitt Types Advantages Disadvantages
Centralized Split OLT utilization (pay as you grow) More distribution fiber
Future proof & easy to change technology Larger network elements in the OSP
Monitoring & maintenance Possibly additional infrastructure
Distributed Split Lower capital expense for customer connection More actives and more splitters
Reduces splitter cabinet requirements Less flexible network
Flexibility in split ratios in serving area Fewer monitoring & maintenance capabilities

How to Choose Between Centralized Split vs Distributed Split?

Except for the information about the differences between Centralized Split vs Distributed Split two deployment methods, here are also a few tips on how to decide on which one to choose. FTTH network architecture will depend on a variety of factors, including your budget and anticipated future scalability.

In addition, the density of your customer base is also one of the most deciding factors. In urban locations, distributed split would be the best for fast scaling and connecting for many users. On the other hand, centralized split is better considering the flexibility for rural or less populated areas.

Conclusion

Before deciding which splitting methods to use in a PON-based FTTH network, please always consider every unique aspect of your network case. Since centralized split vs distributed split have their pros and cons, the best architecture is the one that meets the requirements and expectations of the provider by reducing capital expenses, optimizing long-term operational expenses, and making a future-proof network that can cope with new technologies without dramatic changes.

 

FS PLC splitters

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.9k