English

Cloud & AI: 2021 Key Trends in Business Video Surveillance

Updated on Oct 27, 2021 by
2.2k

Business video surveillance has received considerable benefits from technological advancements. Higher megapixel cameras, better image compression standards and wider field of view are driving better image quality, less bandwidth consumption and improved data storage.

Since security and safety are still the highest priority of every organization present around the globe, all industries and companies are avidly looking forward to the latest and trending technologies in the video surveillance industry where the rapid advancement of artificial intelligence has spurred a shift from traditional video surveillance to a hybrid cloud-based and AI-powered video surveillance.

Trend #1: AI Technology in Business Video Surveillance

Business video surveillance systems backed by AI technology have a number of important features and abilities. The application of AI (Artificial intelligence) has vastly improved the accuracy of detection, reducing the incidence of false alarms. Among all the improvements that AI has brought to video surveillance, human analytics and facial recognition are of the highest expectation.

AI-powered Video Surveillance

Human Analytics

In traditional video surveillance systems, AI video analytics are generally deployed at the NVRs along with AI computers, but with the trending video surveillance systems we shall see the capabilities built directly into the IP camera itself. The use of AI in trending video surveillance can identify humans and differentiate them from other objects such as vehicles.

Artificial intelligence has enabled security cameras with human analytics to identify human behavior for both security-related and non-security-related purposes, such as recognition of an individual passing by, and conduct more complex behavior analysis such as motion heatmapping, foot traffic counting, and suspicious behavior.

For security-related purposes, intelligent analytics in video surveillance can gather access data and detect violation behaviors and emergencies such as fires, floods, etc, to avoid security risks. For example, it can be used to monitor traffic flow to identify some dangerous incidents. As for non-security-related purposes, which in other words is mostly to improve business management efficiency, a typical example is that heatmapping is expected to be taken advantage of by many businesses to measure density and activity across, so as to improve staff awareness and customer service.

Facial Recognition

AI facial recognition has taken video surveillance a step further. It equips video surveillance systems with deep learning capabilities to analyze video pixel by pixel without any human interaction to avoid security risks. It can be used to detect faces in intelligent access control, transportation, banks, commercial buildings, etc.

Facial recognition technology is getting more intelligent and precise. With higher-resolution cameras and the support of more advanced artificial intelligence, the applications of facial recognition are expected to be more often adopted in multiple business video surveillance solutions in the coming years, such as solutions for transportation, commercial environments, etc.

Video Management System (VMS)

Video management needs to be achieved manually in traditional business video surveillance systems with business owners investing in monitoring staff. But now with AI technology, data analysis and corresponding decision-making actions can be achieved autonomously with AI-powered video management software rather than human intervention. Suspicious behaviors and high-risk scenarios within the monitored area can be detected by the software and the AI in the VMS will take the next step to react, which could be an alert message sent to the first responder to minimize loss and risks.

Trend #2: Cloud Video Surveillance Solutions

Cloud is being used among all sorts of businesses due to the many benefits it provides. A cutting-edge cloud-based surveillance solution has dramatically revolutionized the way security systems operate. It cut the costs of personnel and requires far fewer devices maintenance than traditional on-premise systems. What other benefits does it bring into business video surveillance? Keep reading to find out.

Cloud-based Video Surveillance

Easy and Remote Access

Cloud-based business video surveillance solutions allow the video data to be monitored and managed from virtually anywhere. Unlike traditional business video surveillance systems which store video data on a physical hard drive or local servers using wired connections, cloud video surveillance system can record and store footage wirelessly in a cloud storage with an Internet connection. Moreover, the cloud allows the users to have 24/7 access to the footage, from anywhere and at any time.

Data Backup

Video footage recorded by an onsite recorder such as an DVR is easier and more vulnerable to theft or damage. If the recorder in a traditional surveillance system gets damaged, the footage will be gone for good. But having the footage recorded to the cloud will provide additional data backup. In other words, no matter how badly the physical video surveillance system is destroyed, the users will still have the access to the footage which has already been backed up in the cloud.

Flexibility & Scalability

In traditional video surveillance, business owners have to spend money on network video recorders (NVRs) to connect the cameras and store the video footage. The storage space of the NVR and how many channels the NVR has depend on how many cameras will be deployed in the system. But in cloud video surveillance solutions with flexible cloud storage, you won't need video recorders any more. In addition, If the users require larger storage space, it can be updated to a larger one without changing any deployment.

Not just NVRs, neither are other extensive on-premise devices or equipment required in cloud video security systems, which not only saves lots of expenditures on hardware and devices, but also makes the system inherently more scalable with no need for complex on-site installations.

Conclusion

With further technological advancement, traditional video surveillance systems will no longer satisfy the requirements of future business security and that's when AI and cloud will be applied to the business video surveillance solutions. A hybrid AI-powered cloud-based video surveillance system overcomes many concerns in traditional systems, such as complex deployment and installation, data loss, high maintenance cost, system failures, etc.

It's an inevitable trend that AI and cloud will take over in business video surveillance systems. With increased security, ease of use and so many other benefits it brings, hybrid cloud video surveillance will be for sure a better alternative to traditional one for many businesses.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k