English

CWDM - Cost-Effective Alternative to Expand Network Capacity

Updated on Jul 23, 2021 by
14.8k

Fiber optic cabling is highly favorable in the telecommunication world. However, deploying fiber cabling for each individual service can be cost prohibitive, thus Wavelength Division Multiplexing (WDM) technology shines out as an optimal choice - it combines multiple signals onto a single fiber strand by using several wavelengths (frequencies) of light - each frequency carrying a different type of data, enabling cost-efficient upgrade of network capacity. WDM has two variations: Coarse WDM (CWDM) and Dense WDM (DWDM), in which CWDM is well suited to the needs of enterprise networks and metropolitan short-distance transmission.

 

CWDM Technology - Alternative for Increasing Transmission Capacity

CWDM was standardized by the ITU-T G.694.2 based on a grid or wavelength separation of 20 nm in the range of 1270-1610 nm. It can carry up to 18 CWDM wavelengths over one pair of fibers. Each signal is assigned to a different wavelength of light. Each wavelength does not affect another wavelength, so the signals do not interfere. Each channel is usually transparent to the speed and type of data, so any mix of SAN, WAN, Voice, and Video services can be transported simultaneously over a single fiber or fiber pair.

cwdm-system

Figure 1: CWDM System

CWDM is a cost-effective solution to provide a capacity boost in the access network. It can address traffic growth demands without overbuilding the infrastructure. For example, a typical 8-channel CWDM system offers 8 times the amount of bandwidth that can be achieved using a SONET/SDH system for a given transmission line speed with the same optical fibers. It is a perfect alternative for carriers looking to increase the capacity of their installed optical network without replacing existing equipment with higher bit rate transmission equipment, and without installing new fibers.

Key CWDM Network Component: CWDM Mux Demux

A Mux is commonly known as a multiplexer which combines multiple wavelength channels on a single fiber, and a Demux separates them again at the other end. A Mux/Demux set-up is especially useful to increase the end-to-end capacity of deployed fiber. The Mux is typically located in the central office, and the Demux unit is located in either a cabinet or splice closure from which the fibers go to their destination in a star-shaped topology. CWDM Mux Demux provides a cost-effective and efficient way to meet bandwidth requirements in different network scenarios.

cwdm-mux-demux-1

Figure 2: CWDM Mux Demux

Dual-Fiber CWDM Mux Demux VS. Single-Fiber CWDM Mux Demux

CWDM Mux Demux types are divided into Single-fiber CWDM Mux Demux and Dual-Fiber CWDM Mux Demux. Dual-fiber CWDM Mux Demux enables up to 18 channels for transmitting and receiving 18 kinds of signals, with wavelengths from 1270 nm to 1610 nm. The CWDM transceiver inserted into the fiber optic Mux port should have the same wavelength as the Mux port to finish the signal transmission. Single-fiber CWDM Mux Demux should also be used in pairs. Considering that the single-fiber CWDM Mux Demux transmits and receives the integrated signals through the same fiber, the wavelengths for RX and TX of the same port on the single-fiber CWDM Mux Demux should be different. The working principle of single-fiber CWDM Mux Demux is more complicated, compared to the dual-fiber one.

Figure 3: Dual-Fiber CWDM Mux Demux VS. Single-Fiber CWDM Mux Demux

CWDM Applications

CWDM is applied primarily in two broad areas: metro and access network, performing two functions - one is to use each optical channel to carry a distinct input signal at an individual rate, and another is to use CWDM to break down a high-speed signal into slower components that can be transmitted more economically, such as some 10G transceivers.

CWDM in Metropolitan Area Network (MAN)

Metropolitan area network (MAN) refers to the network that covers the city and its suburbs, providing an integrated transmission platform for metropolitan areas. CWDM networks enable wavelength services to be provisioned over a large metro area, with the functional and economic benefits of full logical mesh connectivity, wavelength reuse, and low end-to-end latency. These features apply to the Inter-Office (CO-CO) and Fiber to the Building (FTTB) segments of the metro network. The low latency benefits of CWDM are especially attractive in ESCON and FICON/Fibre Channel-based SAN applications. The less space, low power, and cost benefits of CWDM also enable its deployment in the Outside Plant (OSP) or Remote Terminal (RT) segments of the metro market.

cwdm-in-metropolitan-area-network

Figure 4: CWDM in Metropolitan Area Network

CWDM in LAN and SAN Connection

CWDM has abundant network topology, such as point-to-point, ring, mesh, etc. The ring network can provide self-healing protection: the style of restoring includes link-breaking protection and node failure separation. CWDM rings and point-to-point links are well suited for interconnecting geographically dispersed LAN (local area network) and SAN (storage area network). Corporations can benefit from CWDM by integrating multiple Gigabit Ethernet, 10 Gigabit Ethernet, and Fibre Channel links over a single optical fiber for point-to-point applications or ring applications.

CWDM Integrated in 10 Gigabit Ethernet

With the benefits of low implementation cost, robustness, simplicity of installation, and maintenance, Ethernet has been used intensively in the metro/access system now. As the bandwidth increases, a higher data rate 10 Gigabit Ethernet was put forward. Ethernet integration with CWDM is one of the best-implementing methods. In one of the 10 Gigabit Ethernet standards in the IEEE 802.3ae is a four-channel, 1300nm CWDM solution. However, if CWDM were based on 10 channels of 1 Gbps, then 200 nm of the wavelength spectrum would be used. Compared with TDM (transmission time division multiplexing), 10G CWDM technology may have a higher initial cost, but it can offer better scalability and flexibility than TDM.

CWDM in PON (Passive Optical Network)

PON is a point-to-multipoint optical network that uses existing fiber. It is an economical way to deliver bandwidth to the last mile. Its cost savings come from using passive devices in the form of couplers and splitters, rather than higher-cost active electronics. PON expands the number of endpoints and increases the capacity of the fiber. But PON is limited in the amount of bandwidth it can support. As CWDM can multiply the bandwidths cost-effectively, when combining them, each additional lambda becomes a virtual point-to-point connection from a central office to an end user. If one end user in the original PON deployment grows to the point where he needs his own fiber, adding CWDM to the PON fiber creates a virtual fiber for that user. Once the traffic is switched to the assigned lambda, the bandwidth taken from the PON is now available for other end users. So the access system can maximize fiber efficiency.

wdm-pon-diagram

Figure 5: CWDM in PON

 

CWDM VS. DWDM

Wavelength Spacing

CWDM can transport up to 16 wavelengths with a channel spacing of 20 nm in the spectrum grid from 1270 nm to 1610 nm. While DWDM can carry 40, 80, or up to 160 wavelengths with a narrower spacing of 0.8 nm, 0.4 nm, or 0.2 nm from the wavelengths of 1525 nm to 1565 nm (C band) or 1570 nm to 1610 nm (L band).

cwdm-optical-spectrum

Figure 6: CWDM Wavelength Grid

Transmission Distance

DWDM multiplexing system is capable of having a longer haul transmission by keeping the wavelengths tightly packed. It can transmit more data over a larger run of cable with less interference than the CWDM system. CWDM system cannot transmit data over long distances as the wavelengths are not amplified. Usually, CWDM can transmit data up to 100 miles (160 km).

Modulation Laser

The CWDM system uses the uncooled laser while the DWDM system uses the cooling laser. Laser cooling refers to a number of techniques in which atomic and molecular samples are cooled down to near absolute zero through the interaction with one or more laser fields. Cooling laser adopts temperature tuning that ensures better performance, higher safety, and longer life span of DWDM system. But it also consumes more power than the electronic tuning uncooled laser used by the CWDM system.

Price

The DWDM price is typically four or five times higher than that of the CWDM counterparts. The higher cost of DWDM is attributed to the factors related to the lasers. The manufacturing wavelength tolerance of a DWDM laser die compared to a CWDM die is a key factor. Typical wavelength tolerances for DWDM lasers are on the order of ±0.1 nm, while tolerances for CWDM laser die are ±2-3 nm. Lower die yields also drive up the costs of DWDM lasers relative to CWDM lasers. Moreover, packaging the DWDM laser die for temperature stabilization with a Peltier cooler and thermister in a butterfly package is more expensive than the uncooled CWDM coaxial laser packing.

cost-comparison-of-cwdm-and-dwdm-technology

Figure 7: Cost Comparison of CWDM and DWDM Technology

CWDM offers lower price points as compared with DWDM and hence is extremely amenable to many cost-sensitive access and enterprise applications. In addition, CWDM is very simple in terms of network design, implementation, and operation. CWDM works with a few parameters that need optimization by the user. At the same time, DWDM systems require complex calculations of the balance of power per channel, which is further complicated when channels are added and removed or when it is used in a DWDM networks ring, especially when systems incorporate optical amplifiers. The following table shows the comparison of CWDM and DWDM:

Specifications/Features CWDM DWDM
Full form Coarse Wavelength Division Multiplexing, WDM system having less than 8 active wavelengths per optical fiber Dense Wavelength Division Multiplexing, WDM system having more than 8 active wavelengths per optical fiber
Characteristic Defined by wavelengths Defined by frequencies
Capacity lower higher
Cost low high
Distance short range communication long range communication
Frequencies uses wide range frequencies uses narrow range frequencies
Wavelength spacing more less, hence can pack 40+ channels compare to CWDM in the same frequency range
Amplification light signal is not amplified here light signal amplification can be used here
 

The Future of WDM Technology

According to the Dell’Oro Group, the wavelength division multiplexer (WDM) market revenue is forecasted to reach $14 billion by 2021 driven by the demand for 100+ Gbps coherent wavelengths. Enterprise direct purchasing for data center interconnect (DCI) will deeply influence the WDM market. DCI using WDM equipment is forecast to be a $2.4 B market by 2021. From these statistics, WDM equipment will have a good market in the near future. More recently, two new paradigmatic revolutions have made their way into the optical communication market: ROADM (Reconfigurable Optical Add-Drop Multiplexing) and Coherent Optical Systems. While these optical technologies are the perfect solutions to satisfy the growing demand for bandwidth, they also provide radical cost reduction in the information transmission market.

 

Conclusion

CWDM is an attractive solution for carriers who need to upgrade their networks to accommodate current or future traffic needs while minimizing the use of valuable fiber strands. CWDM’s ability to accommodate Ethernet on a single fiber enables converged circuit networks at the edge, and at high-demand access sites. With traffic demands continuing to rise, the popularity of CWDM with carriers in the access and metro networks will be akin to the popularity of DWDM in the long haul and ultra-long haul networks. In the near future, CWDM will continue to evolve into specialized applications. Combination transport and optical routers or switches are being developed now. Add-on CWDM cards are being included in more transport devices as low cost options. Suppliers are continuing to drive down costs and increase capacity.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.9k