English

Data Center Infrastructure Basics and Management Solutions

Updated on Mar 26, 2022 by
6.6k

Data center infrastructure refers to all the physical components in a data center environment. These physical components play a vital role in the day-to-day operations of a data center. Hence, data center management challenges are an urgent issue that IT departments need to pay attention to. On the one hand, it is to improve the energy efficiency of the data center; on the other hand, it is to know about the operating performance of the data center in real-time ensuring its good working condition and maintaining enterprise development.

Data Center Infrastructure Basics

The standard for data center infrastructure is divided into four tiers, each of which consists of different facilities. They mainly include cabling systems, power facilities, cooling facilities, network infrastructure, storage infrastructure, and computing resources.

There are roughly two types of infrastructure inside a data center: the core components and IT infrastructure. Network infrastructure, storage infrastructure, and computing resources belong to the former, while cooling equipment, power, redundancy, etc. belong to the latter.

Core Components

Network, storage, and computing systems are vital infrastructures for data centers to achieve sharing access to applications and data, providing data centers with shared access to applications and data. Also, they are the core components of data centers.

Network Infrastructure

Datacenter network infrastructure is a combination of network resources, consisting of switches, routers, load balancing, analytics, etc., to facilitate the storage and processing of applications and data. Modern data center networking architectures, through using full-stack networking and security virtualization platforms that support a rich set of data services, can achieve connecting everything from VMs, containers, and bare-metal applications, while enabling centralized management and fine-grained security controls.

Storage Infrastructure

Datacenter storage is a general term for the tools, technologies and processes for designing, implementing, managing and monitoring storage infrastructure and resources in data centers, mainly referring to the equipment and software technologies that implement data and application storage in data center facilities. These include hard drives, tape drives and other forms of internal and external storage and backup management software utilities external storage facilities/solutions.

Computing Resources

A data center meter is a memory and processing power to run applications, usually provided by high-end servers. In the edge computing model, the processing and memory used to run applications on servers may be virtualized, physical, distributed among containers or distributed among remote nodes.

IT Infrastructure

As data centers become critical to enterprise IT operations, it is equally important to keep them running efficiently. When designing data center infrastructure, it is necessary to evaluate its physical environment, including cabling system, power system, cooling system to ensure the security of the physical environment of the data center.

Cabling Systems

The integrated cabling is an important part of data center cable management, supporting the connection, intercommunication and operation of the entire data center network. The system is usually composed of copper cables, optical cables, connectors and wiring equipment. The application of the data center integrated wiring system has the characteristics of high density, high performance, high reliability, fast installation, modularization, future-oriented, and easy application.

Power Systems

Datacenter digital infrastructure requires electricity to operate. Even an interruption of a fraction of a second will result in a significant impact. Hence, power infrastructure is one of the most critical components of a data center. The data center power chain starts at the substation and ends up through building transformers, switches, uninterruptible power supplies, power distribution units, and remote power panels to racks and servers.

Cooling Systems

Data center servers generate a lot of heat while running. Based on this characteristic, cooling is critical to data center operations, aiming to keep systems online. The amount of power each rack can keep cool by itself places a limit on the amount of power a data center can consume. Generally, each rack can allow the data center to operate at an average 5-10 kW cooling density, but some may be higher.

Data Center Infrastructure Management Solutions

Due to the complexity of IT equipment in a data center, the availability, reliability, and maintenance of its components require more attention. Efficient data center operations can be achieved through balanced investments in facilities and accommodating equipment.

Energy Usage Monitoring Equipment

Traditional data centers lack the energy usage monitoring instruments and sensors required to comply with ASHRAE standards and collect measurement data for use in calculating data center PUE. It results in a poor monitoring environment for the power system of the data center. One measure is to install energy monitoring components and systems on power systems to measure data center energy efficiency. Enterprise teams can implement effective strategies by the measure to balance overall energy usage efficiency and effectively monitor the energy usage of all other nodes.

Cooling Facilities Optimization

Independent computer room air conditioning units used in traditional data centers often have separate controls and set points, resulting in excessive operation due to temperature and humidity adjustments. It's a good way for helping servers to achieve cooling by creating hot-aisle/cold-aisle layouts to maximize the flow of cold air to the equipment intakes and the hot exhaust air from the equipment racks. The creation of hot or cold aisles can eliminate the mixing of hot and cold air by adding partitions or ceilings.

CRAC Efficiency Improvement

Packaged DX air conditioners likely compose the most common type of cooling equipment for smaller data centers. These units are often described as CRAC units. There are, however, there are several ways to improve the energy efficiency of the cooling system employing DX units. Indoor CRAC units are available with a few different heat rejection options.

  • As with rooftop units, adding evaporative spray can improve the efficiency of air-cooled CRAC units.

  • A pre-cooling water coil can be added to the CRAC unit upstream of the evaporator coil. When ambient conditions allow the condenser water to be cooled to the extent that it provides direct cooling benefits to the air entering the CRAC unit, the condenser water is diverted to the pre-cooling coil. This will reduce or sometimes eliminate the need for compressor-based cooling for the CRAC unit.

DCIM

Data center infrastructure management is the combination of IT and operations to manage and optimize the performance of data center infrastructure within an organization. DCIM tools help data center operators monitor, measure, and manage the utilization and energy consumption of data center-related equipment and facility infrastructure components, effectively improving the relationship between data center buildings and their systems.

DCIM enables bridging of information across organizational domains such as data center operations, facilities, and IT to maximize data center utilization. Data center operators create flexible and efficient operations by visualizing real-time temperature and humidity status, equipment status, power consumption, and air conditioning workloads in server rooms.

Preventive Maintenance

In addition to the above management and operation solutions for infrastructure, unplanned maintenance is also an aspect to consider. Unplanned maintenance typically costs 3-9 times more than planned maintenance, primarily due to overtime labor costs, collateral damage, emergency parts, and service calls. IT teams can create a recurring schedule to perform preventive maintenance on the data center. Regularly checking the infrastructure status and repairing and upgrading the required components promptly can keep the internal infrastructure running efficiently, as well as extend the lifespan and overall efficiency of the data center infrastructure.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.7k