English

Cisco 3560 Switch Replacements: 1G to 10G Access Upgrade

Updated on Jan 7, 2022 by
9.9k

Today’s question is about network switch replacement. This is a question that most data centers have to face in a time. Because devices there have spent their whole lives or the growth in data traffic quantity has outpaced their capacity. Here take Cisco 3560 switch replacements as an example.

User’s Question: What would you guys recommend to replace some Cisco 3560 switch? Need to keep budget small, but need to do VLANs and multiple port trunks and having some 10GbE capabilities. This will be used for data center.

Answer: Basically, you’re saying that you’d like to replace some Cisco 3560 switches with new switches that support VLANs, multiple port trunking (usually by using link aggregation control protocol [LACP]) and have some 10G ports, right? And on the premise of “keeping the budget small”.

As shown in the following figure (right), in data center Cisco 3560s are commonly used as access switches that connect servers and applications to the network, and the top-tier switch is usually 3750. Since you need to replace 3560 with an access switch that is capable of 10G, Cisco 3650 would be the closest thing. At the meantime, the top-tier switch 3750 is usually displaced by Cisco 3850/Nexus FEX, in essence a change from 1G uplink to 10G uplink.

The change will not bring much trouble to you when you need to install the devices and get support from Cisco Certified Network Assistant. Below are the major differences between Cisco 3560 switches and 3650 switches.

Differences Between Cisco 3560 and 3650 Switch

Cisco 3650 Series

Juniper EX3400 Series

Juniper EX4300 Series

FS S3900 Series


Differences Between Cisco 3560 and 3650 Switch


Comparision of Cisco Catalyst 3560 and 3650
Feature Catalyst 3560 Catalyst 3650
Optional stacking No Yes (160 Gbps)
Native wireless controller supoort over Cisco IOS Software No Yes
Wireless scalability No 25 AP's/1000 clients
10G uplinks 2x10 G (field-replaceable unit [FRU]) 8x10 G, 4x10 G or 2x10 G (fixed)
Buffers per 48 port 6 MB 12 MB
L3 feature Full L3 Full L3
Operating system IOS IOS-XE
Multi-core CPU for hosted services No Yes
Maximum number of VLANs 1,024 (L2) 4,094 (L2)
Total number of MAC address 12,000 32,000

Cisco 3650 Series

The 10G ports of 3650s have three choices. Here are the Cisco 3650 models that can be configured with different numbers of 10G ports:

10G Ports Models Total 10/100/1000 Ethernet Ports Price (US$)
8x10G SFP+ WS-C3650-12x48UR 48 UPOE (including 12 100/1G/2.5G/5G/10G ports) MSRP: 15,800.00
4x10G SFP+ WS-C3650-12x48UQ 48 UPOE (including 12 100/1G/2.5G/5G/10G ports) MSRP: 12,000.00
WS-C3650-8x24UQ 24 UPOE (including 8 100/1G/2.5G/5G/10G ports) MSRP: 8,600.00
WS-C3650-48PQ 48 PoE+ 3,998.11 - 7,035.33
WS-C3650-48TQ 48 3,569.98 - 6,722.99
2x10G SFP+ WS-C3650-48PD 48 PoE+ 3,220.00 - 7,242.99
WS-C3650-24PD 24 PoE+ 1,883.00 - 3,762.74
WS-C3650-48TD 48 2,900.00 - 5,305.86
WS-C3650-24TD 24 1,783.90 - 3,795.99

Considering the vendors might give you a discount, you could get one 3650 series switch at much lower cost than the MSRP (Manufacture Suggested Retail Price). However, these prices do not include optics or software licenses. Besides Cisco 3650, I know some alternatives that are also fairly good 10G access switches in practical use. They are completely affordable and can meet all your needs.

Juniper EX3400 Series

The first type is Juniper EX3400 series switches. EX3400 offers up to 4096 VLANs on Layer 2. All of them have four 10G SFP+ ports (and two 40G ports). The PoE ability is also optional.

Model Ports Price (US$) Max. VLANs Total MAC address
EX3400-24T 241000BASE-T, 4SFP+, 2QSFP+ 959.00 - 1,848.00 4,096 (L2) 32,000
EX3400-24P 241000BASE-T PoE+, 4SFP+, 2QSFP+ 1,112.00 - 3,255.75
EX3400-48T 481000BASE-T, 4SFP/SFP+, 2QSFP+ 2,110.00 - 4,866.98
EX3400-48P 481000BASE-T PoE+, 4SFP+, 2QSFP+ 2,175.80 - 7,256.98
Maximum Switching Capacity: 24T/24P -- 288Gbps, 48T/48P -- 336Gbps

Juniper EX4300 Series

The second type is Juniper EX4300 series switches.

Model Ports Price (US$) 10G Uplink Module Option Max. VLANs Total MAC address
EX4300-24T 241000BASE-T, 4QSFP+ 1,270.00 - 2,868.95 4-port 10G module with SFP+ optics 4.093 (L2) 64,000
EX4300-24P 241000BASE-T PoE+, 4QSFP+ 1,341.00 - 3,296.89
EX4300-48T 481000BASE-T, 4QSFP+ 3,037.19 - 7,256.98
EX4300-48P 481000BASE-T PoE+ 2,449.00 - 5,865.40
EX4300-32F 321000BASE SFP, 4SFP+, 2QSFP+ 3,225.00 - 12,766.98 8-port 10G module with SFP+ optics
Maximum Switching Capacity: 24T/24P -- 448Gbps, 48T/48P -- 496Gbps, 32F -- 464Gbps

Two other switch models from Arista have similar performance with switches mentioned above. But not many vendors can supply them now and the price is much higher compared with others.

Model Ports Price (US$) Max. VLANs Total MAC address
7010T-48 481000BASE-T, 4SFP+ 38,154.16 - 39,169.33 4,096 (L2) 16,000
7048T 481000BASE-T, 4SFP+ 11,018.95 4,094 (L2) 16,000

FS S3900 Series

One more choice is the S3900 series switch from FS. They can do the same job as the switches mentioned above at a lower cost. All the S3900 switches are stackable, and they have 10/100/1000BASE-T RJ45 ports, with 10Gb SFP+ uplinks, meeting your various network needs. Options of CLI/WEB/SNMP/SSH for easy and flexible management. Below are the FS S3900 series switch models.

Model Ports Price (US$) Max. VLANs Total MAC address
S3900-24T4S 24x 10/100/1000BASE-T RJ45, 4x 10G SFP+ 329.00 4,000 (L2) 16,000
S3900-48T4S 48x 10/100/1000BASE-T RJ45, 4x 10G SFP+ 529.00 4,000 (L2) 16,000
S3900-24F4S 20x 1G SFP, 4x 1G RJ45/SFP Combo | 4x 10G SFP+ 479.00 4,000 (L2) 16,000
S3900-24F4S-R 16x SFP ports, 8x 1G RJ45/SFP Combo | 4x 10G SFP+ 439.00 4,000 (L2) 16,000
S3900-24T4S-R 24x 10/100/1000BASE-T RJ45 | 4x 10G SFP+ 329.00 4,000 (L2) 16,000
S3900-48T6S-R 48x 10/100/1000BASE-T RJ45 | 6x 10G SFP+ 459.00 4,000 (L2) 16,000

Summary

Turning to the 10G network might be an urgent problem for lots of enterprises and SMBs. Choosing the right replaced switches and having a suitable network plan is an essential step. All these switches we mentioned above are great choices. And if you need other switch replacement recommendations, please contact sales@fs.com for professional advice or you can check fs.com to see more switch types and network solutions.


Related Articles: Cisco Catalyst 3750 Series Switches SFP Port Connections

Cisco ME 3400 Series Switches Cabling Details Optics Solutions for Cisco Catalyst 4500-X Series Switch

Tags

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.7k