RJ45 Connector and Keystone Jack: Learn the Difference
RJ45 connectors and Keystone jacks are vital components in networking setups. This article will explore their differences from several perspectives to help you choose the appropriate termination type.
RJ45 Connector and Keystone Jack: What are They?
Introduction of RJ45 Connector
RJ45 connectors are standardized connectors used to terminate twisted pair cables, most commonly Ethernet cables. They have eight pins and are designed to interface with Ethernet ports on networking devices such as computers, routers, switches, and hubs.
RJ45 connectors are typically crimped onto the ends of Ethernet cables using a specialized crimping tool. They provide a reliable and standardized means of connecting network devices. For further information about RJ45 connectors, you can refer to the article: Introduction of the RJ45 Interface.
Introduction of Keystone Jack
Keystone jacks are modular connectors that snap into wall plates, patch panels, or surface mount boxes to provide a termination point for Ethernet cables. Keystone jacks provide a convenient way to install and manage network connections in wall outlets and other locations.
They typically feature a female RJ45 connector on one side and terminals on the other side for punching down the individual wires of an Ethernet cable. Keystone jacks are often used in structured cabling systems to create clean and organized network installations.
RJ45 Connector and Keystone Jack: What's the Difference?
While both RJ45 connector and Keystone jack serve important roles in networking, they differ in structure, application, compatibility, and cost, catering to different needs in network setups.
Structure
-
RJ45 Connector: Typically features a male interface with eight pins arranged in a specific configuration to transmit data signals over twisted pair Ethernet cables. They often have a plastic housing with a locking tab for securing the connection.
-
Keystone Jack: Keystone jacks are modular connectors with a female interface. They can snap into faceplates, patch panels, or surface mount boxes. Keystone jacks come in different configurations to support different types of connections, including RJ45 for Ethernet.
Application
-
RJ45 Connector: Primarily used for terminating Ethernet cables. They are commonly employed in networking setups for connecting devices like computers, routers, switches, and hubs to Ethernet networks.
-
Keystone Jack: Used to terminate Ethernet cables at wall outlets, patch panels, or surface mount boxes, providing a modular and customizable solution for network connectivity. This article: How to Terminate and Install Cat5e, Cat6 Keystone Jacks? guide terminating network cables with Keystone jacks.
RJ45 Connector and Keystone Jack: How to Choose?
When deciding between RJ45 connectors and Keystone jacks to meet your networking needs, several factors should be considered:
-
Application Requirement: Consider your network setup, and ensure that the connectors and jacks you choose are compatible with your existing networking devices, such as Ethernet cables, patch panels, and wall plates.
-
Network Performance: Ensure that the specific product you choose meets the performance requirements of your network, especially if you're dealing with high-speed connections like Gigabit Ethernet or above.
-
Future Scalability: Anticipate future growth and expansion of your network infrastructure to accommodate potential changes and upgrades.
-
Reliability: Choose reputable brands and manufacturers to ensure the stability and long-term reliability of the jacks and connectors.
Conclusion
To summarize, RJ45 connectors and Keystone jacks are both utilized in networking, differing primarily in compatibility and application. RJ45 connectors are specialized for Ethernet networking, whereas Keystone jacks provide a versatile, modular solution capable of accommodating diverse connector types to meet various networking requirements.
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023