Differences Between Router and Switch
When constructing a network for a small office, switches and routers are the fundamental equipment that is crucially required. Despite their similar appearances, these devices serve distinct purposes within a network. This article mainly talks about the differences between switches and routers to help you better understand them.
What Is A Network Switch?
Switches enable collaboration and resource sharing among various devices, such as computers, printers, and servers, within a small business network. By connecting these devices, switches enable seamless information sharing and communication, regardless of their physical location within a building or campus. The integration of switches is indispensable when constructing a small business network, as they serve as the crucial link that binds all devices together.
What Is A Router?
Similar to how a switch facilitates the connection of multiple devices to create a network, a router establishes connections between multiple switches and their respective networks, thereby forming a larger network. These networks can be situated in a single location or spread across multiple locations. When setting up a small business network, one or more routers are required. Apart from linking multiple networks, routers enable networked devices and multiple users to access the Internet.
In essence, a router functions as a dispatcher within a network, efficiently directing traffic and selecting the optimal path for data packets to travel. It serves as the gateway between your business and the external world, safeguarding information from security threats, and even determining device prioritization.
Switch vs Router: 8 Key Differences
-
Operational OSI model layers
Router: As per the ISO-OSI model, routers operate at layer 3, known as the network layer. Their role involves directing data packets to their intended destinations based on the IP address specified in the layer-3 IP packet. After forwarding the packet, routers do not retain any memory of its contents.
Network switch: Conversely, network switches operate at the data link layer, which corresponds to layer 2 of the OSI model. These switches perform error checks before forwarding data packets, resulting in improved efficiency. Furthermore, multilayer switches possess the capability to forward data at layer 3 by incorporating routing functionality.
-
Contrasts in their broadcast domains
Router: Routers have individual broadcast domains for each of their ports. The broadcasting domain in routers is divided into segments, preventing propagation.
Network switch: On the other hand, a network switch typically has a single broadcast domain, unless virtual LANs are utilized. An Ethernet switch establishes a distinct collision domain for each of its ports. This allows connected devices to transmit data without encountering any issues. As devices are connected to switch ports, each port becomes its own collision domain, effectively eliminating collisions.
-
Utilization of routing tables during the transmission process
Routers: Routers possess the ability to store IP addresses in routing tables and maintain their own address. Upon receiving a data packet, routers examine the existing routing tables to locate the most suitable match between the addresses in their routing tables and the IP address of the packet's intended destination. Only then do they forward the packet toward its final destination.
Network switch: In contrast, network switches utilize content-accessible memory (CAM) tables to determine MAC addresses for reaching their destinations. This functionality is typically facilitated by application-specific integrated chips (ASIC). Additionally, network switches can store MAC addresses in a lookup table and maintain their address.
-
Modes of transmission
Router: By default, routers operate in full-duplex mode for transmission. However, users have the option to switch to half-duplex mode based on their preferences. Routers generally experience fewer collisions, as collisions have a negative impact on network efficiency.
Network switch: Data transmission in network switches can occur in both full and half-duplex modes. Users can choose to use auto-negotiation mode based on their preferences. Switches divide networks into segments, effectively creating smaller collision domains. In half-duplex mode, each device connected to a switch port operates within its own collision domain. In contrast, full-duplex mode eliminates the risk of collisions by having separate transmitters and receivers, ensuring more efficient transmission.
-
Network types
Router: Routers find applications in a range of environments, including wide area networks (WANs), local area networks (LANs), and metropolitan area networks (MANs). The speed of these network devices varies based on the specific environment they are deployed in. For example, in MAN or WAN setups, routers operate at a faster pace compared to network switches.
Network switch: On the other hand, network switches are exclusively utilized in LAN environments. Within LANs, network switches offer higher speed and performance.
-
Ports differences
Router: Routers are equipped with two ports during manufacturing. However, additional serial ports can be added as required, offering options of 2, 4, or 8 ports. Routers comprise both hardware and software ports. Hardware ports include WAN and LAN ports, as well as USB ports. Software ports enable routers to determine the allocation of data packets and track them. Each application is assigned a specific port number.
Network switch: In contrast, network switches are multiport network bridges. The number of ports in a switch varies based on its intended function. For instance, a home router may have 5 ports, while a larger network switch can accommodate up to 52 ports. The number of devices that can connect to an Ethernet switch is always one less than the total number of physical ports available on the switch. One port on the switch is typically reserved for the connection that links the switch to the router. The switch includes various types of ports, such as access ports, trunk ports, and hybrid ports.
-
Data formats
Router: Routers transmit data in the form of packets.
Network switch: In contrast, data is transmitted in network switches in both frame and packet formats. In L2 switches, data is transmitted in frame form, while in L3 switches, it is conveyed in both frame and packet formats.
-
Translation of port and network addresses
Router: They possess the capability to perform network address translation (NAT) and port address translation (PAT). NAT allows multiple devices to access the internet using a single public address, addressing IP address shortages in IPv4 networks. It also enhances security by concealing the entire network's IP address. PAT, although less flexible than NAT, provides additional address expansion by utilizing unique host port numbers within the global IP address to differentiate translations. Furthermore, routers offer additional services like NetFlow and quality of service (QoS).
Network switch: Conversely, network switches cannot perform NAT or PAT. They also do not provide QoS or NetFlow services.
Conclusion
In the end, a fully functional networking environment cannot exist without routers and switches. Switches connect multiple endpoints to enable resource sharing within a confined network. On the other hand, routers have a broader role in directing traffic between the public or private internet and local destinations. Understanding these differences between switches and routers enables you to utilize them effectively and maximize your network capacity.
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023