English

Ethernet Media Converter Tutorial

Updated on Jan 9, 2024 by
10.3k

 Media Converter

For networking scenarios where the standard 100-meter reach of copper Ethernet cables (UTP or STP) is insufficient, Ethernet media converters for extended distance connectivity present a professional solution to extend connectivity. These devices serve as a bridge, converting signals between copper cables and fiber optics to facilitate long-range Ethernet transmission seamlessly. This article will give you a comprehensive guide to Ethernet media converter usage guide.

What Is an Ethernet Media Converter?

An Ethernet media converter, also known as a fiber to Ethernet converter, is widely applied when distances between two network devices exceed the transmission distance of copper cabling. It can also be used to convert the electrical data signals into light pulses that travel over fiber optic cabling if EMI/RFI emissions or interference arise issues. Because it can electrically isolate both network nodes, eliminating any ground loop concerns or voltage spikes from lightning. It’s also useful for your network transmission since it’s virtually impossible to tap into the transmitted fiber to Cat6 converter signal without detection.

 Media Converter

The Benefits of Using a Media Converter

In modern Local Area Networks (LANs), the complexity arises from the need for high-speed and long-distance data transmission. Media converters play a crucial role in addressing these challenges by seamlessly integrating fiber when required, facilitating efficient expansion within existing cable infrastructure. This pivotal function contributes significantly to the establishment of reliable and cost-effective networks. Now, let's take a look at the key benefits and advanced functions supported by media converters.

Key benefits include:

Speed: Ensures efficient task completion.

Network Expansion: Facilitates the integration of new equipment with enhanced quality and strength.

Economical: Integrates fiber and copper networks without the need for extensive expensive infrastructure.

Reduced Interference: Gentle transition between copper and fiber minimizes electromagnetic interference.

 Media Converter Key benefits

Media converters support advanced functions:

Switch Technology: Enables Ethernet networks at switching rates of 10/100 and 10/100/1000.

Advanced Functions: Supports VLAM, Quality of Service (QoS), Port Access Control, Bandwidth Control.

Deployment Facilitation: Enables new data, voice, and video deployment.

Cost Efficiency: Reduces CAPEX by preserving legacy equipment and allows WDM through wavelength conversion.

Operational Efficiency: Lowers OPEX by offering remote network configuration and troubleshooting in limited personnel locations.

Ethernet Media Converter Types

Ethernet media converter typically has three categories, including standalone media converters, DIN Rail Mount industrial media converters and chassis-based media converters. Standalone converters, or fiber optic to Ethernet converters, are often used when only one or two conversions are needed. Industrial media converters are suitable to be used in large manufacturing plants with harsh conditions and limited space, while chassis-based media converters are used in large MDF (main distribution frame) locations where multiple fiber links need to be converted to UTP.

Standalone Media Converters

Standalone media converters, or fiber optic to Ethernet converters, turn an Ethernet connection into fiber cabling, supporting ultra-fast long distance connections. Besides extending the network connection distance, it can also save you costs and space due to its standalone feature. On one hand, it provides high quality conversion on a unit-by-unit basis instead of buying an entire chassis. On the other hand, the compact configuration can fit anywhere leading no wasted space and doesn’t need an entire rack. It’s suitable for applications in limited space environments such as telecommunication cabinets or a distribution box. The small size is convenient for installation. And plug & play design makes the converters easy to operate.

fiber optic to Ethernet converters

Industrial Media Converters

Industrial media converters are specially designed for harsh environment applications. They can convert copper to fiber, single-mode to multimode, multimode to multimode. They are ideal for extending the distance of copper devices such as IP cameras and wireless access points found in traffic management, oil and gas pipelines, weather tracking, industrial and outdoor applications. FS.com offers a full range of industrial media converters which are available in single-mode dual fiber, multimode dual fiber and single-mode single fiber. They feature small power consumption, low heat, high reliability and good stability.

Chassis-based Media Converters

Chassis-based media converters include a number of independent media converters and a chassis capable of housing up to 16 media converters. This kind of media converter convert signals transmission from one type of cable to another type of cable. Therefore, it can reach longer signal transmission distances between devices designed for short distance cables like Cat 5 twisted pair cables. All media converters in the system have own solid metal case housing, LED status indicators and AC to DC power adapters. They can be used as standalone converters, or installed in the chassis. When you need more room, you can install them in a chassis. Before installation, first you need to remove their metal cases and slide their PC boards into the chassis slots. At that situation, the power supply will come from the chassis instead of each standalone converter. All media converters are hot swappable when used with the chassis. As for this type of media converters, there are managed or unmanaged options.

Chassis-based Media Converters

The managed module is available for installation in the chassis. It’s helpful to monitor the real-time status of all media converters and power supplies in the chassis and send out information about all abnormal situations. Management follows industry standards, including SNMP (simple network management protocol) and HTTP, which allows you to monitor and manage media converters and power supplies from a third-party SNMP management workstation or via a web browser.

The unmanaged or “plug & play” Ethernet media converter is easy for installation and troubleshooting. However, it’s difficult to discover the problem once there is a network issue. So if you select this solution, you can use an SNMP card showing statistics and whole conditions of all media converters in the chassis. This is useful when many chassis are filled with Ethernet media converters in a large data center.

How to Use an Ethernet Media Converter?

Ethernet media converter usually has two types of ports. One is for the copper side (often an RJ45 jack) and the other is for the fiber side (the port can be SC, ST, LC, etc). If you have bought the media converter that you need, you simply plug your copper network cable into the RJ45 jack and then make your connection to your fiber optic cabling. For most unmanaged Ethernet media converters, you are done with your installation once you power up the unit.

Conclusion

Ethernet media converters enable seamless integration of different network cabling for Ethernet networks. They support 10Mbps, 10/100Mbps, 100Mbps, 10/100/1000Mbps, Gigabit and 10 Gigabit. FS also offers solutions that cater to various needs: from short-range connectivity at 220m to wide-area networking up to 120km. Choose from options that include 220m, 550m, ≤1km, ≤10km, ≤20km, and ≤40km to ensure your network is connected over the exact distance you require. Check out FS Ethernet Media Converter and explore a diverse range of fiber networking solutions at FS.com for all your connectivity needs.

You might be interested in

Knowledge
Knowledge
See profile for Margaret.
Margaret
What Is Media Converter and How to Choose It?
Dec 17, 2021
25.5k
Knowledge
Knowledge
See profile for Irving.
Irving
What Are FEF and LFP on Media Converter
Dec 7, 2023
26.7k
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge