English

6 Best Ways to Extend Wi-Fi Range in Your Home and Office

Updated on Feb 20, 2023 by
41.4k

It is incredibly frustrating but really common when encountering wireless connection problems in home, office or factory, such as experiencing poor WiFi during VoIP video conferences. There are many reasons why you get a poor WiFi connection: dead zone, signal interference, obsolete network device, speed limit, WiFi squatter, ect. This article gives you some ways to extend your wireless network signal and increase the wifi range for a better experience. Check out 6 ways to boost your wireless signal, extend your Wi-Fi range, and speed up your connection.

Find a Better Place for Your Router or Wireless access point

No matter for home or office use, the fundamental thing is to keep the range that routers or wireless APs can handle as large as possible. The farther you get from your router's antenna, the weaker the signal. As you may know, the WiFi signal is affected by all kinds of interference, including walls, furniture, electronic appliances, and other wireless devices. If you go from 1 to 2 meters away from the router, the signal is only a quarter as strong, and at three meters it's only ninth as strong. You should strive for a central location that is free from physical obstructions like walls and doors if possible. Don’t keep your router in a closet or a desk drawer if you hope to realize its true potential signals range.

Place the Routers or Wirelss APs in the Right Place

Install a WiFi Extender or Repeater

If you have placed the wireless router or access point at the centralized location but there are still corners out of range, WiFi extender or WiFi repeater is an easy and cheap way to extend WiFi range by adding additional hardware without having to run cables. Although they are named differently, the function of them is almost the same—to take in an existing wireless signal, repeat it, and forward it to the dead zones of the location. See the differences between Wireless AP vs Range Extender if you're having basic problem with these two things.

Set Up Wi-Fi Extenders/Repeaters

While WiFi range extender will work, they are not without their complexities and limitations. The WiFi extenders actually only extend WiFi range, instead of your WiFi signals. Thus, there is no such thing as business-grade extenders because they only support a limited number of devices at a time and the WiFi signal can get weaker when devices are connected simultaneously. Besides, old routers also can be configured into an extender if the router can use open-source firmware.

Upgrade Your Router’s Firmware or Wireless Device

Keeping your device’s firmware current can help you obtain the best WiFi signal that the router can provide. Many Wi-Fi router manufacturers release firmware updates that can help improve your router’s performance. Updating your router’s firmware may also have additional Wi-Fi enhancements, such as security improvements and new features.

Your WiFi network speed can also be influenced by the age of your wireless device: what WiFi standards it supports, as well as how good its processor and antennas are. The latest WiFi 6 technology can offer a 30% faster speed than WiFi 5, WiFi 6-supported devices can theoretically hit 9.6 Gbps. Thereinto, the enhanced WiFi 6 MU-MIMO technology increases 4x capacity for more simultaneous connections, especially in enterprise campus networks. If you're running obsolete hardware, you can't expect the best performance. We have a tendency to upgrade your wireless devices.

Upgrade with Wi-Fi 6 AP

Switch to 5GHz Band

Dual-band technology gradually becomes common for routers or access points because it can broadcast 2.4GHz and 5GHz signals together, supporting a greater range of devices and higher signal by separating network traffic between devices with different bandwidth. When network congestion appears on 2.4GHz, dual-band WiFi access points make it possible to seamlessly switch the 2.4GHz end-users to 5GHz, which reduces the network traffic load and extends wireless network signals. Because it will incur less interference from other electronic devices since the frequency is used less often.

Switch to 5GHz Band

Note:

  • 5GHz band tends to be less congested than 2.4GHz because it offers more channels for devices to use.

  • 2.4 GHz band can be subject to interference from devices like cordless phones, microwaves and other WiFi-supported devices. As a result, the RF interference can impact the 2.4GHz band used by WiFi, effectively slow down the link, and lead to reduced signal strength.

  • 5GHz has a smaller range than 2.4GHz and doesn't penetrate solid objects like walls. The most effective strategy is to use 2.4GHz for basic WiFi applications, and then use 5GHz for high bandwidth applications.

Get a Better Antenna

One of the best ways to extend Wi-Fi range is to add an antenna to your router. If you have a router with a replaceable external antenna, you can easily improve its performance by getting a better one. To figure out if your router supports external antennas, read through your router’s manual. In many cases, the router manufacturer will sell external antennas separately. To reinforce a particular area of signal weakness, you can point a directional antenna toward it, but you need to keep in mind that other directions may suffer. That said, most router antennas tend to be omnidirectional.

Create a Wireless Mesh Network

A wireless mesh network is often seen as the upgrade version of WDS. In a mesh network system, there are dozens or hundreds of routers or access points spread out and act as individual nodes. All the nodes communicate with each other to extend the wireless signals and extend WiFi range.

Different from a WDS system where a WiFi access point is only connected to another access point wirelessly, mesh nodes support multiple wireless hops before connecting to a node that is wired into the network. Each mesh node can reach another node going through multiple hops and leveraging other nodes as repeaters.

The major advantage of a wireless mesh network is intrinsic redundancy and reliability because a mesh network is able to reroute traffic through multiple paths to cope with link failures, interference, power failures or network device failures.

Create a Wireless Mesh Network

Note: When one mesh node reaches another one, the throughput can be cut in half. To avoid such cases, it is feasible to add more nodes to the network backbone and also place the node access points in optimum spots.

FAQs about How to Extend Wi-Fi Range

How far can I extend my Wi-Fi range?

Some Wi-Fi range extenders may allow you to boost your home Wi-Fi up to 2,500 feet. Please note that this isn’t a hard-and-fast range, as it can vary based on your environment and the strength of your Wi-Fi extending device.

Can I extend WiFi range with another router?

Yes, you can extend the range of your WiFi with another router, either by connecting the two routers together using an Ethernet cable or by setting up the new router to function as a Wi-Fi range extender.

What can I use to extend my Wi-Fi signal?

To extend your Wi-Fi signal, you can use a Wi-Fi extender and a mesh Wi-Fi network

What is the difference between a Wi-Fi extender and booster?

In most cases, Wi-Fi extenders and boosters are the same thing. There isn’t a clearly defined difference between an extender and a booster — both are devices designed to improve Wi-Fi coverage. It mainly depends on what the manufacturer decides to call their device.

 

Related articles:

Benefits of Using Wireless APs for WiFi Tracking

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.7k