FHD Rack Mount Enclosure Solution
As the demand for computing power grows rapidly, it’s vital for data center operators to look for the high-density equipment that can offer higher performance without needing to expand into a larger physical space. Fiber enclosure, or fiber splice box, as a necessary fiber cable management component, is widely used in data centers to house, organize, manage and protect fiber optic cables. Simultaneously, these fiber optic enclosures come in different configurations such as rack mount, wall mount enclosure, and indoor or outdoor enclosure. Among these different configurations, rack mount fiber enclosure is the most commonly used in data centers.
What Is Rack Mount Fiber Enclosure?
The rack mount fiber enclosure is made for 19-inch rack mounting and comes in rack units of 1U, 2U, 4U, or more rack units depending on the number of connections required. It also comes in two flavors: slide-out type and cover removable type. The slide-out type is more expensive than cover removable type, but it is more convenient for high-density cabling deployment. The slide-out rack mount fiber enclosure features the pull-out sliding trays, so it does not require the user to remove the whole fiber enclosure from the rack to gain internal access. The following sections will introduce FS.com FHD rack mount fiber enclosure. If you are interested in how to select the rack mount fiber enclosure, please refer to Which Type of Rack Mount Fiber Enclosures Should You Choose?
FHD Rack Mount Fiber Enclosure
FS.com provides a comprehensive line of FHD high-density fiber optic enclosures, including 1U, 2U, and 4U types. The 1U fiber enclosure allows for 4 x FHD fiber adapter panels or 4 x FHD MPO/MTP cassettes up to 96 fibers. The 2U rack mount fiber enclosure can support 8 x FHD fiber adapter panels or 8 x FHD MPO/MTP cassettes up to 192 fibers. And the 4U rack mount fiber enclosure can support either 12 x FHD fiber adapter panels or 12 x FHD MPO/MTP cassettes up to 228 fibers. By the way, the FHD fiber enclosures have the traditional cover removable type and slide-out type for options. The new generation of rack enclosure is upgraded in door latch and slide rail, so that the new-design parallel sliding drawer keeps to pull and push easier and more convenient. More importantly, FHD series fiber optic enclosures provide the versatility and flexibility with a fully modular solution for a variety of fiber optic patching, terminating and splicing applications. The fiber splice tray and fiber slack management spool can be installed into the FHD fiber enclosure for storage of spliced fiber pigtails or managing the excess fiber cable slack. The 1U fiber enclosure can hold up to four fiber splice tray. The video below will show the basic installments and remove of these enclosure accessories inside the FHD cover removable rack enclosure.
Enclosure Accessories Used in FHD Fiber Enclosure
FS.com also offers a wide selection of fiber enclosure accessories for cable management. The fiber splice tray and fiber slack management spool are the most popular enclosure accessories used in FHD rack mount fiber enclosure.
Item | Description | Illustration |
---|---|---|
FHD Fiber Splice Tray | Designed to safely route and store optical fibers. | |
FHD Fiber Slack Management Spool | Effectively manage the excess fiber cable slack. |
Conclusion
The FHD rack mount fiber enclosure solutions meet the demand for high-density cabling and seamless migration to 40G and 100G. This high-density system enables data center technicians to quickly and safely complete the moves, adds and changes (MACs) while simultaneously providing the scalability to optimize cable management in places where maximum density is required. All in all, FHD fiber enclosures provide the perfect solutions for easy-to-manage cabling environments and strong protection of fiber optic cables.
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023