English

Fiber Optic Solutions for Cisco C3KX-NM-10G Module

Updated on Apr 11, 2018 by
7.6k

SFP stands for “Small Form-factor Pluggable”. SFP transceiver is used for Fast Ethernet applications. Switch with a Cisco C3KX-NM-1G module can support SFP. But with the increasing needs for higher data rates, 1 Gbps speed is not enough. Thus, SFP+ (Small Form-factor Pluggable Plus) is created as an expansion of SFP to support data rates up to 10 Gbps or even higher over fiber. Accordingly, switch with a Cisco C3KX-NM-10G module (shown as the following picture) is produced to support both SFP and SFP+ transceivers.

FS Test Assured Program

C3KX-NM-10G Overview

C3KX-NM-10G module fits most Cisco Catalyst 3650-X and 3750-X switches. So you can just upgrade modules instead of replacing them when you need higher transmission speeds. Besides, it’s easy to be configured so that network designers can mix and match the type of transceivers with their own port module preferences. C3KX-NM-10G module has two installation screws on each side, which make it easy to switch things out and make new connection without a fuss.

C3KX-NM-10G module has four slots, including two SFP+ slots and two SFP mini-GBIC slots. The four slots are grouped as two pairs, with each pair consisting of one SFP slot and one SFP+ slot. Each pair supports two 1-Gigabit SFP modules or one 10-Gigabit SFP+ module. That is to say, a 10-Gigabit SFP+ module and 1-Gigabit SFP module cannot operate in a pair at the same time.

C3KX-NM-10G

Supported Combinations of SFP and SFP+ Modules

Combination Method Slots Transceiver Modules
Method 1 Slots 1, 2, 3, and 4 Four 1-Gigabit SFP modules
Method 2 Slots 1 and 2 Two 1-Gigabit SFP modules
Slot 4 One 10-Gigabit SFP+ module
Method 3 Slot 2 One 10-Gigabit SFP+ module
Slots 3 and 4 Two 1-Gigabit SFP modules
Method 4 Slot 2 One 10-Gigabit SFP+ module
Slot 4 One 10-Gigabit SFP+ module

Usually a 10-Gigabit SFP+ module takes precedence over a 1-Gigabit SFP module. But it’s another case when an SFP module is first inserted in Slot 1 and has link. For example, if the SFP in Slot 1 retains link, you insert an SFP+ module in Slot 2 and the SFP+ module in Slot 2 does not operate. If the SFP module in Slot 1 is shut down or removed, the SFP+ module in Slot 2 turns on. The SFP module in Slot 1 does not work as long as an SFP+ module is in Slot 2, whether it has link up or not.

Fiber Optic Solutions for C3KX-NM-10G Module

C3KX-NM-10G module provides 1 Gigabit Ethernet and 10 Gigabit Ethernet data links. It supports 1 Gigabit Ethernet transceiver and 10 Gigabit Ethernet transceivers. The following tables show all SFP and SPP+ transceiver modules for C3KX-NM-10G module.

1 Gigabit Ethernet Transceivers for C3KX-NM-10G Module

Modules Description Cable & Connector
GLC-T 1000BASE-T SFP Transceiver, 100m Cat 5, RJ-45
GLC-SX-MM 1000BASE-SX SFP Transceiver, 550m SMF, LC Duplex
GLC-LH-SM 1000BASE-LX/LH SFP Transceiver, 550m/10km MMF/SMF, LC Duplex
GLC-SX-MMD 1000BASE-SX SFP Transceiver, 550m, DOM MMF, LC Duplex
GLC-LH-SMD 1000BASE-LX/LH SFP Transceiver, 550m/10km, DOM MMF/SMF, LC Duplex
GLC-ZX-SM 1000BASE-ZX SFP Transceiver, 70km SMF, LC Duplex
GLC-ZX-SMD 1000BASE-ZX SFP Transceiver, 70km, DOM SMF, LC Duplex
GLC-BX-D 1000BASE-BX-D SFP Transceiver, 10km, DOM SMF, LC Simplex
GLC-BX-U 1000BASE-BX-U SFP Transceiver, 10km, DOM SMF, LC Simplex
SFP-GE-S 1000BASE-SX SFP Transceiver, 550m, DOM MMF, LC Duplex
SFP-GE-L 1000BASE-LX/LH SFP Transceiver, 10km, DOM SMF, LC Duplex
SFP-GE-Z 1000BASE-ZX SFP Transceiver, 70km, DOM SMF, LC Duplex
GLC-EX-SMD 1000BASE-EX SFP Transceiver, 40km, DOM SMF, LC Duplex

10 Gigabit Ethernet Transceivers for C3KX-NM-10G Module

Modules Description Cable & Connector
SFP-10G-SR 10GBASE-SR SFP+ Transceiver, 300m, DOM MMF, LC Duplex
SFP-10G-LRM 10GBASE-LRM SFP+ Transceiver, 220m, DOM MMF, LC Duplex
SFP-10G-LR 10GBASE-SR SFP+ Transceiver, 300m, DOM MMF, LC Duplex
SFP-10G-SR-S 10GBASE-SR SFP+ Transceiver, 300m, DOM MMF, LC Duplex
SFP-10G-LR-S 10GBASE-LR SFP+ Transceiver, 10km, DOM SMF, LC Duplex
SFP-10G-ER 10GBASE-ER SFP+ Transceiver, 40km, DOM SMF, LC Duplex
SFP-10G-ER-S 10GBASE-ER SFP+ Transceiver, 40km, DOM SMF, LC Duplex
SFP-10G-ZR 10GBASE-ZR/ZW SFP+ Transceiver, 80km, DOM SMF, LC Duplex
SFP-10G-ZR-S 10GBASE-ZR SFP+ Transceiver, 80km, DOM SMF, LC Duplex
SFP-H10GB-CU50CM 10G SFP+ DAC Twinax Cable, 0.5m Passive Copper Cable, SFP+ to SFP+
SFP-H10GB-CU1M 10G SFP+ DAC Twinax Cable, 1m Passive Copper Cable, SFP+ to SFP+
SFP-H10GB-CU3M 10G SFP+ DAC Twinax Cable, 3m Passive Copper Cable, SFP+ to SFP+
SFP-H10GB-CU5M 10G SFP+ DAC Twinax Cable, 5m Passive Copper Cable, SFP+ to SFP+
SFP-H10GB-CU1-5M 10G SFP+ DAC Twinax Cable, 1.5m Passive Copper Cable, SFP+ to SFP+
SFP-H10GB-CU2M 10G SFP+ DAC Twinax Cable, 2m Passive Copper Cable, SFP+ to SFP+
SFP-H10GB-CU2-5M 10G SFP+ DAC Twinax Cable, 2.5m Passive Copper Cable, SFP+ to SFP+
SFP-H10GB-ACU7M 10G SFP+ DAC Twinax Cable, 7m, 10m Active Copper Cable, SFP+ to SFP+
SFP-H10GB-ACU10M 10G SFP+ DAC Twinax Cable, 10m Active Copper Cable, SFP+ to SFP+
SFP-10G-AOC1M 10G SFP+ AOC, 1m Active Optical Cable, SFP+ to SFP+
SFP-10G-AOC2M 10G SFP+ AOC, 2m Active Optical Cable, SFP+ to SFP+
SFP-10G-AOC3M 10G SFP+ AOC, 3m Active Optical Cable, SFP+ to SFP+
SFP-10G-AOC5M 10G SFP+ AOC, 5m Active Optical Cable, SFP+ to SFP+
SFP-10G-AOC7M 10G SFP+ AOC, 7m Active Optical Cable, SFP+ to SFP+
SFP-10G-AOC10M 10G SFP+ AOC, 10m Active Optical Cable, SFP+ to SFP+

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.7k