English

Comprehensive Introduction of Fiber Optic Splitter

Updated on Mar 15, 2023 by
21.2k

FS PLC Fiber Optic Splitter

Fiber optic splitter contains multiple input and output ends. Whenever the light transmission in a network needs to be divided, fiber optic splitter can be implemented for the convenience of network interconnections. This article will help you to gain more knowledge of fiber splitter manufacturing, fiber splitter test, and fiber splitter applications.

How to Manufacture a Fiber Optic Splitter?

In all, there are five steps to manufacture a fiber optic splitter. Each step requires strict control and management of various parameters like environment, temperature, and detailed precision on assembly and equipment.

Step One: Components Preparation

Generally three components are needed. The PLC circuit chip is embedded on a piece of glass wafer, and each end of the glass wafer is polished to ensure highly precise flat surface and high purity. The v-grooves are then grinded onto a glass substrate. A single fiber or multiple ribbon fiber is assembled onto the glass substrate. This assembly is then polished.

Step Two: Alignment

After the preparation of the three components, they are set onto an aligner stage. The input and output fiber array is set on a goniometer stage to align with the PLC chip. Physical alignment between the fiber arrays and the chip is monitored through a continuous power level output from the fiber array.

Step Three: Cure

The assembly is then placed in a UV (ultraviolet) chamber where it will be fully cured at a controlled temperature.

Step Four: Packaging

The bare splitter is aligned and assembled into a metal housing where fiber boots are set on both ends of the assembly. And then a temperature cycling test is needed to ensure the final product condition.

Step Five: Optical Testing

In terms of testing, three important parameters such as insertion loss, uniformity and polarization dependent loss (PDL) are performed on the splitter to ensure compliance to the optical parameters of the manufactured splitter in accordance with the GR-1209 CORE specification.

 

How to Test the Quality of Fiber Optic Splitter?

The quality of a fiber optic splitter is mainly determined by five specifications, namely optical bandpass, insertion loss, return loss, uniformity, and directivity. The following part outlines how to test each specification.

  • The optical bandpass can be tested by connecting the optical splitter to an optical spectrum analyzer with a high-powered light source having a central wavelength of the required bandpass. The attenuation across the required bandpass shall meet the splitter requirements.

  • The insertion loss is tested by using a light source and power meter. The reference power level is obtained and each output port of the optical splitter is measured.

  • The return loss is tested by using a return loss meter. The input port of the splitter is connected to the return loss meter and all the output ports are connected to a non-reflective index matching gel.

  • The uniformity of the optical splitter can be determined by referring to the results from the insertion loss test to ensure that the difference between the highest loss and the lowest loss is within the acceptable uniformity value.

  • Directivity can be measured in a manner similar to the insertion loss test. However, the light source and power meter are connected to each of the input ports and two output ports.

 

How to Apply Fiber Optic Splitters In PON System?

Fiber optic splitters, enabling the signal on the optical fiber to be distributed between two or more optical fibers with different separation configurations (1×N or M×N), have been widely used in PON networks. FTTH is one of the common application scenarios. A typical FTTH architecture is: Optical Line Terminal (OLT) located in the central office; Optical Network Unit (ONU) situated at the user end; Optical Distribution Network (ODN) settled between the previous two. An optical splitter is often used in the ODN to help multiple end-users share a PON interface.

Fiber Optic Splitter Application in PON

Figure 1: Fiber Optic Splitter Application in PON

Point-to-multipoint FTTH network deployment can be further divided into the centralized (single-stage) or cascaded (multi-stage) splitter configurations in the distribution portion of the FTTH network. The centralized splitter uses single-stage splitter located in a central office in a star topology. The cascading splitter approach uses multi-layer fiber splitters in a point to multi-point topology.

Fiber Optic Splitter In Centralized PON Architecture

The centralized architecture generally uses 1×32 splitters in the central office located anywhere in the network. The splitter input port is directly connected via a single fiber to a GPON/GEPON optical line terminal (OLT) in the central office. On the other side of the splitter, 32 fibers are routed through distribution panels, splice ports and/or access point connectors to 32 customers’ homes, where it is connected to an optical network terminal (ONT). Thus, the PON network connects one OLT port to 32 ONTs.

Fiber optic splitter in centralized PON architecture

Figure 2: Fiber optic splitter in centralized PON architecture

Fiber Optic Splitter In Cascaded PON Architecture

A cascaded architecture may use a 1×4/1×8 fiber splitter residing in an outside plant enclosure/terminal box. This is directly connected to an OLT port in the central office. Each of the four fibers leaving this stage 1 splitter is routed to an access terminal that houses a 1×8/1×4, stage 2 splitter. In this scenario, there would be a total of 32 fibers (4×8) reaching 32 homes. It is possible to have more than two splitting stages in a cascaded system, and the overall split ratio may vary (1×16 = 4 x 4, 1×32 = 4 x 8, 1×64 = 4 x 16, 1×64 = 8 x 8).

Figure 3: Fiber optic splitter in cascaded PON architecture

 

Conclusion

Fiber optic splitters enable a signal on an optical fiber to be distributed among two or more fibers. Since fiber splitters contain no electronics nor require power, they are an integral component and widely used in most fiber optic networks. Thus, choosing fiber optic splitters to help increase the efficient use of optical infrastructure is key to developing a network architecture that will last well into the future. To know how to choose suitable optical splitters, please read this article: What Is an Optical Splitter? 

You might be interested in

Knowledge
See profile for John.
John
How Much Do You Know About PLC Splitter?
Mar 26, 2024
33.8k
Knowledge
Knowledge
Knowledge
See profile for John.
John
What Is an Optical Splitter?
Mar 15, 2023
101.8k
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k