English

Fibre Channel vs Ethernet Transceiver, What Are Their Differences?

Updated on Oct 7, 2021 by
19.6k

For Fibre Channel infrastructures, FC transceivers are considered as one of the indispensable components, while Ethernet transceivers plus Ethernet switches are the common matched combination when deploying the Ethernet network. Obviously, these two types of transceivers are used for different applications, but what on earth their differences are? This article will make a comparison between Fibre Channel vs Ethernet transceiver.

What Is Fibre Channel Transceiver?

As a high-speed data transfer protocol, Fibre Channel (FC) can provide in-order, lossless delivery of raw block data. It is primarily used for transmitting data among data centers, computer servers, switches and storage.

Fibre Channel transceivers, accord with Fibre Channel Protocol (FCP), function as the interface between Fibre Channel systems, as well as the interface between optical storage network devices. They are mainly used for Fibre Channel storage network links in data centers. Featuring with miniaturization and low power consumption, FC modules can satisfy the need for faster transfers of larger volumes of information in a lossless way. The Fibre Channel transceivers are basically running at the Fibre Channel speed range from 1Gbps to 128Gbps, with 256Gbps and 512Gbps in the road map. Their common form factors are SFP, SFP+, SFP28, SFP56, and QSFP28.

FC 8G transceiver.jpg

Figure 1: FS FC 8G transceiver


What Is Ethernet Transceiver?

Ethernet, also standardized as IEEE 802.3, refers to a computer networking technology widely used in local area networks (LANs) with good backward compatibility, higher bandwidth, and longer link distances, which is increasingly replacing the previous wired LAN technologies like Token Ring, FDDI, and ARCNET.

Ethernet transceivers are fiber optics that follow the Ethernet protocols to link hardware devices within a network by transmitting and receiving messages mainly for LAN situations. The frequently-used form factors are 1G SFP, 10G SFP+, 25G SFP28, 40G QSFP+, 50G QSFP28, 100G QSFP28, 400G QSFP-DD, and the corresponding transmission speed of Ethernet transceivers are ranging from 1G to 400G. The aforementioned models not only include some regular types of optical transceivers but also cover a wide range of WDM transceivers and BiDi transceivers.

Ethernet 10G-SR transceiver.jpg

Figure 2: FS Ethernet 10G-SR transceiver

Fibre Channel vs Ethernet Transceiver, What Are Their Differences?

Protocols & Security

FC transceivers that belong to Fibre Channel Protocol do not follow the OSI model layering. While Ethernet transceivers are compliant with IEEE 802.3, which will realize packet-based physical communication in a LAN. It's a data-link layer protocol in the TCP/IP stack and belongs to the OSI model.

Fibre Channel is a natural security system. Storage Area Network (SAN) is isolated from the outside world, the risk of storage network attack and data leakage will be reduced. As a result, adopting FC modules in storage networks is much safer. The TCP/IP protocol that Ethernet modules run will make the whole system vulnerable to more frequent attacks on account of the intervening of back-end administration is done over the network.

Reliability

Influenced by their protocols, the difference in transmission modes will cause diversity in transmission results. The compelling advantage of Fibre Channel over Ethernet is its better reliability. The lossless nature of FC has provided excellent performance in storage networking for a long time. That is to say, Fibre Channel modules can provide in-order and lossless delivery of raw block data while Ethernet modules can't.

Besides, Fibre Channel follows SAN system, whereas Ethernet is used generally by NAS (Network-Attached Storage) systems. FC modules are designed for the users that need fast, low latency reliability for block storage. If file-level storage access is required, then Ethernet modules will be considered.

Transmission Speed

As mentioned in the introduction part, Fibre Channel and Ethernet transceivers' transmission speed range is different. Specifically speaking, FC modules can run at 1Gbps / 2Gbps / 8Gbps / 16Gbps / 32Gbps / 128Gbps at present. Ethernet modules can support a wider range of transmission speeds, including 10Mbps / 100Mbps / 1000Mbps and 10Gbps / 25Gbps / 50Gbps / 40Gbps / 100Gbps / 400Gbps.

Furthermore, the FC module's generational speed improvements normally occur in powers of two, from 1Gbps to 32Gbps respectively. The generational throughput improvements of Ethernet modules far outpace Fibre Channel ones. The new-launched 400G Ethernet QSFP-DD modules are nearly 400 times the initial 1G SFP modules. Obviously, Ethernet fiber optic transceivers are more suitable for the increasing need for higher bandwidth.

Applications

The difference between Fibre Channel vs Ethernet transceivers also lies in their applications. Fibre Channel is one of the best ways to transfer large amounts of data between servers and storage devices. Thus, FC modules that connect to FC switches are mostly used in Fibre Channel, storage networking and Ethernet applications. Fibre Channel communications can run directly over Ethernet in the form of Fibre Channel over Ethernet (FCoE). Evidently, the working scenarios of FC transceivers have been applied in large enterprises and data centers.

As an architecture developed almost four decades for LANs, the Ethernet transceivers are generally applied in LAN situation, sometimes with Wide Area Network (WAN) applications. Compared with the working scenarios of FC modules, the Ethernet modules can be seen in various situations from small-sized offices to hyper-scale data centers based on the requirement of the bandwidth.

Matched Switches

The stable connection between transceivers and switches is vital when realizing the abovementioned application scenarios. Normally speaking, FC modules are connected to FC switches, whereas Ethernet modules and Ethernet switches are matched. No mixed usage situations.

As one of the leading choices for SANs, the traditional Fibre Channel networks contain Fibre Channel switches and Fibre Channel HBAs. FC switches are used to connect the storage to the SAN, while the FC HBAs are applied to connect the switches to servers. The variant of Ethernet network switches is wider, which reflects in the stackability, the ports number, the transfer rates that support, etc. When the latest 400G Ethernet fiber optic transceivers are connecting to a 400G network switch, 400GbE will be realized then. Fibre Channel vs Ethernet Switch: What Are the Differences illustrates the differences between these two types of switches.

Summary

Fibre Channel is deeply entrenched in today's big enterprises and large data centers, which makes FC transceivers significant. Ethernet shows its edge for the ability to run multiple storage and networking protocols, which leads to the wide usage of Ethernet network transceivers. Both Fibre Channel transceivers and Ethernet transceivers have their relatively fixed users for their specific networking deployment.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.9k