English

FS 40/100G QSFP28 SWDM4 Optical Transceiver Overview

Posted on Mar 15, 2024 by
182

In the fast-paced world of networking, the demand for high-speed connectivity continues to surge. Enter the 40/100G SWDM4 module, a game-changing solution that combines dual-rate compatibility with the efficiency of Short Wavelength Division Multiplexing (SWDM) technology. This compact yet powerful module offers a wealth of benefits, from increased bandwidth capacity to cost-effective infrastructure upgrades.

What is FS 40/100G SWDM4 Module?

The FS 40/100G SWDM4 dual-rate module is a specialized type of optical transceiver module designed to support both 40 Gigabit Ethernet (40GBASE) and 100 Gigabit Ethernet (100GBASE) transmission rates using Short Wavelength Division Multiplexing (SWDM) technology. This dual-rate module is capable of transmitting and receiving data over four wavelengths (hence the "4" in SWDM4) within the short wavelength range, typically using multimode fiber (MMF) infrastructure. It allows for the simultaneous transmission of multiple data streams, effectively increasing the overall bandwidth capacity of the optical link. The working principle is as follows:

40/100G SWDM4

FS QSFP28 40/100G SWDM4 Specification

Data Rate 40 Gbps 100 Gbps
Form Type QSFP28
Wavelength 850nm
Connector Duplex LC
Cable Type MMF
Max Cable Distance OM3: 240m

OM4: 350m

OM5: 440m

OM3: 75m

OM4: 100m

OM5: 150m

TX Power -7.5~3 dBm -7.5~2 dBm
Receiver Sensitivity L0: -12.9dBm

L1: -12.5dBm

L2: -12.2dBm

L3: -11.9dBm

L0: -9.5dBm

L1: -9.4dBm

L2: -9.4dBm

L3: -9.4dBm

Powerbudget 2dB 1.9dB
Receiver Overload 2.4 dBm 3.4 dBm
Power Consumption ≤3.5W
Extinction Ratio >2 dB
DDM/DOM Supported
Commercial Temperature Range 0℃ to 70℃ (32 to 158°F)
Protocols SWDM MSA, QSFP28 MSA, IEEE802.3bm CAUI-4

What are the Advantages of FS 40/100G SWDM4 Module?

In the realm of network infrastructure, the adaptability and versatility of FS 40/100G SWDM4 Module play a pivotal role in meeting the evolving demands of modern connectivity. Here are some of its advantages:

Dual-rate Compatibility: The module supports both 40 Gigabit Ethernet (40GBASE) and 100 Gigabit Ethernet (100GBASE) transmission rates, providing versatility and future-proofing for network upgrades.

Increased Bandwidth: SWDM technology enables the transmission of multiple data streams over a single optical fiber, effectively increasing the bandwidth capacity of the link compared to traditional single-wavelength solutions.

Utilization of Existing Infrastructure: SWDM4 modules can leverage existing multimode fiber (MMF) infrastructure, allowing for cost-effective upgrades in environments where MMF is already deployed.

Reduced Fiber Requirements: By transmitting multiple data streams over a single fiber, SWDM4 modules help reduce the number of fibers needed for high-speed connections, optimizing space and simplifying cable management.

Compatibility with QSFP28 Form Factor: SWDM4 modules typically use the QSFP28 form factor, which is widely adopted in data centers and enterprise networking equipment, ensuring compatibility with existing hardware and infrastructure.

Interoperability: SWDM4 modules are designed to be interoperable with other SWDM-enabled devices, facilitating seamless integration into existing networks and interoperability with future SWDM-based solutions.

Cost-effectiveness: The ability to support multiple transmission rates and utilize existing fiber infrastructure helps reduce deployment costs and total cost of ownership, making SWDM4 modules a cost-effective solution for high-speed networking.

How to Upgrade the Rate of FS 40/100G SWDM4 Modules?

When using a dual-rate 40/100G module in a 40/100G switch port (depicted by the green box on the left), it's still compatible with a native 40G module plugged into an older switch featuring a single-rate 40G port (illustrated by the orange box on the right). To ensure compatibility, the dual-rate port on the left is configured to operate at 40G mode within the switch software (as indicated by the red outline in the diagram).

When you're ready to upgrade the other end of the connection, simply replace the 40G switch with a new one supporting 100G QSFP28 ports, such as N5860-48SC. Insert the new 40/100G module and configure the switch software on both ends to run the port at 100G. With these steps completed, the upgrade is successfully executed.

40/100G SWDM4

Conclusion

In summary, the FS 40/100G SWDM4 module stands as a versatile and cost-effective solution for modern networking challenges. With its dual-rate compatibility, enhanced bandwidth capacity, and seamless integration capabilities, it offers unprecedented flexibility and efficiency in high-speed connectivity. As networks continue to evolve, this innovative module promises to play a pivotal role in driving performance and scalability across various industries and applications.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.7k