English

How to Choose the Right Cat6a Cable for Your 10G Networks?

Updated on Mar 20, 2021 by
46.3k

The dramatic growth in data center throughput has led to the increasing usage and demand for the 10G network. Cat6a cabling solution is designed for high-performance 10GbE and above. Category 6a cable, aka Cat6a cable, is currently the preferred Ethernet cable to meet and exceed the requirements for the 10GBASE-T applications. Various Cat6a network cable types like UTP vs SFTP may confuse you, and what other factors should be taken into considerations when selecting Cat6a Ethernet cables? This article may inspire you for your Cat6a cable selection.

Cat6a Cabling

Cat6a Cable Types for 10GBase-T: UTP vs F/UTP vs SFTP

Category 6a patch cable has been extensively tested and proven to support 10GBASE-T networks. There are many types of Cat6a cables that are added to different protection materials. Three major Cat6a cable types are: Unshielded Twisted Pair (UTP), Shielded Twisted or Foiled Twisted Pair (S/UTP or F/UTP), and Shielded and Foiled Twisted Pair (SFTP). The table below further shows these three different types of copper Ethernet cables—UTP vs F/UTP vs SFTP:

UTP S/UTP or F/UTP SFTP
UTP-cat6a-cable FUTP-cat6a-cable STFP-cat6a-cable
Unshielded Twisted Pair Shielded Twisted or Foiled Twisted Pair Shielded and Foiled Twisted Pair
UTP cable features pairs of twisted pairs of wires and each of them is individually shielded using a metal foil, increasing the outer diameter of the cable. S/UTP and F/UTP cable feature unshielded pairs that are shielded by a single metal foil, helping keep out electrical noise from interfering. As the combination of S/UTP and F/UTP, SFTP cable owns foil shielding around the individual twisted wires, providing the highest protection level from interference.

With features like extra internal airspace between the twisted pairs, Cat6a UTP cable can minimize crosstalk and ANEXT in 10GBASE-T networks. But the effects of ANEXT are not eliminated. Therefore, ANEXT measurement is essential for Cat6a UTP cable, which is complex and time-consuming.

Cat6a S/UTP or F/UTP cable is better than UTP cable to some degree. The foil shield acts as a barrier reflecting the noise from machinery, lights, motors, and other sources of EMI and RFI. And the foil shield also can protect the data signals from leaking out of the copper cable. In addition, Cat6a F/UTP cable does a much better job of eliminating ANEXT than Cat6a UTP, providing significantly more headroom for 10GbE over copper.

Compared with Cat6a UTP and F/UTP cable, Cat6a SFTP patch cable provides the maximum level of protection from interference and is found in the highest performance cables. With the double shield, the Cat6a SFTP cable allows for the fastest and stable transmission for 10GBASE-T networks. Furthermore, the additional foil on individual pairs can limit the amount of crosstalk and ANEXT effectively. Cat6a SFTP patch cable is currently prevalent in various verticals like government, healthcare, and education.

SFTP is indeed a fair option for 10G network deployment. The following video introduces the internal structure, typical applications, and Fluke test of FS Cat6a SFTP patch cable.

 

Consideration Factors for Best Cat6a Cable

After knowing how to choose from Cat6a UTP vs F/UTP vs SFTP cables, some other parameters of Cat6a cables also affect the performance. Here are several key considerations to weigh when choosing the right Cat6a cable.

Cable Size and Weight

Cat6a cable operates at frequencies up to 500 MHz—twice that of Cat6. Controlling noise and crosstalk at higher frequencies, the Cat6a cable is up to 50% larger than its Cat6 predecessor. A larger size means fewer cables can fit into a cable tray or conduit, which is a big concern in retrofit installations. While many available Cat6a options remain significantly larger and heavier, some of the latest Cat6a cables are only about 15% larger than Cat6.

Bend Radius

Larger cable diameters of Cat6a cables mean a larger bend radius, which is important when routing cables in tight spaces such as inside wall cavities. The bend radius also affects the ability to route cables for maximum airflow within racks. The smaller the bend radius, the easier the cable is to route and install.

Installation

Most Cat6a Ethernet cables are larger because they have more and thicker materials. More twists in the copper pairs, larger splines separating the pairs, and thicker outer jackets. All of these lead to a longer time to prepare and terminate Cat6a cables. Normally, thinner cables take less time to install.

EMI Shielding

There is a perception that shielded cable provides better noise immunity, but the effectiveness of the shield depends on the quality and reliability of the shield termination, balance of the twisted pairs, and quality of the local and remote ground connection. The impedance of the ground connection can increase higher frequencies and differences in ground potential can couple noise into the conductors. Cable designs that effectively surround the conductors with a Faraday cage can provide an electromagnetic barrier without the potential drawbacks of grounding.

Channel Length

When transmitting PoE, some small-diameter Cat6a cables may not support a transmission distance of 100 meters per channel. However, without a doubt, Cat6a cables can support a 100-meter transmission distance in other data transmissions. Cables that can support the full 100 meters not only provide additional performance margin but also support a wider range of data center configurations, including rack-top configurations, end-of-row configurations, and mid-row configurations. Therefore, you can decide whether to deploy Cat6a cables based on your specific needs.

Network Infrastructure

When selecting the proper cable for your business, you also need to take the overall network infrastructure into consideration, like whether your business owns or rents the building. Things like the primary usage or your 10G network, the potential infrastructural changes, etc. are also should be taken into account.

Plan for Future Growth

Cat6a cables have become the standard configuration for new constructions, experiencing an upward trend in applications in hospitals, data centers, and universities, thanks to the performance upgrades brought by CAT6A cables. The future-oriented features provided by Cat6a cables have contributed to their popularity and widespread deployment. Cat6a cables should be prioritized in the following scenarios:

  • Planning to upgrade speeds to 10 Gbps over long distances, up to 100 meters.

  • The planned lifespan of the new cable network is 5 years or more.

  • Seeking to install a cost-effective cable solution, but replacing it with a higher-spec cable in the future might be expensive.

 

The Bottom Line

Before deciding on the best Cat6a cable, all factors need to be weighed up so that the Cat6a Ethernet cable you buy is future-proofing for your 10GBASE-T networks. Cat6a UTP, S/UTP, F/UTP, and SFTP cables are all available for 10GBASE-T. SFTP Cat6a patch cable with better performance shows more advantages in the 10GBASE-T network deployments.

What's more, you need to evaluate your current and future data requirements. Cat6a cabling infrastructure requires proper design, planning, products, and installation practices. Before you choose the right Cat6a cable, take the abovementioned factors into consideration to realize an optimized Cat6a structured cabling system for your 10 gigabit Ethernet networks.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k