English

What is Distribution Layer and How to Choose Distribution Switch

Updated on May 25, 2021 by
44.4k

The distribution layer is the second layer of the Cisco three-layer hierarchical model. Switches connected in this layer are known as the distribution switches. Unlike access switches, distribution switches do not provide any service to end devices. This article will introduce what the distribution switch is and how to select the right distribution layer switches for your enterprise network.

What is the Distribution Layer?

The Cisco three-layer hierarchical model contains three layers: core, distribution, and access. The core layer is the backbone of the network. It provides a high-speed connection between different distribution layer devices. The distribution layer connects the access layer to the core layer. The access layer provides initial connections to end users.

The distribution layer is the smart layer in the three-layer model. Routing, filtering, and QoS policies are managed at the distribution layer. Distribution layer devices also often manage individual branch-office WAN connections.

What is Distribution Switch?

The switch working in the distribution layer is called distribution switch which receives traffic from the access layer and forwarding it to the core layer, determining the workgroup access as well as providing policy-based connectivity.

However, aggregation switch is not a must-have in every situation, and access switches can be connected directly to the core switch without passing through the aggregation switch, especially when there is a short transmission distance, and the core layer has enough access ports to connect directly to the access layer. In this condition, one can save the overheads, relieve the maintenance burden, and network conditions are also easier to monitor.

What does a Distribution Switch Do?

A distribution switch aggregates the traffic from the access layer, and forward and switch the data packets. A distribution switch handles local routing, filtering, traffic balancing, QoS priority management, and security mechanisms, IP address conversion, traffic shaping, and multicast management based on the user traffic of the access layer, according to which then forward user traffic to the core switching layer or route locally. It also complete the conversion of various protocols (such as aggregation and redistribution of routes, etc.) to ensure that the core layer connects areas running different protocols.

Factors to Consider When Choosing Distribution Switches

With the general factors such as port type, port density and port speed considered, the following section will focus on the switch forwarding rate and functions that the distribution layer requires. Here are the factors for reference.

Layer 3 Function

It is always the responsibility of distribution switches to process Layer 3 data. The traffic generated from the access layer devices needs to be segmented into VLANs, requiring the upper-class switches to provide inter-VLAN routing functions so as to enable the multiple VLANs to communicate with each other. Since the core layer has a heavy task to handle the forwarding of the extremely high volumes of traffic, distribution switches with Layer 3 functionality are deployed to ease the workload of the core switches.

Forwarding Rate

The forwarding rate embodies the processing capabilities of a switch in the form of the data number that a switch process per second. It is a critical factor to consider when choosing a distribution switch. It is often the case that the forwarding rate of distribution switches is higher than the access switches. If the packet forwarding rate is too low, the distribution switch will not accommodate full wire-speed communication.

Redundancy

Redundancy is an important issue to consider for distribution switches. It is suggested that distribution switches should support multiple and hot swapping power supplies so as to achieve higher availability. With the redundant power supplies, the distribution switches can still operate normally without affecting the network traffic even if one power supply fails. In the meantime, the power supply can be replaced with a new one while the other one keeps operating as usual.

Link Aggregation

To forward all the traffic generated from the access layer to the core layer as fast as possible, distribution switches should support link aggregation so as to increase the network performance by keeping the traffic among a bunch of links balanced. Another key feature to use link aggregation is when a failure occurs, link aggregation will provide quick recovery. Generally speaking, link aggregation is an essential factor to take into consideration, which both increases availability and provides redundancy.

Security Policy

Security policy needs to be employed on the distribution layer switches to prevent promiscuous traffic through the network and allow others to go through. With the use of security policies such as access control list (ACL), the distribution switches can identify which types of traffic are permitted to communicate and which does not match the ACL rules defined on the switch ensuring the security of the whole enterprise network.

QoS Capacity

Setting up an intelligent QoS is essential for effective network capacity. As so many users sending traffic of various types within the LAN, deploying distribution switches with QoS features will read packets and prioritize delivery based on the policies so as to enable the important traffic to go first. It will ensure the audio and video data communicate in an adequate bandwidth.

Conclusion

To sum up, the distribution layer is the second layer of the Cisco three-layer hierarchical model. The switch working at this layer is called distribution switch which receives traffic from the access layer and forwarding it to the core layer, determining the work group access as well as providing policy-based connectivity. To choose the right distribution switch, there are several factors to consider, such as port type, port density and port speed, layer 3 function, forwarding rate, redundancy, link aggregation, security policy, QoS capacity etc,.

Related Articles:

How to Choose the Right Access Layer Switch? 

Understanding Link Aggregation and LACP [FAQs]

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k