InfiniBand Cable: Key Component of High-performance Computing
In the fast-paced world of high-performance computing (HPC), where data-intensive applications and demanding workloads reign supreme, the need for efficient and high-speed network connectivity has never been greater. InfiniBand Cable is a critical component in the realm of high-performance computing (HPC) and data-intensive applications. In this article, we delve into the features, advantages, and diverse applications of InfiniBand cable, shedding light on its pivotal role in shaping the future of computing.
What Is InfiniBand Cable?
InfiniBand cables are factory-terminated copper cable assemblies constructed of high-speed twinaxial shielded cable terminated to 4X MicroGigaCN™ type connectors on each end. The cables are designed for insertion into standard 4X receptacles. It is specifically used to establish reliable and fast connections between servers, storage devices, and other network components. InfiniBand cables are known for their ability to provide high bandwidth and low latency, making them suitable for demanding applications that require efficient data transfer and parallel computing.
Link Rates Development of InfiniBand Cables
The development of InfiniBand cables has undergone significant advancements in terms of data transfer rates to meet the ever-increasing demands of high-speed connectivity. Here is an overview of the link rate development for InfiniBand cables:
Category | 1X | 4X | 8X | 12X |
Single Data Rate (SDR) | 2.5Gbps | 10Gbps | 20Gbps | 30Gbps |
Double Data Rate (DDR) | 5Gbps | 20Gbps | 40Gbps | 60Gbps |
Quad Data Rate (QDR) | 10Gbps | 40Gbps | 80Gbps | 120Gbps |
Fourteen Data Rate (FDR) | 14Gbps | 56Gbps | 112Gbps | 168Gbps |
Enhanced Data Rate (EDR) | 25Gbps | 100Gbps | 200Gbps | 300Gbps |
High Data Rate (HDR) | 50Gbps | 200Gbps | 400Gbps | 600Gbps |
Next Data Rate (NDR) | 100Gbps | 400Gbps | 800Gbps | 1200Gbps |
eXtended Data Rate (XDR) | 200Gbps | 800Gbps | 1600Gbps | 2400Gbps |
Advantages of InfiniBand Cables
InfiniBand Cable provides several advantages that make it a preferred choice in high-performance computing (HPC) and data-intensive environments. The picture below shows the advantages of InfiniBand Cable, and high bandwidth and low latency are outstanding advantages of it.
-
High Speed and Bandwidth: InfiniBand Cable offers exceptionally high data transfer rates, ranging from 10Gbps to 800Gbps (depending on the generation). This high-speed connectivity enables rapid and efficient communication between network components, allowing for fast data transfers and reduced processing time.
-
Low Latency: InfiniBand Cable provides extremely low latency, minimizing the time it takes for data to travel between devices. This low-latency characteristic is crucial for real-time applications, high-frequency trading, scientific simulations, and other time-sensitive workloads where immediate response and quick data processing are essential.
Types of InfiniBand Cables
There are different types of InfiniBand cables designed to meet various connectivity needs. The most common types of InfiniBand cables include:
-
InfiniBand DAC Cables: InfiniBand DAC (Direct Attach Copper) cables are copper-based cables with connectors on both ends. These cables are pre-terminated with InfiniBand connectors, such as QSFP (Quad Small Form-factor Pluggable) or SFP (Small Form-factor Pluggable), and are used for short-range connections. DAC cables provide a cost-effective solution for high-speed data transfer within a rack or between neighboring racks.
-
InfiniBand AOC Cables: InfiniBand active optical cables use fiber optic technology for data transmission. They consist of optical fibers and active components, such as transceivers, to convert electrical signals into optical signals. These cables are capable of longer reach compared to copper cables and provide high-speed, low-latency connectivity. InfiniBand AOC cables are commonly used for inter-rack or inter-building connections.
-
InfiniBand Breakout Cables: InfiniBand Breakout cables are specialized cables designed to split or breakout high-density connectors into multiple lower-density connectors. These cables convert a single high-density connector, such as QSFP, into multiple lower-density connectors, such as SFP or QSFP28. Breakout cables enable efficient utilization of network resources and provide flexibility in connecting devices with different connector types or configurations. They are commonly used in scenarios where there is a need to connect multiple devices or systems with different port densities or form factors.
Differences Between InfiniBand Cables and Ethernet Cables
InfiniBand Cables and Ethernet Cables are two distinct types of interconnect technologies used in networking. Here are some key differences between them:
-
Application: InfiniBand Cables are primarily designed for high-performance computing (HPC) environments and data centers with demanding workloads. They excel in low-latency, high-bandwidth applications, such as scientific simulations, financial trading, and parallel computing. Ethernet Cables, on the other hand, are widely used in general networking scenarios, including office networks, internet connectivity, and local area networks (LANs).
-
Data Transfer Rates: InfiniBand Cables typically offer significantly higher data transfer rates compared to Ethernet Cables. InfiniBand supports data rates ranging from 10Gbps to 800Gbps (and beyond), while Ethernet commonly ranges from 10Mbps to 100Gbps. The higher data rates of InfiniBand make it more suitable for data-intensive applications that require rapid data processing and high-speed communication.
-
Latency: InfiniBand Cables provide extremely low latency, making them ideal for applications that demand real-time responsiveness and minimal delay. Ethernet Cables generally have higher latency compared to InfiniBand, although advancements in Ethernet technology have reduced latency over the years.
-
Network Topology: InfiniBand supports both point-to-point and switched fabric topologies. It is commonly used in high-performance clusters and supercomputers, where nodes are interconnected in a high-speed, high-bandwidth network. Ethernet, on the other hand, is typically deployed in a star or tree network topology, connecting multiple devices to a central switch or router.
-
Cost: Ethernet Cables are generally more cost-effective compared to InfiniBand Cables. Ethernet technology has widespread adoption, leading to economies of scale and lower prices for Ethernet equipment. InfiniBand, being a more specialized and high-performance technology, often comes with a higher price tag.
InfiniBand Cables | Ethernet Cables | |
Application | Primarily designed for high-performance computing (HPC) and data centers with demanding workloads | Widely used in office networks, internet connectivity, and local area networks (LANs) |
Data Transfer Rates | 10Gbps to 800Gbps (and beyond) | Commonly 10Mbps to 100Gbps |
Latency | Low latency | Higher latency |
Network Topology | Support both point-to-point and switched fabric topologies | Typically deployed in a star or tree network topology |
Cost | High | Low |
NVIDIA InfiniBand Cables Recommendation
NVIDIA InfiniBand cables are typically used to link ToR switches down to NICs, storage devices, and CPU servers, or link up to switch-to-switch interconnect applications throughout the network infrastructure. It includes InfiniBand DAC cables and InfiniBand AOC cables.
NVIDIA InfiniBand DAC Cables
FS NVIDIA InfiniBand DAC cables are suited for interconnecting high-speed 40G-800G networking applications such as servers, switches, data centers, high-performance computing networks, enterprise cores, and distribution layers. The DAC Twinax cables have optimized construction to minimize insertion loss and cross-talk and are available in a range of wire gages from 26AWG through 30AWG.
Product | Description | Form Factor | Length |
40G DAC Cable | NVIDIA InfiniBand QSFP+ 40G Direct Attach Copper Twinax Cable | QSFP+ to QSFP+ | 0.5m/1m/1.5m/2m/3m/4m/5m |
56G DAC Cable | NVIDIA InfiniBand QSFP+ 56G Passive Direct Attach Copper Cable | QSFP+ to QSFP+ | 0.5m/1m/1.5m/2m/3m/4m/5m |
100G DAC Cable | NVIDIA InfiniBand QSFP28 100G Passive Direct Attach Copper Twinax Cable | QSFP28 to QSFP28 | 0.5m/1m/1.5m/2m/3m |
200G DAC Cable | NVIDIA InfiniBand QSFP56 200G Active Direct Attach Copper Twinax Cable | QSFP56 to QSFP56 | 3m/5m/7m |
200G DAC Cable | NVIDIA InfiniBand QSFP56 200G to QSFP56 2x100G Passive Direct Attach Copper Breakout Cable | QSFP56 to 2x QSFP56 | 0.5m/1m/1.5m/2m |
400G DAC Cable | NVIDIA InfiniBand OSFP 400G to QSFP56 2x200G Passive Direct Attach Copper Breakout Cable | OSFP to 2x QSFP56 | 1m/1.5m/2m |
800G DAC Cable | NVIDIA InfiniBand OSFP 800G Passive Direct Attach Copper Twinax Cable | OSFP to OSFP | 0.5m/1m/1.5m |
800G DAC Cable | NVIDIA InfiniBand OSFP 800G to OSFP 2x400G Passive Direct Attach Copper Breakout Cable, Finned Top | OSFP to 2x OSFP | 0.5m/1m/1.5m/2m |
800G DAC Cable | NVIDIA InfiniBand OSFP 800G to OSFP 4x200G Passive Direct Attach Copper Breakout Cable | OSFP to 4x OSFP | 0.5m/1m/1.5m/2m |
NVIDIA InfiniBand AOC Cables
NVIDIA InfiniBand AOCs are extremely low-cost optical interconnect cables. The optical fiber is buried in the connector, which acts as a DAC, but with a link distance of up to 100 meters. InfiniBand cables provided by FS are available for FDR10, FDR, EDR, HDR, and NDR rates. They are widely used in high-performance computing, hyper-scale, enterprise, and DGX artificial intelligence systems.
Product | Description | Form Factor | Length |
40G AOC Cable | NVIDIA InfiniBand QSFP+ 40G Active Optical Cable | QSFP+ to QSFP+ | 1m/3m/5m/7m/10m/15m/20m/25m/30m/50m/100m |
56G AOC Cable | NVIDIA InfiniBand QSFP+ 56G Active Optical Cable | QSFP+ to QSFP+ | 0.5m/1m/1.5m/2m/3m/4m/5m |
100G AOC Cable | NVIDIA InfiniBand QSFP28 100G Active Optical Cable | QSFP28 to QSFP28 | 1m/2m/3m/5m/7m/10m/15m/20m/30m/50m/100m |
200G AOC Cable | NVIDIA InfiniBand QSFP56 200G Active Optical Cable | QSFP56 to QSFP56 | 1m/2m/3m/5m/10m/15m/20m/30m/50m/100m |
200G AOC Cable | NVIDIA InfiniBand QSFP56 200G to QSFP56 2x100G Breakout Active Optical Cable | QSFP56 to 2x QSFP56 | 1m/2m/3m/5m/10m/15m/20m/30m |
200G AOC Cable | NVIDIA InfiniBand QSFP56 2x200G to QSFP56 2x200G Breakout Active Optical Cable | 2x QSFP56 to 2x QSFP56 | 3m/5m/10m/15m/20m/30m |
400G AOC Cable | NVIDIA InfiniBand OSFP 400G to QSFP56 2x200G Breakout Active Optical Cable | OSFP to 2x QSFP56 | 3m/5m/10m/15m/20m/30m |
Summary
As technology continues to advance, the demand for faster and more efficient data transfer solutions will only increase. InfiniBand cables are well-positioned to meet these demands, providing the necessary speed, reliability, and scalability for future computing needs. Their high-speed capabilities, low latency, and scalability make them an indispensable component in modern data centers, enabling organizations to achieve optimal performance and productivity.
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023