English

Investigate the Differences in the PCI Family of Interface Standards

Posted on Mar 29, 2024 by
111

In the realm of computer hardware, a variety of interface standards coexist to ensure effective communication and expansion between components. From the PCI to the advanced M.2 interface, each standard plays a unique role. Understanding the differences between interfaces such as PCI, PCI-X, and PCI-E is crucial for selecting the right network cards to enhance system performance. In this article, we will delve into the characteristics and main differences among these network adapters' technological standards.

PCI (Peripheral Component Interconnect)

PCI (Peripheral Component Interconnect), as an early mainstream computer bus interface standard, facilitates data transfer between hardware devices like graphics and network cards and the motherboard. Intel proposed the PCI (Peripheral Component Interconnect) "Peripheral Component Interconnect" bus protocol in 1991 and established the PCI-SIG (PCI Special Interest Group), which is responsible for the formulation and promotion of the standard. Since then, it has been widely implemented in the electronics and communications fields. Designed for 32 or 64 bits wide and operating at 33MHz or 66MHz, PCI had wide compatibility but slower speeds.

PCI-X (PCI eXtended)

PCI-X (Peripheral Component Interconnect eXtended) is an improved version of PCI that supports three different clock frequencies, namely 33MHz, 100MHz and 133MHz, which means it supports higher data transfer rates with a maximum rate of 1GB/s (133MHz * 64bit/ 8 = 1GB/s). Although its bandwidth is greater, PCI-X's adoption was limited in the consumer market, mainly in servers and enterprise computing contexts.

PCI-E (PCI Express)

PCI-E (Peripheral Component Interconnect Express) is a high-speed serial computer expansion bus standard that significantly increases data transmission rates through a point-to-point connection model. Unlike the parallel shared bus attributes of PCI and PCI-X, PCI-E is a serial independent bus and a differential signal, which has stronger anti-interference ability and means that the transmission rate can be higher. PCI-E utilizes "lanes" as serial connections, each being a two-way serial interface, and the data supports x1, x4, x8, x16 and x32 bit widths.

Parallel Connection vs Serial Connection

PCI-E Network Card

PCI-E network cards are hardware expansion cards that utilize the PCI-E interface, including graphics cards, sound cards, and other types of expansion cards. A notable feature of these cards is their compatibility with various slot specifications (x1, x4, x8, x16), offering greater flexibility and potential for expansion.

Bus type

FS has been committed to providing efficient data transmission and solutions for optimizing network performance. In this digital era, PCIe network cards have become a key component to achieve high-speed data transmission and improve network performance. FS strongly recommends PCIe network card technology to meet growing data demands and provide an excellent network connection experience. The following table shows the NVIDIA, Intel and Marvell PCIe network cards provided by FS.

Categories
Data Rate
Ports
Host Interface
100G QSFP56 / 200G QSFP56 / 400G OSFP / 400G QSFP112
Dual / Single
PCIe 4.0 x16 / PCle 5.0 x16
25G SFP28 / 100G QSFP28 / 100G QSFP56 / 200G QSFP56 / 400G OSFP / 400G QSFP112
Dual / Single
PCIe 3.0 x8 / PCIe 4.0 x8 /
PCIe 3.0 x16 / PCle 5.0 x16 / PCIe 4.0 x16
10GRJ45 / 10G SFP+ / 25G SFP28 / 40G QSFP+ / 100G QSFP28 
Dual / Quad / Single
PCIe 2.0 x8 / PCIe 3.0 x4 /
PCle 4.0 x16 / PCIe 3.0 x8 /
PCIe 4.0 x8
16G SFP+ / 32G SFP+
Dual
PCIe 3.0 x 8

Mini PCI-E & M.2 (NGFF) & Add-in Card

Mini PCI-E is a smaller version of the PCI-E standard, primarily used in laptops and compact devices. It provides similar technological advantages to PCI-E but is optimized for space-constrained devices.

The M.2 interface, formerly known as the Next Generation Form Factor (NGFF), is designed for internal hardware connections, especially for SSDs in small devices. The M.2 standard is not only more compact but also delivers higher data transmission speeds and is one of the most popular storage solutions today.

Add-in Card broadly refers to any expansion card that can be added to a computer's motherboard, inclusive of but not limited to the aforementioned PCI series cards.

Conclusion

Recognizing and understanding the differences between these interface standards can help users make informed choices for their computer systems. Whether seeking high-speed data transfers or needing to configure within a limited space, the various PCI standards and interfaces discussed provide solutions to meet diverse requirements. As technology continues to evolve, these interface standards have become an integral part of building efficient, high-performance systems.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.7k