English

Blank Multimedia Adapter Patch Panel for Mixing Fiber and Copper Cabling

Updated on Jul 23, 2018 by
4.2k

No matter we are constructing a copper network or a fiber optic network, inline coupler or fiber adapter always plays an important role in terminating or connecting between two lines. Now both copper networking and fiber optic networking technologies are being developed to meet the continuously increased bandwidth needs. And there are cases where we have to implement mixing fiber and copper link, such as link aggregation through EtherChannel or IEEE 802.3ad standards. Then how to effectively and efficiently couple both copper keystone jacks and fiber connectors on one panel? This post will provide the solution by using the blank multimedia adapter patch panel, which can manage and organize a wide variety of fiber and copper cabling.

blank multimedia adapter patch panel-1

Why Mixed Fiber and Copper Link?

At first, let’s have a glance at why there is a need for mixing fiber and copper cables. Ten years ago, people were asking if it was possible to have copper and fiber as part of the same port-channel group. And now, the term link aggregation is no longer new in constructing network architecture. And EtherChannel technology or IEEE 802.3ad both serves for link aggregation. Link aggregation combines multiple network cosnnections in parallel in order to increase throughput beyond what a single connection could sustain, and to provide redundancy in case one of the links should fail. It groups a number of physical Ethernet links to create a single high-bandwidth data path. It can provide fault-tolerance and high-speed links between switches, routers and servers, and enhance the connection reliability and resilience. It is possible to aggregate copper ports for one link and fiber ports for the second link, but the important thing is to keep the two links at the same speed and as full-duplex. Under this circumstance, blank multimedia patch panel is designed to achieve the purpose.

Benefits of Blank Multimedia Adapter Patch Panel

When one link consists of both copper Ethernet patch cable and fiber patch cables, the blank multimedia patch panel makes a difference. For standard adapter panels with fixed ports, the patch cable that can be used is limited to one type. For example, every keystone patch panel can hold only one category style Ethernet patch cable, whether it is for Cat5e or Cat6 patch cables; and every preloaded fiber adapter panel can hold only one type of connector, such as single-mode LC APC duplex, LC UPC duplex, multimode SC APC duplex, etc. However, our blank multimedia adapter patch panel is much flexible in copper and fiber mixed implementations. It allows users to aggregate up to six different types of ports at one time. These ports can be either copper or fiber. The inserted keystone jacks or inline couplers can be Cat6a, Cat6, Cat5e or Cat5. And the fiber optic adapters can be standard LC duplex, SC simplex and MTP/MPO. Users can install various port types on demand.

blank multimedia adapter patch panel-2

Moreover, it is very cost-effective as it may avoid port wasting. There are six blank ports on the mutimedia adapter patch panel. Generally, users can make use of all of them or deploy suitable number of adapters on it, so as to avoid waste of loaded ports.

blank multimedia adapter patch panel-3

In addition to these two major benefits to the users, blank multimedia adapter patch panel also has some other good features. It has a two-tier design, and the cover plate on the rear can add mounting stability. Also plastic clips are optional for fiber adapter installation. It will be very easy to configure the snap-in modules on the panel. One bonus this patch panel can bring is that it is fitted with FS FHD fiber optic enclosures and cable management panels, which provides a clean, flexible and tidy cable managing for your network.

Choose Blank Multimedia Patch Panel

Blank multimedia adapter patch panel allows customization of installation for multimedia applications requiring integration of fiber patch cables and copper cables. It is an ideal solution for a mixing copper and fiber link in some implementations. The flexible configuration it brings and cost-effectiveness it owns will no doubt make it a favorite in applications that require multiple port types. Every move, add, or change of coupler on it will be effortless. FS designed this blank multimedia adapter patch panel for your convenience in fiber patching and cable management. For more details, please visit FS.com.

Related Article

Fiber Patch Panels: Network Necessities

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.9k