English

What Open Network Switch Means to SDN Deployment

Updated on Apr 3, 2018 by
4.8k

Business now is becoming more network-centric than ever, which further stretches the limit of network speed and agility. SDN (Software-defined networking) has thus been brought into the public eye, as a lower-cost alternative to traditional network hardware. The journey to SDN has been made easier with open network switch—together they create a software-based approach to build more scalable and agile networks that can better align and support the system requirement. So what exactly is open network switch and how it benefit SDN implement? That what we are gonna explore in this article.

SDN: The Future of Networking

When looking into SDN technologies, you’ll hear a lot about the benefits of centralized control and networking visibility. SDN is valued for its ability to decouple the control plane from the packet-forwarding (data) plane within the network. In this case, network configuration and management can be made from a central location, rather than accessing every specific switches or services through the network. Companies thus can reap great benefits from the reduced operational costs, improved network agility and simplified system provisions. One of the prominent features of SDN is the SDN controllers—with northbound interfaces that can communicate with applications via application programming interfaces (APIs), it enables direct program of the network. SDN now is becoming practical and the deployment of which is heating up recently. Here is a simple graph showing SDN architecture.

SDN

Open Network Switch: Embrace the Prime Time

Open network switch, as a completely open platform, is typically used as a top-of-rack switch and/or as part of an SDN deployment. Unlike brand switch, open network switch hardware and software are separated. This separation of open network switch software and hardware makes open network switch very popular in SDN. Users have more freedom to buy software from one vendors and hardware from the other, which greatly splashing the overall cost. Open network switch has advanced a lot from what it’s used to be and has get fully prepared for a broader adoption—it has improved significantly in cost and reliability, features and capabilities, as well as network operations.

N8550-32C

How SDN Facilitate Open Network Switch Deployment?

Open network switch is maturing into mainstream adoption in an SDN deployment, which rivals traditional switches witha much lower price and equivalent operational costs. Open network switch has shown they can hold their own in SDN deployments and supporting industry standards. In SDN environment, the SDN controller serves as the OS of open network switch. The SDN controller usually use protocol like OpenFlow or another southbound API to program open network switch to create routing tables and route connections. This allows the customers to flexibly design and set their network and switches. SDN has become the primary drives of open network switch prevalent for the following reasons.

Openness: Although open network switch has no direct relation with SDN, they share the same characteristic—openness. Open network switches provide the flexibility to choose hardware and software. As for SDN, it simplifies network design and operation by providing instructions through the SDN controllers instead of multiple, vendor-specific devices and protocols. This similarity makes SDN users accept the open network switches more easily in the aspect of concept.

Decreased Complexity: SDN allows all networking components to be controlled through a singular device. Both physical and virtual devices are controlled by a single API, making the work of network administrators much easier. And this control method convinces users that the quality of open network switch is reliable, for problems are often caused by software but not hardware.

Reduced Price: Many brand vendors do not attach much importance to the hardware manufacture, so some of them begin to expand the market of open network switch. And the quality of those open network switches has been verified by customers. Besides, many small vendors also cut their price to attract customer, which further brings down the cost.

Conclusion

It’s said that the proliferation of SDN technology will fundamentally transform the telecom industry. Open network switch promises high levels of freedom for networking that greatly fits for SDN environment. It also helps avoid vendor lock-in and OEM shipping delays. Considering to start your own open network switch initiative? It’s suggested to gradually move to this field, and determine how open network switch deployments can benefit your network.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.7k