English

Open Network Switch: Will It Be the Great Choice for Next Generation Network?

Updated on Jun 1, 2022 by
6.5k

With the increasing maturity of cloud computing and 5G technology, large enterprises and data center providers have improved their requirements for network equipment. Therefore, more and more enterprises prefer open network switches for data centers to achieve simple and flexible management and deployment.

 

What Is Open Network Switch?

Open network switches, or white label switches, are open network switches with decoupling of hardware and software. They are usually based on Linux and run on off-the-shelf chips, which help network administrators customize the device according to the needs of the organization. Nowadays, open network switches are wildly used in large enterprises like Google, Microsoft, Facebook, etc.

Generally, open network switches have three main features: firstly, they are built on commodity hardware; secondly, they use Application Specific Integrated Circuit (ASICs) from established vendors; thirdly, open network switches run an Open Network Operating System (ONOS). In addition, open network switches are commonly used in Software-defined Networking (SDN), which enables them to achieve network programmability—one of the most significant differences from traditional switches.

what is open switch

How Does Open Network Switch Work?

As mentioned above, open network switches use standardized chips and ONOS, which can better meet users' needs to achieve seamless integration of network and computing storage at a relatively low price.

With the help of hardware and software decoupling technology, hardware in white box networking can be standardized while software can be customized, thus creating a flexible and open operating system. In this way, users can choose a suitable operating system based on their requirements. For instance, customers can buy hardware and software from different open network switch vendors, and then install it by themselves.

Furthermore, open network switches replace the proprietary switch interface from large legacy switch vendors with generic Linux interfaces, realizing network programmability while improving the performance of Linux platform at the same time. Besides, Linux interfaces are also more acceptable and easy-management for server administrators.

 

Why Is Open Network Switch Getting Popular?

Compared with traditional switches, open network switches do show their advantages in several respects, including performance, operation, price, etc. That's the reason why they are increasingly becoming the first choice of many large enterprises.

  • High performance: Open network switches usually have higher port density, so they perform better than traditional layer 2 or layer 3 switches. Additionally, open network switches are also more scalable without the limitation of traditional layer 2 or layer 3 protocols. Therefore, they can facilitate a more concise leaf-spine network topology while providing simpler connectivity and higher performance.

  • Simplicity: A large difference between open network switches and traditional switches is network programmability. With the help of ONOS, open network switches can easily achieve network automation and high flexible, scalable network connectivity, while the functions of traditional switches are quite limited.

  • Free choice: The traditional switches integrate hardware tightly into software, leaving users with no freedom of choice. In contrast, since hardware and software are disaggregated in a white box network, customers are free to choose and customize their hardware and software based on their needs.

  • Fast innovation: In traditional enterprise networks, companies handle the increased traffic loads by upgrading edge switches or switch chassis, which is time-consuming and also complex. However, because open network switches are assembled from commodity parts, they can innovate faster with a DevOps and community approach.

  • Low cost: Severed as a part of SDN deployments, open network switches support OpenFlow protocol, which can reduce the network cost. Besides, they can be sold with other open-source software or just as bare metal devices, significantly saving CapEx and OpEx compared to traditional networks.

    Open Network Switch

    Open Network Switch Trends and Challenges in Data Center and Cloud

    As more and more enterprises turn to network infrastructure that supports cloud computing, traditional switches cannot meet companies' demands for realizing the maximum profit. In this case, the advantages of open network switches have increasingly emerged.

    Marketing Trend of Open Network Switches

    The data center market is fundamentally changing due to the impact of the pandemic. According to IDC, in the first half of 2020, the favored large-scale cloud environment open network switch revenue grew by more than 34%, which promoted segment from fourth in 2019 to third in the overall switch market.

    In fact, the largest cloud providers, such as Google and Amazon, primarily deploy open network switches on their networks, which have pushed the development of open network switches market. However, with the segment market becoming gradually crowded, open network switches vendors will attempt to expand the market to tier-2 cloud providers, large enterprises or telecom service providers. In this way, the open network switches market share of the largest cloud providers may get threatened. For example, according to IDC, Cisco's share of data center switches has fallen from more than 53% to 41.4% in the first half of 2020.

    To sum up, it is clear to see that open network switches are becoming popular among the cloud providers. Although they are in their early days, they still hold enormous potential for telecom networks and many data centers.

    Challenges of Open Network Switches

    By now, you probably have a clear idea of the merits of open network switches. But no one is perfect. It's also necessary to know the challenges faced by open network switches.

    For one thing, open network switches are mainly deployed in cloud data centers. As for large-scale network scenarios like metro network, they are still at their very early stage.

    For another, the current market share of open network switches is still very low. In most cases, open network switches are deployed alongside traditional switches, which affects the formation of a complete end-to- end switch system. Thus, the performance benefits of open network switches will be limited.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Howard.
Howard
What Is Open Networking?
Jun 1, 2022
6.0k
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge