English

OSPF vs BGP: Which Routing Protocol to Use?

Updated on May 7, 2021 by
109.5k

Both OSPF (Open Shortest Path First) and BGP (Border Gateway Protocol) are routing protocols that make routing decisions across the Internet. They represent a set of rules or algorithms that instruct network routers on how to communicate with each other, so they can redirect traffic to the best path. OSPF vs BGP, what are their differences? How to choose between the two?

OSPF vs BGP: What Are the Differences?

The main difference between OSPF and BGP is that OSPF is an intra-domain routing protocol using link state routing, and the routing operation is performed inside an autonomous system while BGP is the inter-domain routing protocol that uses path vector routing, with the routing operations performed between two autonomous systems. Some other distinctions between OSPF vs BGP include:

  • Configuration: OSPF is easily-configured while BGP configuration is a lot more complex.

  • Convergence rate: OSPF can achieve convergence (the time a router takes to share and update the latest routing information) faster. In contrast, the BGP has a slow convergence rate.

  • Network topology or design: OSPF is a type of hierarchical network topology or design while BGP is a type of mesh topology or design.

  • Resources requirement: OSPF requires intensive use of memory and CPU resources. With BGP on the other hand, the size of the routing table dictates the required device resources.

  • Scale: BGP is more flexible and scalable than OSPF and it is also used on a larger network.

  • Preferred path: OSPF is used to determine the fastest route while BGP puts emphasis on determining the best path.

  • Protocol: In OSPF, internet protocol is used. While in BGP, transmission control protocol is used.

Here is a chart summarizing the differences of OSPF vs BGP:

  OSPF BGP
Gateway Protocol Internal gateway protocol External gateway protocol
Implementation Easy Complex
Convergence Fast Slow
Design Hierarchical network possible Meshed
Need for device resources Memory and CPU Intensive Scaling is better in BGP although it relies on the size of the routing table
Size of the networks Used on primarily smaller scale network which could be administered centrally Mostly used on large scale networks such as the internet
Function The fastest route is preferred over shortest Best path is determined for the datagram
Algorithm Used Dijkstra algorithm Best path algorithm
Protocol IP TCP

OSPF vs BGP: How to Choose?

Now that you have gained a basic understanding of ospf and bgp, you may want to know when and how to choose from or apply them? On the one hand, if you are conducting internal routing, such as routing within a site, company, or campus, you will want to use OSPF as it is used for internal network routing. This would typically work between switches and routers in the same location. On the other hand, if you are looking at building in-site with multiple homes, you might want to consider BGP. Generally, most of the service providers would adopt the BGP to carry customers' routes.

what is ospf vs bgp

One thing to mention is that they do not necessarily compete with each other, instead, they are used together in most cases. In the data center, OSPF is usually the common protocol for internal routing between network switches and/or routers. When that traffic needs to travel to another organization, whether it be to an MPLS network with other sites or the internet, BGP usually comes into play.

Here we list three popular network switches that support both bgp and ospf.

  N5860-48SC S5850-48T4Q S5860-20SQ
Ports 48 x 10Gb SFP+; 8 x 100Gb QSFP28 48 x 10G BASE-T; 4 x 40Gb QSFP+ 20 x 10G SFP+; 4 x 25G SFP28; 2 x 40G QSFP+
OSPF
BGP
Key Features MLAG, Stack, VXLAN, EVPN, OSPFV2/V3, BGPV4/V6, Netconf, PFC, ECN, GR VLAN, QoS, IGMP Snooping, Link Aggregation, Static Routing, RIP, OSPF, IPv6 support, VxLAN/MPLS/EVPN, Advanced Routing Protocol (BGP/ISIS), MLAG QoS, IGMP Snooping, Link Aggregation, IPv6, L3 Static Routing, RIP, OSPF, Advanced Routing Protocol (BGP/ISIS), Advanced Security, Stack
Application Scenario Small-sized data centers and cloud computer services The next generation Metro and enterprise network SMB or campus networks requiring low latency and high-density backbone architectures with basic routing capability.
AC/DC Power Supply AC AC AC/DC

Although BGP is used between multiple autonomous systems as an external routing protocol, many network giants like Microsoft and Facebook would use it internally – in this case, BGP is typically fit for very large networks which OSPF fails to handle. One of the many reasons that BGP does not function well as an internal gateway protocol is that it is very slow to converge.

Related Article: 

RIP vs OSPF: What Is the Difference? 

EIGRP vs OSPF: What’s the Difference?

You might be interested in

Knowledge
See profile for Rameez Arif.
Rameez Arif
Top of Rack and End of Row: What's the Difference?
Jun 27, 2022
30.2k
Knowledge
See profile for John.
John
MLAG vs. vPC: What's the Difference?
May 19, 2022
45.6k
Knowledge
See profile for Howard.
Howard
VXLAN: the Future for Data Center Networks
May 20, 2023
7.9k
Knowledge
See profile for Howard.
Howard
EVPN-VXLAN: How to Use It in Data Center
May 20, 2023
10.2k
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge