English

A Quick View of QSFP-SFP10G-CVR

Updated on Oct 28, 2021 by
8.1k

QSFP+ to SFP+Converter Module

With the wide deployment of the 40G network, it's worthwhile to consider how to connect the present 10G network to the 40G network. Currently, there are several adaptable solutions that can help to realize 40G-10G migration: 40G QSFP+ to 4x10G SFP+ DAC breakout cables, 40G QSFP+ to 4x10G SFP+ AOC breakout cables, MTP/MPO-LC breakout cables, and the QSFP-SFP10G-CVR modules. Among them, QSFP-SFP10G-CVR module can use the existing 10G cabling for a 40G-10G transition.

 

What Is a QSFP-SFP10G-CVR Module?

The QSFP-SFP10G-CVR module, also known as QSFP+ to SFP+ adapter or 40G-10G adapter, is a type of the QSA adapter. It is built in a QSFP+ form factor with a cage for the SFP+ module at the back. That is to say, a low-speed SFP+ transceiver can be plugged into its back, allowing single-channel SFP+ transceivers to connect to 4-channel QSFP+ ports. The QSFP+ to SFP+ adapter is acting as an interface for the SFP+ transceiver during the process. With this adapter, 40G-10G migration is allowed when the other end of the network is running at lower speeds.

QSFP-SFP10G-CVR features with low insertion loss, low crosstalk, secure latching mechanism, QSFP+ MSA compliant, and trouble-free installation and network bring-up. It also has wide applications in data servers, routers and switches, networked storage systems, data center networking, and InfiniBand (IB).

10G sfp

Figure1: QSFP-SFP10G-CVR Module

 

QSFP-SFP10G-CVR: Reliable QSA Solution for 40G-10G Migration

Since the QSFP+ to SFP+ adapter ensures smooth connectivity between 40G and 10G devices by using SFP+ based cabling, it has been considered as an effective solution for converting 40G ports to the 10G ports after launch.

QSFP-SFP10G-CVR supports all SFP+ cables and is compatible with mainstream switch models and SFP+ modules. A list of SFP+ transceiver modules that can be plugged into it is provided in the table below.

Item Product Name Product Description
1 SFP-10G-SR 10GBASE-SR SFP+ module for multimode fiber
2 SFP-10G-LR 10GBASE-LR SFP+ module for single mode fiber
3 SFP-10G-ER 10GBASE-ER SFP+ module for single mode fiber
4 SFP-10G-ZR 10GBASE-ZR SFP+ module for single mode fiber
5 10G SFP+ copper cables SFP+ copper cables (1m to 10m lengths)
6 10G SFP+ active optical cables SFP+ active optical cables (1m to 100m lengths)

Here is a typical 40G-10G application case: with the cooperation of two 10GBASE-SR SFP+ transceiver modules, an LC duplex multimode fiber patch, and one QSFP-SFP10G-CVR adapter, 40G to 10G migration will be realized smoothly.

Figure 2: Direct connection for QSFP+ to SFP+ adapter module

 

QSFP-SFP10G-CVR Adapter vs. 40G QSFP+ Breakout Cables

40G QSFP+ to 4×10G SFP+ Breakout Cables Overview

QSFP+ to SFP+ breakout cable consists of a QSFP+ connector on one end and four SFP+ connectors on the other end. Generally speaking, QSFP+ to SFP+ breakout cable can be divided into direct attach copper cable (DAC) and active optical cable (AOC). They are used to transmit 40Gbps data into four separate streams of 10Gbps data over a fan-out cable in a point-to-multipoint configuration.

QSFP-SFP10G-CVR Adapter or QSFP+ Breakout Cables?

As mentioned above, we can use a QSFP-SFP10G-CVR adapter to convert a QSFP+ port to an SFP+ port. Or adopting QSFP+ to 4x10G SFP+ breakout cables to split a 40G port between a switch or a server into four 10G ports. In a word, both QSFP+ to SFP+ adapter and QSFP+ breakout cables are providing adaptable options for the 40G-10G transition. But what's the difference between them? The distinctions of the two solutions will be analyzed in three aspects: performance, cost, and utilization.

Figure 3: DAC&AOC Breakout Cables

Performance

QSFP+ to 4x10G SFP+ breakout cables split the 40G channel into 4x 10G channel, which provides four times more data transmission than QSFP-SFP10G-CVR adapter that just provides connectivity only for a single 10G connection.

Cost

It's not difficult to find that a product's pricing is related to its popularity in the market to a certain extent. QSFP-SFP10G-CVR may be more expensive than expected on the market on account of the exclusive patent by some vendors. For short-reach transmission (<10m), DAC breakout cables provide the most cost-effective solution.

Utilization

QSFP+ to 4x10G SFP+ breakout cables have mature technology compared to QSFP-SFP10G-CVR adapter, which hasn't been widely used yet for the aforementioned factors.

Figure 4: Direct Connection for 40G QSFP+ to 4SFP+ DAC

Considering the application in different scenarios, each solution has its adoptable point. If there is only one 10G device that needs to connect the switch, using a QSFP+ to SFP+ adapter is more appropriate. Or there are multiple 10G devices in dispersed locations that need to connect to 40G switches. In this case, the adapter also offers a cost-effective solution. However, if the distribution of these 10G devices is rather concentrated, QSFP+ breakout cables will be better for an optimal ROI.

 

Conclusion:

Although QSFP-SFP10G-CVR modules can just perform a single 10G connection and may cost more for the exclusive patent by some vendors, they are the optimal choice for converting 40G ports to the 10G ports after launch. With QSFP-SFP10G-CVR adapter, which supports all SFP+ cables and is compatible with mainstream switch models and SFP+ modules, smooth connectivity between devices that use 40G QSFP+ port and 10G SFP+ port will be realized.

 

Related Article:

40G QSFP+ to 10G SFP+ Configuration Guide

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.9k