English

Similarities and Differences Between Router and Gateway

Posted on Jul 20, 2021 by
73.7k

The backbone of Internet communication relies on the nuanced operation of various technological components. Within this network architecture, routers and gateways often surface as pivotal elements that keep digital traffic in orderly lanes. They are seen as synonyms all the time and do have something in common here. However, you also need to get a general idea about the differences between gateway and router from now on. Let's find the answers in this article that discussed gateway vs router and their major similarities and differences.

What Is a Gateway?

As the name implies, a gateway is a network entity, also known as a protocol converter. It connects the computers of one network to another and defines the boundaries of the network. If two networks with different protocols want to be connected to each other, both networks need to have gateways that provide a point of presence and entry for computers from both networks to communicate. In other words, gateways can join different systems.

Network gateways exist in routers, switches, or PCs. When communication is carried out within the same network segment, there is no need to involve the gateway. Only when the host communicates with devices outside this network segment, all packets need to be sent to the gateway device and then forwarded through the processing protocol of the gateway device.

Figure 1: powerful security provided via gateway

What Is a Router?

An internet router is a switching device that is responsible for receiving, analyzing and forwarding the data packets from the network to connected computers. A home router connects to the modem and acts like a traffic director on your local network, which connects your devices via WiFi signal or Ethernet, tunneling information between them and out to the modem. And the enterprise router has more powerful functions than a home router such as VPN service and flash memory, etc. Besides, there are wired and wireless router options available.

the application of the router

Figure 2: the application of the router

Gateway VS Router: What Is the Similarity?

The similarity between gateways and routers lies in their principal function: directing traffic. Both serve as distribution and directing points in a network. Whether a device is a gateway or a router, its primary role is to ensure that data gets from one point to another over networks. They are integral in managing network traffic, controlling the paths that data packets travel, and ensuring that communication between different networks is possible. Sometimes, a network may use routers both as end-point and access-point, in this case, the router becomes a gateway.

A gateway device often works with a router and a switch to complete the routing process. When a gateway receives a packet, it translates the protocol, and the router directs it to the next router.

It must be pointed out that network cards have to be inserted into both gateways and routers to facilitate this communication and virtually all routers and gateways have this setup shipped out of the factory without requiring the user to buy a separate network card.

Gateway VS Router: What Is the Difference?

Within the realm of networking, the difference between gateways and routers is significant. A router functions as an advanced network layer device responsible for managing and routing data packets across network devices, which is essential for effective Internet communication. In contrast, a gateway acts as pivotal hardware connecting and facilitating traffic between disparate networks, essentially serving as the doorway for data interchange. Besides, routers and gateways are very different in their working principle.

Before arriving at the router, packets go to the gateway channel first, and the network gateway checks the header information at once. After checking for any kind of error in the destination IP address and packet. According to the needs of the destination network, it carries out data conversion and protocol conversion on the packet, which is also the most critical step. Finally, the processed packet is forwarded to the router to establish intelligent communication between the two different networks.

The internet router extracts the destination address from the received packet, determines the network number in the address, and then looks up the routing table to find the entry matching the destination network. The routing table determines the next stop, destination, output interface, and other routing-related parameters that match the current packet. Finally, the packet is sent to the computer with the best route.

In layman's terms, gateways and routers are like the gates and elevators of a castle. When outsiders want to enter the castle, they must first pass the inspection and arrangement through the gate, so that they have the same characteristics as other people in the castle, and then they can be sent to the elevator. Then the elevator headquarters will choose the fastest elevator for them according to the characteristics and purpose of these strangers and finally, arrive at the destination.

Router and gateway differ in other ways besides their definitions and working principles:

Differences Router Gateway
Function To ensure that data packets are switched to the right address with the best route To connect two networks of different protocols as a translator
Networks It routes the data packets via similar networks It connects two dissimilar networks
Support Dynamic Routing Yes No
OSI Layer Work on layer 3 and layer 4 Work on layer 5
Additional Features wireless networking, static routing, NAT, DHCP server, etc network access control, protocol conversion, etc
Hosted On dedicated appliance (router hardware) dedicated/virtual appliance or physical server

Table: the differences between routers and gateways

Conclusion

In summary, gateways vs routers are pivotal to the functioning of today's interconnected networks, but they serve different and vital roles. The relationship between them is summed up in one sentence: a gateway is a concept while a router is a device that implements a gateway. If your devices are on the same network, then routers and gateways can be peer-to-peer. But if you want to connect two different networks with different protocols, the gateway can suit your demands. Some routers and gateways in the market can already replace each other, and the technology and capabilities will continue to evolve and become more sophisticated over the next few years.

 

Related Articles:

Is Enterprise Router Better Than Home Router

Different Types of Routers in Networking

How FS Security Gateway Ensures Enterprise Network Security

How FS Security Gateway Helps to Optimize Network Performance

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k