English

3 Tests That Matter to Fiber Patch Cable Quality

Updated on Apr 12, 2021 by
8.0k

To provide customers with high-quality fiber patch cables, manufacturers carry out a series of tests during the designing and manufacturing process. These optical fiber tests are critical for nearly every type of fiber network. It is necessary for not only vendors but also end users to learn what these tests are to know fiber patch cable quality and then decide the feasibility in your application. This post is going to introduce the three tests: 3D metrology, insertion loss (IL) test & return loss (RL) test, and endface clarify, which provide end users with confidence that the quality cables are high-quality and address their importance to fiber patch cables.

1. 3D Metrology Test: Guarantee of High-Quality Connector Endface

3D metrology test, or three-dimensional surface measurement, is a key test for controlling the performance of fiber optic connectors. In the production and functioning of fiber optic cable components, 3D interferometer, as the instrument to perform optical interferometry, plays an important role to enable vendors to inspect the fiber endface and control strictly the endface dimension. The three main properties measured are the radius of curvature, apex offset, and fiber height.

Radius of Curvature

As you can see in the image below, radius of curvature is the roundness of the ferrule’s endface. The radius of curvature of high-quality fiber patch cable connector endface should be controlled in a certain range. Too tight of a radius will put too much compression on the glass and too loose will put too much on the surrounding ferrule with not enough glass compression. Too much or too little radius can cause light scatter or inadequate physical contact for optimal signal transfer. Only a proper radius will allow for right compression and maximum performance.

3D metrology test radius of curvature.jpg

Figure 1: 3D metrology test: radius of curvature

Apex Offset

Apex offset refers to the linear distance between the highest point of polished ferrule endface and the center of fiber. It is a key term to amplify during polishing process. Incorrect polishing can be the reason for apex offset.


3D metrology test apex offset.jpg

Figure 2: 3D metrology test: apex offset

In theory, mated connectors with centered apex offsets should have perfect core-to-core connection, without any air gap. If there is a large apex offset, an air gap can be created, resulting in high IL and RL. Optical connectors with PC or UPC ferrules should set the apex offset at 0 degrees vertical angle during polishing. When ferrule is perfectly perpendicular to the polishing surface, the apex will be the exact center of fiber. APC ferrule is another case. The ferrule should be at an angle of 8 degrees to the fiber, instead of perfectly vertical. For more information about PC, UPC and APC polish styles, see PC vs UPC vs APC Connector: Selecting the Right Fiber Connector Type.

Fiber Height

Fiber height is the height that a fiber core extends from the ferrule surface. The fiber height should be not too high or too low. If too high, the fiber may bear the risk of being damaged when mated; if too low, gap will occur between the mated connector, resulting in increased insertion loss. Especially for those transmissions with stringent insertion loss requirements, gaps are certainly something you should avoid.


3D metrology test fiber height.jpg

Figure 3: 3D metrology test: fiber height

Standard 3D interferometer values are different in fiber modes and polish styles, thus the specific products should meet or exceed relevant industry-accepted endface geometry standards. The following chart is the endface geometry requirements of MTP single mode trunk cable connector based on IEC/PAS 61755-3-31 and IEC/PAS 61755-3-32.

Item Requirements
Ferrule X angle (SX) -0.2~0.2° (PC and APC)
Ferrule Y angle (SY) ±0.2°
Ferrule X radius (RX) ≥2000 mm
Ferrule Y radius (RY) ≥5 mm
Fiber Curvature Radius (RF) ≥1 mm
Fiber height (H) 1000~3000 nm
Max fiber height diff (HA) 500 nm
Max adjacent height diff (HB) 300 nm
Coplanarity ≤2000 nm
Core dip -100nm~+200 nm

2. IL & RL Test: Critical Measurement for Optical Deployment

IL, or insertion loss, is the loss of signal power resulting from inserting a device in a transmission line or optical fiber. RL, or return loss, refers to the loss of signal power reflected to the light source. In Reference to Insertion Loss and Return Loss for Fiber Connectors, IL and RL definition, the causes and tips for optimizing the values of the insertion/return losses are introduced.

No matter for the manufacturing process or installation, IL & RL test matters a lot. For optical cable vendors, the insertion loss and return loss tested should be conformed to a series of corresponding standards. For example, TIA standards specify a maximum fiber connector insertion loss of 0.75dB, which is considered as the worst-case situation. For most fiber connectors in the market, they have a range of 0.3dB to 0.5dB for standard loss and 0.15dB to 0.2dB for low loss. Manufacturers use IL & RL tester/meter to check if the values are within the normal limits so that the end-users could receive qualified products.

For end-users, apart from taking the IL & RL value written in the product specification lists for reference to design the optical link and choose other devices and assemblies based on the reference value, it is also possible to test by yourself if testing tools are available. It helps installers troubleshoot and identify faulty system components. OTDR, OFDR are frequently used techniques used for measuring return loss.

3. Endface Clarity: Necessary Inspection to Ensure Endface Cleanliness

We have talked about fiber cleaning a lot of times, to be more specific, the connector endface cleaning. Endface clarity is an essential procedure in optical fiber maintaining no matter 40 years ago or today. Manufacturers do endface inspection to confirm if there are contaminants, scratch or crack over the connector endface. Almost every fiber optic engineer has fiber optic cleaning testers/tools such as pen cleaner or cassette cleaner, which frequently appear while installing cables.


Endface clarify.jpg

Figure 4: Endface clarify

Why is it important to do endface clarity? The cleanliness and smoothness of the fiber optic connector endface is one of the basic and important procedures for maintaining quality fiber optic connections. It is different from any other kind of cleaning due to the deformation of connector endface and the particle contaminants reside on it. Even microscopic dust can increase return loss and even cause potentially permanent damage to connectors. Moreover, the dust between two endfaces can scratch the surfaces, causing an air gap or misalignment between fiber cores, which degrades the optical signal. Since these contaminants are so tiny to see without a microscope, if you mate a dirty plug, the other plug can also get contaminated. Therefore, even though vendors have done endface clarity during fiber optic connector testing, every time before connectors are mated or after they are un-mating, you should be diligent in inspecting endfaces and cleaning them. More information about connector cleaning is in this post: How Much Do You Know About Fiber Connector Cleaning?

Conclusion

In summary, the fiber optics industry improves the fiber connector quality by exploring the key parameters that need to be measured and industry associations and committees work to define the manufacturing criteria for fiber quality assurance. If the fiber patch cables have gone through these three tests above and the test results meet the standards, they will be competent to contribute to the high-quality optical transmission. For end-users, it is required to check whether vendors carry out these tests and affirm the test parameters with these test reports provided.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.7k