English

The Bandwidth and Window of Fiber Optic Cable

Updated on Apr 12, 2021 by
27.6k

For fiber optic cable, theoretically speaking, its bandwidth is infinitely high, transmission capacity is infinitely large and the transmission distance is infinitely far. Besides, optical fiber cable is also light in weight, and all of these features make it an ideal medium for data transmission, which is capable of transmitting unlimited telephone and TV signal. However, in the current application of optical cable, the result is far from the theory. Regardless of the fragile physical properties of silicon, the transmission capability of fiber optic cable has opened a few windows.

What Is the Bandwidth and Window of Fiber Optic Cable?

In May 2002, the ITU-T organization divided the fiber optical communication system into six bands as O, E, S, C, L and U6. Multi-mode optical fiber at 850nm is known as the first window,  single-mode optical fiber at O band is referred to as the second band. C band is called as the third window, L band is the forth window and E band is the fifth window. The following table shows the  wavelength bands for both multimode fiber optic cable and single-mode fiber optic cable.

Frequency band Window Wavelength range (nm) Frequency range (THz)
/ 1 850(770-910) /
Original band 2 1260-1360 237.9-220.4
Extended band 5 1360-1460 220.4-205.3
Short wavelength band / 1460-1530 205.3-195.9
Conventional band 3 1530-1565 195.9-191.6
Longer wavelength band 4 1565-1625 191.6-184.5
Ultralength wavelength band / 1625-1675 184.5-179.0

The frequency range in the table above refers to the frequency of light. According to the formula  speed = wavelength x frequency, we can easily figure out the frequency of light. Its relation to the transmission loss of fiber optic cable and wavelength has been displayed as follow:

bandwidth of optical fiber

In the early days of fiber optic communication the LED was employed as a light source due to its low price. Multi-mode fiber optic cables that operate at 850nm and 1300nm became the first choice for building small network, while single-mode optical fiber cables, working at 1310nm and 1550nm with laser as the light source , were the foundation for constructing large network. If there were more windows available for single-mode optic cable, one fiber optic cable would achieve ultra high speed transmission by transmitting signals at different wavelength at the same time by employing WDM (wavelength division multiplexing) technology, thus maximizing the potential of single mode fiber. Telephone and network and be using at the same time via ADSL (asymmetric digital subscriber line) modem. That’s because voice and data use different frequency. And this principle is similar with WDM and ADSL technology, which are usually applied in main networks that require higher bandwidth.

The Bandwidth and Window of Fiber Optic Cable in Application

For intelligent building, the mainly adopted fiber optic cable are multi-mode optical cable which supports short distance transmission, such as multi-mode optical fiber cable that operates at 850nm or 1300nm with LED as the light source, or multi-mode optical fiber cable working at 850nm with VCSEL laser. Single-mode fiber optic cable is often adopted in buildings that with a longer distance to each other.

Intelligent building applications, fiber optic cable is often close to support multi-mode-based, such as multi-mode fiber optic cable with the emission wavelength of 850nm or 1300nm LED light source, or 850nm VCSEL laser wavelength. Single-mode used in long distance system buildings, single-mode fiber optic cable with emission wavelength 1310nm or 1550nm FP or DFB laser, means that most of the fiber optic cable is only open a window. Single-mode fiber optic cable works together with FP or DFB which transmit wavelength of 1310nm or 1550nm. That’s to say most optical cable only open one window.

Conclusion

Whether the transmission windows of fiber optic cable can be opened or not and how many windows can be opened will be subject to several factors as dispersion, loss, WDM as well as light source and network equipment. In the long term, fiber optic cables that supports multiple windows are bound to have stronger practicability, compatibility and scalability.

Related Article: How to Identify the Fiber Optic Cable Color Code?

Tags

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.7k