English

The Development of MTP Cables

Updated on Aug 4, 2022 by
1.3k

The development of cloud computing drives enterprises to deploy high-density data centers to meet their growing data transfer needs. In fact, the importance of fiber optic cables in data center deployments cannot be underestimated, as fiber optic cables are an integral part of every network infrastructure. Among most fiber cables, the emergence of MTP cables has gained wide acceptance in network deployment for their high flexibility, ease of installation and cost-effectiveness, etc. The following will focus on MTP cables and their development tread in data centers.

 

MTP Cables Basic Guide

MTP cable is short for Multi-fiber Termination Push-on and is a registered trademark of US Conec. As an advanced version of MPO cable, MTP cable supports 40G/100G transmission, accommodating 8/12/24/48 or more fibers in one MTP connector, with less space and better airflow conditions. What's more, MTP connectors are also compatible and intermateable with MPO connectors. Generally, there are three types of MTP cables: MTP trunk cables, MTP harness cables, and MTP conversion cables. All of them are suitable for high-density data center cabling networks, which also enable large-capacity and high-performance transmission. For more information about MTP cables, please read MTP® Connector: What Is It and Why to Use It?

MTP Cables

 

The Development Trend of MTP Cables

For a long time, cabling and wiring management has been an essential part of data center deployments. Actually, optical fibers have undergone several evolutions with the development of network infrastructure. Generally, the development of optical fiber connectors can be divided into two stages: In the first stage, operators choose to upgrade fiber optic connectors from traditional FC, ST, SC to LC, MTRJ with the goal of saving network infrastructure space. However, with the growth of data traffic and business, LC and MTRJ connectors can no longer meet their demands for high-density transmission. Therefore, in the second stage of optical fiber development, operators turn to multi-core use with MU and MPO/MTP connectors.

MTP cables are increasingly playing an important role in data centers and enterprise networks. They can easily upgrade from current 40G/100G networks to 400G data centers with better performance and lower network infrastructure costs. The advantages of MTP cables are as follows:

  • Save space: With 16 multi-core fiber optic cables, data centers can achieve full utilization of fibers while deploying, which is very space-saving. In addition, MTP cables can accommodate 864 fibers, making them ideal for data centers with limited space.

  • Low insertion loss: Typically, the insertion loss of MTP cables is about 0.35db, which can be comparable to single fiber connectors.

  • Fast installation: Before the advent of MTP cables, the operators and installers usually spent a long time terminating and testing 144 fibers. Now, with the help of MTP cables, installers can connect 16-core or 24-core fiber connectors for 8-channel applications. They can also use pre-terminated plug-and-play cables, which makes it much easier to install and upgrade the cabling system.

advantages of MTP cables

 

Evolution Timeline of MTP Cables

As a high-density and low-insertion-loss cable, MTP has continued to evolve for over a decade. Below is the development timeline of MTP cables:

  • In 2004, the fiber count for the MTP connector was increased, allowing it to support packing up to 72 fibers into one format.

  • In 2005, multimode MTP Elite connectors were released, which enables fast system installation with lower-cost transceivers.

  • In 2007, the low insertion loss version of the multimode MTP Elite was released.

  • In 2010, the multimode version supports up to 24 fibers to be connected in one connector.

  • In 2012, the standards body approved the MTP format for use in data centers.

  • In 2013, the Industry standards body accepted the MTP format for transceivers.

  • In 2015, a new MTP 16 format was introduced that accommodates up to 16 fiber connections in a single row.

  • In 2016, the new MTP 16 will be available in a single-mode version.

 

The Next Generation of MTP Cables

As mentioned above, MTP cables show lots of advantages compared to other optical fiber cables. However, operators also encounter some challenges when deploying MTP cables in data centers. For instance, it's complicated for installers to distinguish the male and female connectors of MTP cables when dealing with thousands of fibers that not only transmit but also receive. These may increase the complexity of cable management and lead to deployment delays.

Despite all the challenges, MTP cables still enjoy a great reputation and promise in data centers and companies. In fact, the latest generation of MTP cables has overcome the difficulty of changing the gender and polarity of connectors, which makes it easier to configure the field. What's more, with a development history of more than 20 years, MTP cables continue to provide outstanding value for a wide range of networking technologies and always work as an indispensable part of data center deployments.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k