English

All About the Working Temperature of Optical Transceivers

Updated on Oct 7, 2021 by
11.6k

It's widely acknowledged that a qualified optical transceiver will undergo a series of rigorous tests before delivery. Evidently, temperature tests are considered as one of the important parts during the whole testing process. How to define the temperature of the optical transceivers? Why is the operating temperature important to the modules? What factors will have an impact on optical transceivers' working temperature? This article will clarify the above questions respectively.

Basics of Optical Transceivers Working Temperature

The temperature range of the optical transceiver determines the available temperature numerical value of the module. Different modules come with different temperature variants depending on their types, form factors, applications, and manufacturers. Conventionally, the fiber optic transceivers are categorized in three temperature levels in view of their applications in practice:


  • Commercial Temperature Range: 0 °C to 70°C (denoted by "COM")

  • Extended Temperature Range: -20°C to 85°C (denoted by "EXT")

  • Industrial Temperature Range: -40°C to 85°C (denoted by "IND")


Temperature Ranges of Optical Tranceivers.jpg

Generally speaking, fiber optic transceivers are mainly deployed in small-sized homes and offices, and large-scale data centers. However, it is likely to deploy the optical transceivers in some sparsely populated regions such as deserts, river valleys, oceans, mountains and so on. When purchasing, the parameter of the temperature range of the modules will be presented in the specification table. It's wise to select from the above mentioned three types of temperature ranges based on the specific application situations.

Why Optical Transceivers Operating Temperature Range Matters?

Each transceiver module comes with a vendor-defined operating temperature range. If the temperature goes too high or too low, i.e. exceed or beyond the normal temperature range, then the modules will fail to perform well or even won't operate normally. Consequently, there is a risk of leading delays or network breakdowns.

A Challenge From Higher Temperatures

High temperature has an effect on optical communication, so various methods have been created to tackle the heat issues—installing a cooling system in the data center and such. If you are considering conducting deployment in some severe environments, temperature is 100% non-negligible. When the operating temperature is too high, the module will counter a spike in optical power resulting in incorrect reception of signals and disordered operation. Or even worse, the module would be burned.

A Threat From Lower Temperatures

Normally, operating an optical fiber system will generate heat. Unlike the previous situations, operating at temperatures lower than the vendor-defined temperatures is seldom encountered in the data communications industry. If the operating temperature is too low, the function of the optical transceiver also will be unstable and abnormal. As a result, avoid installing commercial optical transceivers in an environment with a temperature below 0°C in most cases.

Note: Temperature monitoring and control system is recommended for the real-time monitoring and compensation, which ensures that the modules are operating with stable luminous power and correct module extinction ratio.

What Will Affect the Working Temperature Range of Optical Transceivers?

Unqualified Workmanship

Modules with low-quality materials and a poor built-in design will show more sensitivity towards temperature deviations, resulting in poor heat dissipation. The abnormal temperature of the transceiver will happen frequently. As a result, the unstable operation cannot be avoided. The key to solve this problem is not complicated at all. Find a trustworthy supplier that has a rigorous testing system of the temperature of the modules.

Second-hand Modules Reusage

As an alternative to some users, adopting used modules is considered to be "cost-effective." Indeed, the price of second-hand modules is lower and they might work normally in some situations. But it's still worth-mentioning that second-hand transceivers are more prone to temperature sensitivity issues because of some of their internal parts. If the working temperature range of a new module is 0-70℃, then the used module won't reach the level mostly. Once it works abnormally, the replacement and maintenance fee will be much higher than the money you've saved in the very beginning.

Summary

It's critical to maintain the operating temperature of the optical transceivers stable and within the range is critical, which benefits the daily operation. There is a tendency for more optical transceiver suppliers to provide various modules that accord with the temperature requirements. FS, keeping pace with the trends, provides various types of optical transceivers including commercial and industrial ones. Every single module experienced elaborate tests including temperature tests in the FS testing center to ensure high quality and performance.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k