English

Tutorial on Bi-Directional Transmission Technology

Posted on Aug 15, 2016 by
10.7k

Migrate to 40G With BiDi Technology

Tutorial on Bi-Directional Transmission Technology

Optical fiber communication has been showing a trend toward higher transmission capacities, larger transmission spans, higher flexibility and lower transmission costs during the past few years. Within this background, we had ushered in the era of bi-directional transmission technology, or BiDi technology for short.

BiDi Technology—Less Fibers for Faster Speed

For bi-directional transmission technology, “bi-directional” is meant in sense of using optical fiber in two directions, similar to the use of single railway track in two directions. BiDi technology allows transceivers to both transmit and receive data to/from interconnected equipment through a single optical fiber. In the early stage of optical fiber communication, one optical fiber transmits signals of only one wavelength, one optical fiber can only transmit signals of one wavelength. That means at least two fibers are needed to accomplish the full-duplex communication with one optical fiber transmitting Tx optical signals, and the other optical fiber transmitting Rx optical signals. This is the conventional two-fiber Bi-Directional communication. However, with the never insatiable need for more capacity and greater performance, the existing network resources are getting harder to manage it. To maximize the capacity and usage of optical fibers, BiDi technology cropped up, which can use one optical fiber to implement the transmitting and receiving of optical signals, thus saving optical fiber resources and doubling your network capacity.

Inside the BiDi Products

Currently, the main BiDi products are BiDi transceivers, which also referred to as WDM transceivers. Different from the common a two-fiber bi-directional optical transceiver, which is composed of TOSA and ROSA, the BiDi transceiver adopts BOSA to replace the TOSA and ROSA, achieving bi-directional transmission over a single optical fiber. BiDi transceivers split light into different wavelengths. They must work as a matched pair having the correct receive and transmit wavelength.

Inside the BiDi Products

Case Study: Migrate to 40G With BiDi Technology

The transition to 40G is in its full force, driven by the increasing demand for unimagined capacity and performance from the servers and data centers. It seems that these severs and applications can never be satisfied. For them, enough is never enough. Even if you have not prepared for a 40G Ethernet, you will need it very soon. However there exist some challenges for it.

Problems Facing 40G Migration

 10G SR transceivers operate over dual-fiber multimode fiber (MMF) with LC connectors. But 40G SR4/CSR4 transceivers operate over MMF ribbon with MPO connectors. As a result, 40G MPO-based SR4/CSR4 transceivers cannot reuse aggregation fiber infrastructure built for 10G connectivity.  The common 40G transceivers require 12 fiber strands in practice which are terminated by MTO-12 connectors. But we can see from the picture below that only 8 fiber strands carry traffic, causing 4 fiber strands unused and wasted.

Problems Facing 40G Migration

Solution With 40G QSFP BiDi Transceiver

To solve above problems, 40G QSFP BiDi transceiver based on BiDi transmission technology had emerged. It can transmits full-duplex 40G traffic over one dual-fiber LC connector OM3 or OM4 MMF cable. So, it has the capability to reuse 10G fiber infrastructure. In other words, it enables data center operators to upgrade to 40G connectivity without making any changes to the previous 10G fiber cable plant, resulting in zero-cost cabling migration from direct 10G connections to direct 40G connections.

Solution With 40G QSFP BiDi Transceiver

Present Application and Future Prediction of BiDi Technology

Currently, BiDi technology is widely adopted by enterprises to get upgraded to 40G performance, for it can save a huge cost, whether for upgrading the current data center or building a new one. The table below shows the costs and savings of migration and new deployment of 288 direct connections with 40G BiDi technology.

Present Application and Future Prediction of BiDi Technology

From the table, we can see that with such a huge saving for a data center migration or expansion, 40G BiDi transceivers based on BiDi technology will continue to gain popularity in 40G Ethernet. Since the market for 40G BiDi is broad, have you ever thought about 100G BiDi? Will there be 100G BiDi transceivers in the future? 100G Ethernet is racing to us, and the discussion of 200G and even 400G Ethernet has started heating up among data center professionals. Under this circumstance, there has been talk that a 100G BiDi optic will be available soon to the market, and I believe that should happen sometime this year. There is no standard for 100G BiDi right now, but we can still predict that the 100G BiDi will utilize an LC connector running on duplex signals. The unknown is the distance it will run on OM3/OM4 glass.

Application Precautions

 BiDi transceivers must work as a matched pair having the correct receive and transmit wavelength. Pay attention to the color of pull taps on optical modules. An optical module with the yellow pull tap needs to be used with an optical module with the blue pull tap. Optical modules with pull taps of the same color cannot be used together.  No standard has been released for BiDi transceivers. The wavelengths supported by BiDi modules from other manufacturers may differ from each other. Therefore, the BiDi transceiver from one manufacture may not interwork with optical modules from other manufacturers.  Before BiDi transceivers are used, it is recommended to make a unified planning, for example, to determine the wavelength for upper layer devices and the wavelength for access devices, so as to prevent inter-working failures because of wavelength differences during implementation.

Summary

The obvious advantage of utilizing BiDi transceivers is the reduction in fiber cabling infrastructure costs by reducing the number of fiber patch panel ports, reducing the amount of tray space dedicated to fiber management, and requiring less fiber cable. Although BiDi transceivers cost more compared with traditional two-fiber transceivers, the cost savings of utilizing less fiber is more than enough to offset the higher price of them. And the 100G BiDi transceiver will run to us sooner or later, which may become the most economical and efficient choice for your fiber optic network. Let’s wait and see.


You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.7k