English

A Comprehensive Understanding of Tunable DWDM Transceiver

Updated on May 4, 2023 by
12.6k

Tunable DWDM transceivers allow users to tune their wavelengths based on actual network demand. This results in a reduction in the number of spare transceivers that are used for avoiding DWDM network breakdown, and offers flexibility to adapt to the growing network. On the market, tunable modules mainly include 10G SFP+, XFP, and 25G SFP28 tunable DWDM transceivers. Then, are there any differences between the tunable 10/25G and standard 10/25G DWDM modules? This post will explain their differences in working principle, application, and cost, then use the FS box to show how to change the wavelength of the DWDM tunable transceiver.

Tunable DWDM vs Fixed-wavelength DWDM Transceiver

In DWDM transmission, tunable DWDM transceivers allow for wavelength adjustments within a certain range, providing flexibility and scalability, albeit at a higher cost and complexity; whereas fixed-wavelength DWDM transceivers operate stably on specific wavelengths, offering simplicity, reliability, and lower costs, albeit with limited flexibility. The choice depends on network requirements and cost considerations.

Working Principle

Each fixed-wavelength DWDM module is designed with a specific wavelength, so the module can only be deployed in the network node that requires the corresponding wavelength. For example, an SFP+ transceiver with C21 wavelength can only work with the port of C21 wavelength on a DWDM MUX. However, with the tunable SFP+ fiber module, users can use the module to connect any ports of the same DWDM MUX through fiber cables since the wavelength of the tunable transceiver can be tuned to adapt to the different port wavelengths.

Application

With different working principles, standard DWDM optical modules are traditionally deployed in networks that require little channel change or addition. Since tunable DWDM transceivers can be adjusted to operate on different wavelengths, they offer scalability and versatility in network design. Operators can add or modify wavelengths without needing to change hardware.

Cost

The cost of an individual fixed-wavelength transceiver is indeed lower than a tunable DWDM module. But in the long run, tunable optics will reduce OPEX. For example, in a large 10G SFP+ DWDM system that includes more than hundreds of nodes with different wavelengths, users have to provide up to hundreds of backup standard DWDM SFP+ transceivers to avoid unnecessary breakdown, which will greatly increase the operating cost. In this case, tunable optics help reduce the demand for DWDM SFP+ transceiver inventory, which will reduce the cost and maximize network flexibility.

Use FS BOX to Tune Wavelengths of Tunable DWDM Transceiver

FS box can tune the wavelengths of tunable transceivers. It’s a device used to solve real-time compatibility needs and upgrade the transceiver firmware (visit FS Box Introduction to learn more). All the operations can be done on the FS Box Smart Cloud Platform after plugging the fiber module into the corresponding port of FS box. Users can find information about their plugged tunable transceiver on the page, including its current wavelength. They can select any available wavelength from the dropdown menu. Then, click“start”, and the tuning will be done. The following video shows the ways to check and tune the wavelength of an SFP+ tunable DWDM transceiver.

 

Tunable DWDM Module FAQ

1. 10G Tunable XFP vs SFP+ DWDM tranceiver, is there any difference?

Tunable SFP+ DWDM modules comply with SFP+ MSA, while 10G DWDM XFP optical modules use XFP MSA standard (check tunable DWDM Transceiver Datasheet to learn more). The size of SFP+ is smaller than 10G XFP. Users can choose a suitable 10G tunable module based on the ports of their devices. Note that, on the market, SFP+ is the mainstream design in the 10G network.

2. Are the wavelengths of tunable DWDM module and fixed-wavelength DWDM module the same?

Tunable DWDM transceiver module runs on 50GHz C band wavelength with 0.4nm spacing. And it usually supports channels from C16 to C61. But this depends on the network switch or router manufacturers (like Cisco, Juniper) and which channels it supports. Standard DWDM transceiver support 50GHz (0.4nm spacing) and 100GHz (0.8nm spacing) C band wavelength. And since the channels of 50GHz include the 100GHz channels, it means that tunable DWDM with 50GHz can work on 100GHz wavelength. Therefore, there is no big difference between them.

3. How compatible are Tunable DWDM transceivers? 

Tunable DWDM modules are typically compatible with standard DWDM systems but require ensuring interoperability with existing equipment and network elements. Thorough testing and validation should be conducted before deployment.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k