English

What Are the Main Internal Components of Optical Transceivers?

Updated on Oct 7, 2021 by
10.0k

As a key element in optical communication systems, optical transceivers serve as media between network devices to transmit and receive data. There has been lots of articles and guides on transceiver modules in the perspective of the package type while only a few of them cover the internal elements. This post is going to elaborate the main internal components of optical transceivers.

Internal Components of Optical Transceivers

The main components of an optical transceiver can be generally divided into three parts: the externally visible housing, optoelectronic devices and PCBA. Uncover the metal casing of a transceiver module, you will find the inside components and sub-assemblies joint together.

Optoelectronic Devices

Optoelectronic devices are the core components of an optical transceiver module. For transceivers designed for diverse applications, the optoelectronic devices are not the same.

TOSA and ROSA in General Optical Transceivers

For general optical transceivers, there are two optoelectronic devices called TOSA and ROSA, each performing the exact reverse functions for their purposes.


  • What is TOSA?

TOSA stands for Transmit Optical Sub-Assembly, which bears the responsibility of converting an electrical signal into an optical signal. It is made up of light source (light emitting diode or laser diode), optical interface, monitor photodiode, metal and/or plastic housing, and electrical interface. However, the assembly units are not immutable. In accordance with the transmission distance or application of the optical module, there may be other components such as filter elements in TOSA.

Nowadays the majority of optical modules use laser diode (LD) as light source. Compared with light emitting diode (LED), LD has lower power consumption, higher output and higher coupling efficiency. Even though LED in small quantities is still in use of low speed and short distance transmission owing to its advantage of low cost and long service life. Figure 1 shows the basic structure of a typical TOSA with LD.

Figure 1 What is TOSA.jpgFigure 1: What is TOSA?


  • What is ROSA?

ROSA refers to Receiver Optical Sub-Assembly, the primary function of which is to convert the optical signal transmitted from TOSA into electrical signal. ROSA contains a photodiode (PD), optical interface, metal and/or plastic housing, and electrical interface. Like TOSA, the concrete components of ROSA depends on specific functionality and application of the transceiver. Other components such as amplifier may be included, aiming to reshape input signals degraded by long-distance transmission. The preamplifier converts a current signal to a voltage signal and amplifies the signal to a high voltage gain, while the post-amplifier equalizes the output signal of the preamplifier to an amplitude level suitable for input to the following digital circuit. The following picture indicates the principle of ROSA including Avalanche Photodiode (APD) and Transimpedance Amplifier (TIA).

Figure 2 What is ROSA.jpgFigure 2: What is ROSA?

A pair of ROSA and TOSA are combined together inside a transceiver, forming the main transceiver elements and enabling transmitting as well as receiving.

BOSA in BiDi Transceivers

BOSA is short for Bi-Directional Optical Sub-Assembly. It is apparent that BOSA has something to do with BiDi transceivers just as the name indicates. BOSA generates with the development of optical transceiver manufacturing technology. As the transceivers are made much smaller, TOSA and ROSA can be integrated during the coupling process. BOSA are integrated by TOSA, ROSA and a WDM filter, enabling it to support two wavelengths on a fiber using bidirectional technology.

PCBA

What Is PCBA?

PCBA is the abbreviation of Printed Circuit Board Assembly. It can be also called PCB Assembly or Printed Circuit Assembly. Surface Mounted Technology (SMT) and Dual In-line Package (DIP) are both common methods used in PCB Assembly. Generally, PCB bare board passes through the SMT upper part, and then passes through the entire process of the DIP plug-in. Active and passive electronic components are soldered onto the printed circuit board then the PCBA can be used in a transceiver. PCBA performs the functions of assuring integrated circuits and other electronic components fixed, ensuring the quality of the electronic equipment, and so on.

Difference Between PCB and PCBA

Simply speaking, the main difference between PCB and PCBA is that PCB is a bare board but PCBA is a finished one. PCB, which means Printed Circuit Board, is a carrier for electrical connection of electronic components. PCBA is a completed assembly, which is to say, apart from PCB, there are other parts that are assembled onto the PCBA. After the process of assembling PCB with Surface Mounted Technology (SMT) or something else is finished, PCBA is completed.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.2k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.7k