English

What Is 25GBASE-T?

Updated on Mar 14, 2020 by
13.7k

25GBASE-T, or 25G Ethernet over twisted-pair, has become a sought-after technology over the past few years driven by cloud computing. With 25Gbps on a single channel, 25GBASE-T can also be a viable solution to meet the ever-higher demands for bandwidths, making it especially suitable for data centers and server rooms. This article will give an all-round introduction of 25GBASE-T.

25GBASE-T Standard and Technology

The 25GBASE-T standard was developed by IEEE 802.3 Task Force 802.3bq in 2016, which uses all twisted-pair cabling to support data transmission up to 25Gbps.

NameStandardMediaMedia CountGigabaud per laneReachRS-FEC (802.3by CL 108)
25GBASE-T802.3bq (CL 113)Cat 8 balanced twisted-pair structured cabling4 pairs2.00030 mNo

Table 1: 25GBASE-T Standard

25GBASE-T technology can be built on the well-established 10GBASE-T technology and developed to support 40GBASE-T. Comparing 10GBASE-T, 40GBASE-T, and 25GBASE-T transmission parameters in table 2, including baud rate, cancellation, relative signal-to-noise (SNR) margins, it demonstrates that the complexity of 25GBASE-T cabling over 30m resembles 10GBASE-T cabling over 100m. And the Channel row also indicates that 25GBASE-T follows the 30m-channel design of the earlier developed 40GBASE-T technology, largely reducing the complexity of 25GBASE-T equipment and minimizing time to market. In addition, SerDes (Serializer/Deserializer) technologies have already been widely available for 25GBASE-T. And technologies such as single-lane of 100GBASE-T 4-lane PMD (Physical Medium Dependent) and CAUI-S (Gigabit Attachment Unit Interface) specifications, as well as SFP28 can be reused in 25GBASE-T.

Parameter10GBASE-T (ref-CI55)40GBASE-T (ref-CI 98d1.0)25GBASE-T (example)
Channel100m, CI55.7 (e.g., Cat6a)30m, CI 98.7d1.0 (e.g., Cat8)30m, CI 98.7d1.0 (e.g., Cat8)
Baud (MHz)80032002000 (example)
RX_ENOB (bits)9.5-107.86.5-7.5
Channel IL (dB, Nyquist)46.929.422.6
Channel round trip (baud)8801056660
Echo Cancellation (dB)5547 (-6dB) to 5543 (-12dB) to 55
Next Cancellation (dB)4034 (-6dB) to 4028 (-12dB) to 40
FEXT Cancellation (dB)2522 (-3dB) to 2519 (-6dB) to 25
Relative SNR Margins (dB)0 (ref)+2.7dB to 0.2dB+8.7dB to +4dB

Table 2: 25GBASE-T vs 10GBASE-T vs 40GBASE-T

25GBASE-T Benefits

Why is 25GBASE-T so well-received within such a short period of time? The main reasons are the following 25GBASE-T benefits.

Excellent Switch I/O Performance and Fabric Capability

25GBASE-T allows bandwidth capacity to be scaled cost-effectively so as to support next-generation server and storage solutions for cloud and web-scale data centers. Through 25GBASE-T, these data centers can achieve 2.5 times the network bandwidth performance of 10GBASE-T. Transmitted across a single channel, 25GBASE-T also provides 4 times the switch port density per switching chip and network scalability of 40GBASE-T requiring 4 channels to fully utilize the port capabilities.

Practical Auto-Negotiation and High Compatibility

25GBASE-T enables switch ports to automatically link at different speeds, simplifying network upgrades and reducing connectivity costs with an industry-standard interoperable specification, which makes 25GBASE-T easier enter in the early market occupied by the existing devices. The commonly interoperable systems are 10GBASE-T, 40GBASE-T, 50GBASE-T, 100GBASE-T. 25GBASE-T offers backward compatibility with 10GBASE-T and potential forward compatibility through auto-negotiation, undoubtedly increasing connectivity efficiency and saving costs.

Flexible Topology

25GBASE-T PHY (Physical Layer) can support a much broader range of topology architectures than 25G over Twinax DAC (direct attach copper) connections to easily facilitate all types of cabinet-to-cabinet, (Middle of Row) MoR, and (End of Row) EoR switch-to-server structures, which is attributed to the longer transmission distance of 25GBASE-T. And many large cloud data centers see as an advantage for managing switches in hundreds of racks. Limited to about 5 to 7m, 25G DAC cables are primarily targeted to ToR (Top of Rack) topologies where switches connect directly to servers in the same cabinet.

25GBASE-T Topology.jpg

Figure 1: 25GBASE-T Topology

Lower Costs

25GBASE-T can reduce capital expenditures (CAPEX) and operating expenses (OPEX). Utilizing a 1x25Gbps channel, 25GBASE-T enables a simple and seamless 10G-25G-100G migration path compared with the traditional 10G-40G-100G path. In addition, the 10G-25G-100G path also avoids rewiring and network redesign, significantly cutting down the required number of switches and cables, namely CAPEX. As to the OPEX, 25GBASE-T offers superior switch port density by requiring just one channel compared with the four-channel 40GBASE-T, which brings lower power requirement and lower cost per unit of bandwidth.

25GBASE-T Application

As mentioned earlier, the application advantage of 25GBASE-T lies in its 30 m reach zone over the same Cat8 cables as 40GBASE-T, filling the gap for longer distances to support MoR and EoR connections and making it popular in cloud data centers for switch-to-server applications. Read this article for more details: Cat8 Cable for 25G/40GBASE-T Network. It is shown that 25GBASE-T can work anywhere in data centers, including fat tree, leaf and spine architecture, interconnected fat tree fabrics, traditional three-tier architecture, for full-mesh, interconnected mesh, and centralized switching.

25GBASE-T Switch-to-Server Connection.jpg

Figure 2: 25GBASE-T Switch-to-Server Connection

Conclusion

Nowadays 25GBASE-T has gained more and more attention, as it offers excellent network bandwidth performances and high scalability with good compatibility. It also enables a more cost-effective path for network migration to 100G and ever higher speeds without rewiring. And 25GBASE-T is suitable for MoR and EoR architectures while saving considerable costs for cabling and management. All in all, 25GBASE-T is an optimal solution for cloud data centers and server rooms.

Related Article:

25G Direct Attach Cables (DAC & AOC) Overview

25G SFP28 Transceiver Module Overview

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.9k