English

Cloud Server vs Dedicated Server: Which One to Choose?

Posted on Jun 16, 2022 by
3.7k

FS Rack Servers

As digital transformation takes shape and businesses face increasing market demands, many are rethinking their hosting plans to ensure reliable and scalable infrastructure that meets their current and future data needs.

Cloud servers and dedicated servers are two popular choices if you are looking for top-tier performance and uptime, but these hosting models excel at different use cases. Which one is the right option for your business needs?This article explains the difference between cloud and dedicated servers and outlines the features of both hosting types. We provide all the info you need to make an informed decision and identify the hosting option that fits your use case, business needs, and budget.

Cloud Server vs Dedicated Server: Definitions

Cloud Servers

A cloud server is a virtual server running in a cloud computing environment. These servers provide users with on-demand virtual resources and offer unrivaled scalability (both up and down).

Clients that rely on a cloud server do not need to buy or maintain any hardware. The cloud provider handles maintenance while users adjust virtual resources (processing, RAM, storage, etc.) to create an optimal configuration.

Dedicated Server

A dedicated server is a remote or physical server set aside specifically for an organization, individual, or application. These servers are highly customizable and offer businesses several choices for hosting and managing site traffic. Such as the RS3110 offered by FS, a 1U rack server, offering a range of pre-configured and customizable options to meet the needs of modern and growing businesses.

You can use this server to host services and applications or for data storage and backup services. And since this server isn't shared, you may also use it internally for hosting and provisioning special services, e.g., implementing network and dedicated file servers.

 

     ''Also Check- FS RS3110 Server

 

What Are the Differences Between Cloud Server and Dedicated Server?

Cloud servers and dedicated servers are common hosting choices for companies looking for high reliability and performance. While the two hosting models rely on different infrastructures, both server types perform the same basic functions as they can store data, receive requests for the stored info, process requests and return data back to the user. But there are many differences between them.

Performance

Companies that require consistent high performance tend to run on dedicated physical servers. Dedicated servers offer unrivaled processing speed as the units process data locally, so there is virtually no delay in retrieving and processing information and dedicated resources ensure that there are no delays due to queuing of requests. Dedicated servers are ideal for microsecond computing use cases such as heavy computing or high frequency trading. Compared with dedicated servers, cloud servers have too many data resources, and there may be a little delay.

Management

In terms of maintenance and management, cloud servers are relatively simple. Customers have no hardware maintenance, they just need to have multiple dashboards and tools. These dashboards and tools extend setup, monitor devices, enable performance alerts on individual components, and create cloud-based backups.

Most different from cloud servers, dedicated servers require advanced expertise for proper maintenance and management. Responsible teams must monitor servers for potential risks. In the event of a failure, the IT team must keep the setup up-to-date with the latest patches, replacing faulty IT parts and minimizing server slowdown and downtime. There are servers with remote management and software monitoring capabilities that can track status in real time to monitor applications on the server, perform troubleshooting and enforce a robust backup strategy. Take FS servers as an example, the servers are equipped with Integrated BMC Management and IPMI2.0, which can realize the stable operation of the server.

 

     ''Also Check- FS Servers

 

Security

Cloud servers are not an insecure type of hosting if you choose the right carrier. Still, you'll be sharing the environment with unwitting tenants, so some concerns about data privacy are warranted. Dedicated servers offer unparalleled data privacy as a single tenant uses the hosting environment. You don't have to worry about other users, but you have to do it yourself to ensure security.

Cloud Server vs Dedicated Server: How to Make a Choice?

Once you understand your business needs, you can consider what server type you should use. Both cloud servers and dedicated servers come with a line of benefits, but each type excels at different use cases.

Advantages of Cloud Servers

  • E-commerce sites with seasonal surges in traffic.

  • Small business apps with unpredictable usage levels.

  • Email servers.

  • IaaS, PaaS, or SaaS offerings.

  • Apps that require rapid server deployments.

  • Systems that need uninterrupted hosting.

Advantages of Dedicated Servers

  • Large websites with high traffic and a huge user base.

  • Apps that require high CPU processing, RAM, and disk space (multiplayer game servers, big data analytics, database hosting, etc.).

  • Stable apps that are unlikely to see usage spikes.

  • Systems that host sensitive data.

dedicated servers

Summary

To sum up, there are many differences between cloud servers and dedicated servers, but each has its own advantages. Cloud servers excel in deployment time and scalability. But for businesses that require complete control and high performance requirements, a dedicated server is the ultimate solution. With the continuous development of data centers, the current market demand for dedicated servers is also stronger. Based on this, FS provides standard and customized servers, and you can customize server accessories according to your actual needs and enjoy free professional technical support.

You might be interested in

Knowledge
See profile for John.
John
Guidelines for Organizing Server Rack
Mar 11, 2021
67.4k
Knowledge
See profile for Rameez Arif.
Rameez Arif
How to Choose the Right Data Center Server Rack Size
Aug 27, 2022
12.0k
Knowledge
Blog
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge