What Is A Wireless Network?
wireless network, also known as a Wi-Fi network, has become an essential part of our modern-day connectivity. Wireless networks have become ubiquitous, appearing at every corner we turn, from residential routers to mobile phones. It has revolutionized the way we access the internet and communicate with devices and each other. In this article, we talk about the concepts, types, and components of wireless networks as well as their ways of working.
What Is A Wireless Network?
A wireless network is a computer network that utilizes radio waves as a means of communication between devices, eliminating the need for wired connections. The term "wireless" signifies the absence of physical connections, such as cables, between devices within the network. Instead, devices exchange information by transmitting and receiving radio signals wirelessly. This technology has gained significant popularity due to its ability to provide mobility within a home environment, eliminating concerns about tripping over cables. Wireless networks offer numerous advantages, including enhanced mobility, flexibility, and simplified installation processes.
Types of Wireless Network Connections
Apart from a local area network (LAN), there are several other prevalent categories of wireless networks, such as a personal-area network (PAN), a metropolitan-area network (MAN), and a wide-area network (WAN).
-
LAN: The most prevalent form of wireless networking is known as Local Area Networking (LAN). It links multiple computers within a single building or a small cluster of buildings. For instance, in an office building, different offices can be connected through a local area network, enabling file and printer sharing among them.
-
PAN: Another type of wireless networking is Personal Area Networking (PAN). It establishes connections between one or more portable electronic devices, such as cell phones, PDAs, digital cameras, and video game consoles. PANs can range from simple setups involving communication between two devices to complex systems that facilitate communication among thousands of devices.
-
MAN: A Metropolitan Area Network (MAN) connects numerous computers situated in diverse locations across a city or region. These networks typically have a central hub that coordinates communication between individual nodes.
-
WAN: A Wide Area Network (WAN) interconnects computers over a large geographic area, spanning countries or even continents. The Internet is a prime example of this type of network.
The Components of A Wireless Network
A wireless network comprises various components:
-
Clients: These are the devices we commonly consider as end-user devices, referred to as "clients." With the expansion of Wi-Fi, a wide range of devices utilize Wi-Fi for network connectivity, including phones, tablets, laptops, desktops, and more. This allows users to move freely within the coverage area without losing their connection to the network. In certain scenarios, such as in offices or warehouses, mobility is essential. For instance, employees may need to use scanners to register packages for shipping, and a wireless network provides the necessary flexibility for them to move around the warehouse.
-
Access Point (AP): An access point (AP) serves as a Wi-Fi transmitter that broadcasts a network name known as a Service Set Identifier (SSID). Users connecting to this network typically have their traffic bridged to a local-area network (LAN) wired network, such as Ethernet, enabling communication with the larger network or even the Internet./p>
How Does Wi-Fi Network Work?
A wireless network based on Wi-Fi technology transmits signals through radio waves, which differ in frequencies and modulation compared to cellular phones and radios. In a typical Wi-Fi network, the Access Point (AP) broadcasts a specific network that provides connectivity. This network is identified by a Service Set Identifier (SSID), visible to users when they view the available networks on their smartphones or laptops. The AP communicates this information through beacon transmissions, which can be seen as announcements saying, "Hello, I have a network here. If it's the network you're looking for, you can join."
When a client device receives the beacon from the AP, it converts the radio frequency (RF) signal into digital data, which is then interpreted by the device. If the user wishes to connect to the network, the device sends messages to the AP in an attempt to join, and when security measures are enabled, it provides the appropriate credentials to authenticate its access. These processes are known as Association and Authentication. If either of these processes fails, the device cannot successfully join the network and cannot communicate further with the AP. Assuming successful association and authentication, the ultimate goal for the end user is to transmit data. Data from the client device (or from the AP to the client) is converted from digital format to an RF modulated signal, which is then transmitted over the air. Upon reception, the signal is demodulated, converted back to digital data, and forwarded to its destination, often the internet or a resource on the larger internal network.
Wi-Fi communication operates within specific frequency bands approved for transmission, primarily the 2.4 GHz and 5 GHz bands in most parts of the world, with some countries adding the 6 GHz frequencies as well. These frequency bands differ from those used by cellular networks, meaning Wi-Fi and cell phones do not compete for the same frequencies. However, it's important to note that other technologies can operate within these bands. For instance, the 2.4 GHz band accommodates various products, including Bluetooth, ZigBee, cordless keyboards, and audio/video equipment, which can cause interference.
To sum up, whether it's accessing the web on our smartphones, streaming content on our tablets, or connecting smart devices in our homes, understanding the concept of a wireless network is crucial in navigating the digital world we live in.
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023