English

What Is Software-Defined Networking (SDN)?

Updated on Jun 1, 2022 by
10.3k

The advent of Software-Defined Networking (SDN) has revolutionized the way data centers operate, offering enhanced flexibility, scalability, and control. In this blog post, we will explore the concept of SDN, how it functions, its various types, and the benefits it provides in comparison to traditional networking approaches.

 

What Is SDN?

SDN, short for Software-Defined Networking, is a networking architecture that separates the control plane from the data plane. It involves decoupling network intelligence and policies from the underlying network infrastructure, providing a centralized management and control framework.

 

The Importance of SDN in Data Center

In modern data centers, where agility and efficiency are critical, SDN plays a vital role. By virtualizing network resources, SDN enables administrators to automate network management tasks and streamline operations, resulting in improved efficiency, reduced costs, and faster time to market for new services.

 

How does SDN Work?

SDN operates by employing a centralized controller that manages and configures network devices, such as switches and routers, through open protocols like OpenFlow. This controller acts as the brain of the network, allowing administrators to define network behavior and policies centrally, which are then enforced across the entire network infrastructure.

SDN network can be classified into three layers, each of which consists of various components.

  • Application layer: The application layer contains network applications or functions that organizations use. There can be several applications related to network monitoring, network troubleshooting, network policies and security.

  • Control layer: The control layer is the mid layer that connects the infrastructure layer and the application layer. It means the centralized SDN controller software and serves as the land of control plane where intelligent logic is connected to the application plane.

  • Infrastructure layer: The infrastructure layer consists of various networking equipment, for instance, network switches, servers or gateways, which form the underlying network to forward network traffic to their destinations.

Software Defined Networking (SDN) Layer

To communicate between the three layers of SDN network, northbound and southbound application programming interfaces (APIs) are used. Northbound API enables communications between the application layers and the controller, while southbound API allows the controller communicate with the networking equipment.

 

Types of SDN

Depending on how the controller layer is connected to the SDN devices, SDN network can be divided into four different types which we can classify as follows:

Open SDN

Open SDN has a centralized control plane and uses OpenFlow for the southbound API of the traffic from physical or virtual switches to the SDN controller.

API SDN

API SDN, is different from open SDN. Rather than relying on an open protocol, application programming interfaces control how data moves through the network on each device.

Overlay Model SDN

Overlay model SDN doesn't address physical netwroks underneath but builds a virtual network on top of the current hardware. It operates on an overlay network and offers tunnels with channels to data centers to solve data center connectivity issues.

Hybrid Model SDN

Hybrid model SDN, also called automation-based SDN, blends SDN features and traditional networking equipment. It uses automation tools such as agents, Python, etc. And components supporting different types of OS. Hybrid model SDN is often used as a phrase-in approach to SDN.

 

Benefits of SDN

Different SDN models have their own merits. Here we will only talk about the general benefits that SDN has for the network.

Centralized Management

Centralization is one of the main advantages granted by SDN. SDN network enables centralized management over the network using a central management tool, from which data center managers can benefit. It breaks out the barrier created by traditional systems and provides more agility for both virtual and physical network provisioning, all from a central location.

Security

SDN controller provides a centralized location for network engineers to control the entire security of the network. Despite the fact that the trend of virtualization has made it more difficult to secure networks against external threats, SDN brings massive advantages. Through the SDN controller, security policies and information are ensured to be implemented within the network. And SDN is equipped with a single management system, which helps to enhance security.

Cost-Savings

SDN network lands users with low operational costs and low capital expenditure costs. For one thing, the traditional way to ensure network availability was by redundancy of additional equipment, which of course adds costs. Compared to the traditional way, a software-defined network is much more efficient without the need to acquire more network switches. For another, SDN works great with virtualization, which also helps to reduce the cost for adding hardware.

Scalability

Owing to the OpenFlow agent and SDN controller that allow access to the various network components through its centralized management, SDN gives users more scalability. Compared to a traditional network setup, engineers are provided with more choices to change network infrastructure instantly without purchasing and configuring resources manually.

 

The Difference Between SDN and Traditional Networking

In terms of infrastructure, traditional networks rely on hardware-centric setups, tightly integrating control and data planes in devices. In contrast, SDN is software-based, separating the control plane from the data plane, which significantly enhances its flexibility. This differentiation allows SDN to offer a more adaptable and programmable infrastructure compared to the rigid configurations of traditional networks.

Regarding security, traditional networks implement fragmented security measures on individual devices, whereas SDN centralizes security management through the controller. This centralized approach in SDN enables a more cohesive and responsive network-wide security implementation, offering better adaptability and coordination against evolving threats than the decentralized security measures of traditional networks.

Conclusion

SDN is transforming the way data centers operate, providing tremendous flexibility, scalability, and control over network resources. By embracing SDN, organizations can unleash the full potential of their data centers and stay ahead in an increasingly digital and interconnected world.

You might be interested in

Knowledge
Knowledge
See profile for Howard.
Howard
What Is Open Networking?
Jun 1, 2022
6.1k
Knowledge
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge