What Is Wi-Fi 6E? Why Do You Need It?
Wi-Fi 6E has arrived, and regardless of your current awareness of its importance, it's undeniably an exhilarating breakthrough! In this article, we embark on an exploration of the fundamental aspects of Wi-Fi 6E, decipher why it holds such immense significance, and uncover the myriad ways it elevates our network connectivity experience.
What’s Wi-Fi 6E?
Wi-Fi 6E is an extension of the Wi-Fi 6 standard released by the Wi-Fi Alliance, allowing operation in the 6 GHz frequency band while also supporting the 2.4 GHz and 5 GHz bands. Within the 6 GHz band, Wi-Fi 6E devices can take full advantage of an additional 1200 MHz spectrum. This new frequency band is free from interference and overlaps, providing Wi-Fi devices with more capacity, wider channels, and reduced latency. It paves the way for future innovative applications, including augmented reality/virtual reality (AR/VR) and 8K streaming, and elevates wireless connectivity performance to a new level.
How Does Wi-Fi 6E Work?
Wi-Fi 6E operates in the 6 GHz frequency band, increasing channel and spectrum resources, incorporating advanced features of 802.11ax, and cooperating with Target Wake Time (TWT) and high-order modulation technology to deliver higher capacity and more efficient network performance to meet the demands of modern networks.
-
Utilizing the 6 GHz Frequency Band: Wi-Fi 6E not only leverages the existing 2.4 GHz and 5 GHz frequency bands but also introduces the availability of the 6 GHz frequency band.
-
Expanding Channels and Spectrum Resources: Wi-Fi 6E networks are equipped with an additional 14 80 MHz channels and 7 160 MHz channels, enhancing their channel and spectrum resources.
-
Leveraging Advanced 802.11ax Features: Features such as 8x8 MU-MIMO, OFDMA, and BSS Color are used to provide up to four times the capacity, efficiently handling a multitude of high-bandwidth, low-latency applications.
-
Target Wake Time (TWT): TWT is employed to improve network efficiency and extend device battery life, making it particularly crucial for low-power communications in IoT devices.
-
1024-QAM Modulation: This technology enables the transmission of more data within the same amount of spectrum, increasing throughput for emerging bandwidth-intensive applications.
Do You Need Wi-Fi 6E?
In today's fast-paced digital world, the demand for robust and high-performance Wi-Fi connectivity has never been greater, and as reliance on Wi-Fi continues to grow, so do the challenges it faces.
-
Increasing Wi-Fi Device Numbers: With the surge in Wi-Fi devices, from smartphones to IoT equipment, the demand for connectivity is on the rise.
-
Heavier Traffic on Wi-Fi: As bandwidth-hungry applications like 4K video streaming, online gaming, and video conferencing become more prevalent, the need for additional bandwidth is evident.
-
Congestion in Legacy Frequency Bands: Early Wi-Fi frequency bands, such as 2.4GHz and 5GHz, have become crowded due to the multitude of networks operating within them.
-
Network Interference: Traditional Wi-Fi frequency bands are susceptible to interference from other electronic devices and neighboring networks, resulting in network performance issues.
How Significant Is Wi-Fi 6E?
-
Greater Capacity: With 7 new 160MHz wide channels, it allows more devices to connect to the network simultaneously without causing congestion, enabling it to meet the growing demands of device density and connections.
-
Less Interference: The 6GHz spectrum benefits from management and efficiency of Wi-Fi 6, avoiding interference from other wireless devices and networks, thereby enhancing network stability and performance.
-
Higher Performance: The wider spectrum and channel width provide higher throughput, resulting in faster data transfer speeds, making it ideal for gaming, augmented/virtual reality, robotics, and large file downloads.
FS Wi-Fi 6E Product
Experience an unprecedented level of power with the AP-N635 wireless access point! Ideal for large conference centers, campuses, large venues, etc.
-
Unlock the New 6 GHz Radio:Up to 7775 Mbps the Available Capacity
-
Multi-rate 2.5G/5G Ethernet Port Boosts Total Internet Throughput
-
160 MHz Frequency Bandwidth, Supporting 5/6 GHz-prior Access
-
Managed via Airware Cloud/Wireless Controller/Security Gateway or Operate Alone
-
Seamless Roaming with Airware Cloud/Wireless Controller/Security Gateway
-
WPA3, WIDS and RF Interference Tracking, etc. Ensure Data Security
-
Support OFDMA, MU-MIMO, 1024-QAM, TWT
-
Powered by 802.3bt PoE (PoE injector sold separately)
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023