English

Why Green Data Center Matters

Updated on Jun 21, 2022 by
6.3k

Background

With the continuous growth of new data storage requirements and the steady enhancement of green environmental protection awareness, green data centers appear in the concept of enterprise construction. Newly retained data must be protected, cooled, and transferred efficiently. This means that the huge energy demands of data centers present challenges in terms of cost and sustainability, and enterprises are increasingly concerned about the energy demands of their data centers. It can be seen that sustainable and renewable energy resources have become the development trend of green data centers.

Green Data Center Is a Trend

A green data center is a facility similar to a regular data center that hosts servers to store, manage, and disseminate data. It is designed to minimize environmental impact by providing maximum energy efficiency. Green data centers have the same characteristics as typical data centers, but the internal system settings and technologies can effectively reduce energy consumption and carbon footprints for enterprises.

The internal construction of a green data center requires the support of a series of services, such as cloud services, cable TV services, Internet services, colocation services, and data protection security services. Of course, many enterprises or carriers have equipped their data centers with cloud services. Some enterprises may also need to rely on other carriers to provide Internet and related services.

According to market trends, the global green data center market is worth around $59.32 billion in 2021 and is expected to grow at a CAGR of 23.5% in the future to 2026. It also shows that the transition to renewable energy sources is accelerating because of the growth of green data centers.

As the growing demand for data storage is driving the modernization of data centers, it also places higher demands on power and cooling systems. On the one hand, data centers need to convert non-renewable energy into electricity to generate electricity, resulting in rising electricity costs; on the other hand, some enterprises need to complete the construction of cooling facilities and server cleaning through a lot of water, all of which are ample opportunities for the green data center market.

For example, Facebook and Amazon continue to expand their businesses, which has also increased the need for data storage of global companies. These enterprises need a lot of data to complete the analysis of potential customers, but these data processing needs will require a lot of energy. Therefore, the realization of green data centers has become an urgent need for enterprises to solve these problems, and this can also bring more other benefits to enterprises.

Green Data Center Benefits

The green data center concept has grown rapidly in the process of enterprise data center development. Many businesses prefer alternative energy solutions for their data centers, which can bring many benefits to the business. The benefits of green data centers are as follows.

Energy saving

Green data centers are designed not only to conserve energy, but also to reduce the need for expensive infrastructure to handle cooling and power needs. Sustainable or renewable energy is an abundant and reliable source of energy that can significantly reduce power usage efficiency (PUE). The reduction of PUE enables enterprises to use electricity more efficiently. Green data centers can also use colocation services to decrease server usage, lower water consumption, and reduce the cost of corporate cooling systems.

Cost reduction

Green data centers use renewable energy to reduce power consumption and business costs through the latest technologies. Shutting down servers that are being upgraded or managed can also help reduce energy consumption at the facility and control operating costs.

Environmental sustainability

Green data centers can reduce the environmental impact of computing hardware, thereby creating data center sustainability. The ever-increasing technological development requires the use of new equipment and technologies in modern data centers, and the power consumption of these new server devices and virtualization technologies reduces energy consumption, which is environmentally sustainable and brings economic benefits to data center operators. For those interested in understanding how technology intersects with ecological responsibility, the article "Eco-Friendly Networking: Green Technologies" serves as an excellent resource.

Enterprise social image enhancement

Today, users are increasingly interested in solving environmental problems. Green data center services help businesses resolve these issues quickly without compromising performance. Many customers already see responsible business conduct as a value proposition. Enterprises, by meeting compliance, regulatory requirements and regulations of the corresponding regions through the construction of green data centers, improve the image of their own social status.

Reasonable use of resources

In an environmentally friendly way, green data centers can allow enterprises to make better use of various resources such as electricity, physical space, and heat, integrating the internal facilities of the data center. It promotes the efficient operation of the data center while achieving rational utilization of resources.

5 Ways to Create a Green Data Center

After talking about the benefits of a green data center, then how to build a green data center. Here are a series of green data center solutions.

  • Virtualization extension: Enterprises can build a virtualized computer system with the help of virtualization technology, and run multiple applications and operating systems through fewer servers, thereby realizing the construction of green data centers.

  • Renewable energy utilization: Enterprises can opt for solar panels, wind turbines or hydroelectric plants that can generate energy to power backup generators without any harm to the environment.

  • Enter eco mode: Setting the alternating current UPS to eco mode is one way to go green. This setup can significantly improve data center efficiency and reduce PUE. Alternatively, enterprises can reuse equipment, which not only saves money, but also eliminates unnecessary emissions from seeping into the atmosphere.

  • Optimized cooling: Data center infrastructure managers can introduce simple and implementable cooling solutions, such as deploying hot aisle/cold aisle configurations. Data centers can further accelerate cooling output by investing in air handlers and coolers, and installing economizers that draw outside air from the natural environment to build green data center cooling systems.

  • DCIM and BMS systems: DCIM software and BMS software can help data centers managers identify and document ways to use more efficient energy, helping data centers become more efficient and achieve sustainability goals.

Conclusion

Data center sustainability means reducing energy/water consumption and carbon emissions to offset increased computing and mobile device usage to keep business running smoothly. The development of green data centers has become an imperative development trend, and it also caters to the green goals of global environmental protection. As a beneficiary, enterprises can not only save operating costs, but also effectively reduce energy consumption. This is also an important reason for the construction of green data centers.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k