English

Why Should You Use Cumulus Linux OS?

Updated on Sep 27, 2021 by
14.7k

Note: FS has discontinued Cumulus Linux system for N-series switches. As per our policy, customers will continue to get support from FS technical assistance team, and the valid warranty provided is maintained on the product. For customers who are interested in FS N-series switches, you can choose either bare metal ones or those loaded with FSOS.

cumulus linux benefit

With technology development, network managers meet some new challenges, such as how to make networks simpler, more affordable and faster to deploy? And compared to traditional data center network which is locked and proprietary, there is a trend to change to modern data center which is open to choice of application, operating system and hardware. How to fulfill the purpose? Cumulus Linux is designed to provide an open platform for innovation. With Cumulus Linux, your network will be faster, easier and affordable.

cumulus linux vs. traditional data center

What Is Cumulus Linux?

Cumulus Linux is a powerful open network operating system which allows you to automate, customize and scale using web-scale principles like the world’s largest data centers. The code used to create Linux is free and available to the public to view, edit and for users with the appropriate skill to contribute to. This open approach enables choice with the best hardware, software, application, network architectures and no vendor lock-in. Cumulus Linux is the only solution that allows you to affordably build and efficiently operate your network like the world’s largest data center operators, unlocking vertical network stacks.

What is cumulus linux

Why Cumulus Linux?

Built for automation, scalability and flexibility, Cumulus Linux is the world’s most flexible open network operating system for bare metal switches which allows you to build a data center network that ideally suits your business needs. The key functionalities of Cumulus Linux are as follows.

why cumulus linux

CAPEX Savings

Reduced CAPEX can be achieved by lowering the cost of acquiring open switches and optics. As can be seen from the following picture, the total cost of bare metal MSRP is much lower than that of Cisco.

CAPEX savings by using cumulus linux

OPEX Savings and Operational Efficiencies

Allowing complete freedom of choice and supplying chain control with industry-standard 50+ hardware platforms, you can choose compatible hardware based on your needs and budget. By adopting Linux principles for networking, customers have achieved operational efficiency and reduced their time to production by as much as 95%, while reducing their TCO by up to 60%. With rich ecosystem and converged administration, Cumulus Linux helps to get simpler, scalable, faster-to-deploy networks. And OPEX is reduced by leveraging existing talent and assigning more switches per engineer.

Efficient Troubleshooting and Monitoring

Cumulus Linux leverages traditional Linux and networking tools such as SNMPv2/v3, SPAN/ERSPAN, and integrates with advanced monitoring tools such Collectd, Ganglia, Nagios. Furthermore, it provides advanced troubleshooting with tools such as Cumulus Linux’s Prescriptive Topology Manager for topology consistency against a topology graph.

Network Command Line Utility (NCLU)

Automation and consistency are critical characteristics of web scale IT, which is why Cumulus Linux was designed with automation top of mind. To make the process even easier, Cumulus’s NCLU allows network operators and system administrators to harness the power of Linux networking and quickly automate using NCLU module.

Summary

Cumulus Linux is the ultimate choice when it comes to flexibility and innovation, enabling the best of breed hardware and technology ecosystem. Providing economical scalability and choice flexibility, Cumulus Linux can run multiple network paths without the need for multiple switches, giving you traffic isolation and network segmentation for multiple devices.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.9k