Wi-Fi 6 Upgrade: Why You Should Move Up to Wi-Fi 6?
WiFi 6 (802.11ax) belongs to the most recent wave of WiFi technology. It offers enhanced WiFi speeds and dependable connections, allowing you to indulge in seamless streaming, quicker downloads, and the ability to connect additional smart home devices without compromising your internet performance. This article explains some reasons for the WiFi 6 upgrade.
WiFi 6 Delivers Top-notch Performance In Busy Households With Multiple Devices
This latest WiFi standard builds upon the already impressive technology of WiFi 5 (802.11ac). While WiFi 5 introduced gigabit speeds to our WiFi connections, it struggles to provide the optimal WiFi experience as the number of devices in smart homes continues to increase. WiFi 6 utilizes orthogonal frequency division multiple access (OFDMA), a critical feature that enhances overall network efficiency. This enables multiple devices with diverse bandwidth requirements to connect to your WiFi network seamlessly.
WiFi 6 Offers The Swiftest Real-world Speeds And Extended Range Capabilities
In WiFi technology, each frequency band (2.4 GHz or 5 GHz) is composed of component streams through which our WiFi data travels. Both WiFi 5 and WiFi 6 support the highest number of streams, enabling gigabit WiFi speeds. However, WiFi 6 takes it a step further by increasing the number of streams to an impressive 12 across the 2.4 GHz and 5 GHz bands, surpassing WiFi 5's limit of 8 in a dual-band setup.
This increase in the number of streams results in faster connection speeds, providing client devices with more pathways to communicate with the WiFi router. In fact, client devices that support WiFi 6 experience a remarkable 40% speed boost compared to their WiFi 5 counterparts.
WiFi 6 Is Designed For The Smart Home
The proliferation of Smart Home devices and Internet of Things (IoT) applications is increasing rapidly. Consequently, the number of WiFi-connected devices in an average home is escalating from around 10 devices to as many as 50 or even more. Each WiFi-connected device, such as lightbulbs, smart switches, door locks, appliances, or cameras, adds to the load on your WiFi network. WiFi 6 has been specifically designed to accommodate this surge in devices without compromising WiFi speeds. As a result, you can enjoy a seamless streaming experience while ensuring uninterrupted connectivity for lights, switches, thermostats, and any other IoT device you incorporate into your smart home.
WiFi 6 Routers Are Perfectly Suited For Streaming 4K/8K UHD Content
The smooth playback of high-resolution videos necessitates a consistently high-speed connection. In households with multiple users, streaming such high-definition videos places even greater strain on the network. However, WiFi 6 routers are equipped with advanced features like ultra-fast processors, expanded memory, and an increased number of radio streams. These enhancements enable WiFi 6 routers to effortlessly handle the simultaneous streaming of multiple high-definition video sessions, eliminating issues like stuttering, buffering, or other frustrating disruptions commonly experienced with older WiFi technologies.
WiFi 7 vs WiFi 6 & WiFi 6E
The transition from WiFi 5 to WiFi 6 brought about substantial improvements. However, there is now another option available: WiFi 7. This latest wireless standard represents a quantum leap forward from both WiFi 6 and WiFi 6E, offering even greater benefits. With faster speeds, reduced latency, and significant capacity enhancements, WiFi 7 has evolved from its predecessors to meet the growing demands of users. It shares many similarities with WiFi 6 and 6E but incorporates notable improvements. To delve deeper into the comparison between WiFi 7 and WiFi 6, you can explore our dedicated article on the subject.
How to Upgrade to WiFi 6
WiFi 6 upgrade means you need a compatible computer or phone and router. Here’s how to upgrade to WiFi 6:
-
To enhance your computer or phone's capabilities, consider upgrading them. For computers, you have the option to either install a new WiFi adapter or purchase a completely new device. While it is generally possible to replace components in desktop PCs, laptops typically do not offer this flexibility. Most new computers and phones are already equipped with WiFi 6, but it's advisable to verify the compatibility beforehand.
-
Another step you can take is to invest in a WiFi 6 router. It is important to conduct thorough research to determine the best model for your specific needs, as different routers offer various features. While WiFi 6E routers boast the highest specifications, they may not be necessary for most households. The setup process for a WiFi 6 router varies depending on the model, so consulting the accompanying manual is recommended.
-
In most cases, you may not need to download and install specific software drivers, as Windows 10 and 11 already support WiFi 6 by default. However, it's worth noting that certain drivers may not be included in the Windows update, requiring manual driver updates or the use of an automated driver updater. Mac users can check for available software updates and install them if necessary.
Conclusion
It's a good idea to upgrade your gear now if your router is three years old or more. You can start by buying a Wi-Fi 6 router and then upgrade your gadgets one by one. Not only will this spread out the costs, but it will also help you understand whether the switch is worth it. If you're considering a WiFi 6 upgrade, contact us.
You might be interested in
Email Address
-
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023