English

Wi-Fi 6 vs 5G: Technology and Use Cases Comparison

Updated on Nov 24, 2020 by
11.5k

It's known that 5G networks will provide 50x more speed, 10x less latency, and 1,000x more capacity than its predecessor 4G/LTE, delivering faster connectivity for better user experiences. Wi-Fi 6, the 6th generation of Wi-Fi technology with a theoretical bandwidth of 9.6Gbps, provides higher speed, larger capacity, better efficiency, wider coverage, lower power consumption, smarter management, and more devices to serve simultaneously. Both 5G and Wi-Fi 6 are the latest versions of their respective technologies. What are their similarities and differences? And what about the applications of 5G and Wi-Fi 6? An in-depth analysis of Wi-Fi 6 vs 5G will be unfolded.

Wi-Fi 6 vs 5G Comparison

 

Technology comparison Wi-Fi 6 vs 5G

Network security

Both 5G and Wi-Fi 6 offer secure methods of communication with 5G excelling slightly more with better privacy and default security. Wi-Fi 6 networks use WPA3 certification, which enables strong 256 bit AES encryption. WPA3 also allows devices to join via QR code to accommodate the rise in IoT sensor support.

Ensuring users' authentication request packets are encrypted, 5G solves the issue about user information leakage left by 4G. With robust end-to-end encryption built into the technology, 5G uses SIM authentication rather than usernames, passwords or certificates for gaining access to the network. Many of us are familiar with the SIM cards in our cell phones that provide service. SIM data contains identity and subscriber information to determine what level of access the user and device has to the network. Administrators can use physical SIM cards or eSIM to provision devices via QR code. Additionally, 5G also enhances security by extending the key length from 128 bits to 256 bits. A longer key means higher security.

Technology type

Many of the differences between Wi-Fi 6 and 5G stem from the difference between their technology types, which is the most notable distinction between Wi-Fi 6 and 5G. 5G is successor to 4G LTE cellular technology where as WiFi 6 is successor to 802.11ac Wi-Fi standard - a version of WLAN technology. Cellular technologies from 1G to 5G follows 3GPP specifications.

License

5G technology is carrier-based, access traffic of all terminals must pass through the carrier's network, This means operators exclusively operate cellular networks on licensed spectrum bands, which are meant to prevent interference between connected devices. When a new terminal attempts to access the network, applying for a license is a must. What's more, carriers must assist if any expansion of network coverage is required.

Wi-Fi 6 uses an unlicensed spectrum, Wi-Fi networks are flexible and convenient to deploy or expand. If more users are involved or wider coverage is required, the deployment process is to add APs and customize policies to control the network resources accessible to different types of terminals and their access bandwidth. The new terminals can easily access the Wi-Fi network by creating an account. On the other hand, Wi-Fi 6 can suffer from interference from neighboring networks. That is because the Wi-Fi frequency bands are public and prone to interference, so conflicts will happen as the number of users increases. OFDMA and MU-MIMO adopted in Wi-Fi 6 will effectively solve this problem by improving network efficiency and capacity. Therefore, wireless network stability increases dramatically in the Wi-Fi 6 era, not inferior to 5G.

Spectrum Usage

2.4 GHz and 5 GHz are the two frequency bands that Wi-Fi 6 carries. 2.4 GHz band is used as a wireless frequency commonly but with high interference. 5 GHz Wi-Fi frequency band is faster in speed and better in anti-interference. Due to the higher frequency nature, its transmission distance is shorter. With the permits of more frequency bands, Wi-Fi 6 can be extensively developed in the future.

5G frequency bands can be divided into two categories. The frequency bands lower than 3 GHz have been used on existing networks with diverse usages. As a result, 3.5 GHz frequency bands are mainly used in the 5G era. The sub-6 GHz (operating below 6 GHz) can also be used for 5G applications, which offers stronger coverage and penetration capabilities.

Currently, the frequency bands used by Wi-Fi are free of charge, indicating that any person or company can use these bands without registration. Compared to Wi-Fi, the 5G spectrum is a strategic resource that can only be sold to carriers of the country. Actually, some governments have begun to allocate 5G spectrums to business entities for the combination of telecom and vertical industries, but the spectrum sharing still is considered as a problem that needs to be considered.

Network Devices

Embedded with the Wi-Fi function, countless devices like smartphones, laptops, printers, projection TVs are allowed to access personal or enterprise networks. Current WLAN APs support IoT protocols, enabling these devices to be directly connected to the Wi-Fi network. If some of the devices don't support Wi-Fi, they may rely on RFID, ZigBee, or Bluetooth. Unlike Wi-Fi, the 5G networks emphasize more on personal mobile terminal prioritization, allowing most mobile phones and some tablets to access cellular networks using SIM cards.

Summary: Wi-Fi 6 vs 5G Comparison Table

Specifications Wi-Fi 6 5G
Technology WLAN Cellular
Standard IEEE 802.11ax 3GPP Rel. 15 and beyond
Modulation 1024QAM 256QAM
MIMO 8T8R/12T12R-8 streams Indoor: 4T4R-4 streams
Outdoor: 64T64R-16 streams
Spectrum Unlicensed Licensed
Terminal Types Various enterprise terminals (PCs, projectors, monitoring devices, etc.) Mainly mobile terminals, few enterprise devices embedded with SIM cards
Security 5G cellular connections are more secure compare to unknown wifi connections. 5G will be as secure as 4G LTE today. 5G supports multiple authentication and key management features. WiFi 6 supports WPA3 security protocols to provide high security.
Management Enterprise management personnel Carriers
Cost of deployment Cheaper Expensive
Application Indoors Outdoors
 

Use cases Wi-Fi 6 vs 5G

5G is a new trend in the telecom industry and has benefited more and more users. Since 5G can cover both the inside and outside of complexes, Wi-Fi technology will no longer be needed? 5G vs Wi-Fi 6, will 5G push Wi-Fi into obscurity? Trying to pick a winner between them is just missing the point. The following analysis will show how these two technologies differ and complete each other.

Wi-Fi 6 vs 5G Application

Indoor Coverage

On the one hand, both 5G and Wi-Fi 6 can be deployed in daily network connection inside the building. Generally, 5G can accommodate one terminal per square meter, equating to one million terminals per square kilometer. Therefore, this solution is not suitable for the sites where each user has at least two terminals or for some high-density areas. With the flexible Wi-Fi 6 solution, this problem can be easily handled. Wireless AP is a de-facto choice for most users. The AP's transmit power can be controlled to reduce the coverage area. Therefore, two or three terminals can be connected to the network synchronously per square meter. Besides, directional antennas can be deployed to cover special areas with high-density access requirements.

On the other hand, 5G and Wi-Fi 6 can also be applied for IoT services. 5G massive machine-type communications (mMTC) is designed for connecting massive IoT devices. But it is difficult to directly install 5G NICs on the necessary devices for communication due to the different IoT protocols required for different applications. Most of the WLAN APs now have integrated function modules like RFID, ZigBee, and Bluetooth, and can support more IoT protocols via external cards. Combining IoT with Wi-Fi will offer a cost-effective solution, which makes Wi-Fi fit for indoor scenarios with massive IoT devices.

Outdoor Coverage

Typically, outdoor Wi-Fi 6 is mainly used to provide users in some high-density scenarios like parks & playgrounds, while 5G is better suited to provide larger scale outdoor coverage such as scenic spots. 5G outdoor macro base stations outperform Wi-Fi 6 in both coverage range and roaming. Therefore, 5G is now the optimal choice for supporting autonomous cars, drones, and some IoT devices (such as smart street lamps) in smart cities.

Here is a sketch to show the typical application scenarios of Wi-Fi 6 and 5G for both indoors and outdoors.

Wi-Fi 6 vs 5G_ Indoor and Outdoor Application

Entertainment Exploration

Emerging applications in the entertainment field like VR/AR/4K/8K have high bandwidth requirements. For example, 4K requires a bandwidth of more than 50 Mbps whereas VR/AR requires a bandwidth of over 100 Mbps.

5G adopts two high-frequency bands to improve user bandwidth: Sub-6G and mmWave – the former supports the maximum frequency bandwidth of 100 MHz, while the latter with 400 MHz. Due to their large size and limitations on installation space, smaller 4T4R MIMO antennas are generally used rather than 64T64R Massive ones. Since the number of micro base stations deployed must match the number of APs, the costs of indoor 5G coverage have increased accordingly.

All of the high-performance Wi-Fi 6 APs support 8x8 MIMO with three non-overlapping channels in the 80 MHz frequency bandwidth. A terminal supporting 2x2 MIMO, theoretically, whose 80 MHz frequency bandwidth can provide a bandwidth of 1.2 Gbps, easily meeting the bandwidth requirements of VR/AR/4K. Yet 5G is better for those latency-sensitive remote assistance VR applications that only one user is getting involved at a time.

Industrial Manufacturing

Traditionally, manufacturers could only connect applications through wired technologies. The emergence of devices like AGVs, industrial AR, and machine vision are applied on a large scale making IoT wireless networks a necessity for production workshops. Wi-Fi 6 with high bandwidth and low latency can meet the demands for industrial production networks, which are deployed for wireless access in some intelligent production and manufacturing scenarios.

In some specific situations that have applications extremely sensitive to latency, like collaborative robots requiring a latency of less than 5 ms, it's inadvisable to transmit the data of such applications (requiring a latency less than 20 ms) over Wi-Fi networks. 5G will provide an optimal solution for this kind of scenario.

Wi-Fi 6 vs 5G Pros & Cons Table

  Wi-Fi 6 5G
Pros Mainstream enterprise wireless solution.(spectrum, terminals, easy and flexible deployment, better management, expenses.) Leading wireless technology. (MIMO, service latency, mobile roaming, outdoor coverage)
Cons Not perform well in large-scale outdoor coverage scenarios.
Cannot meet the ultra-low latency requirements (< 10 ms).
Higher costs for indoor deployments.
Weak terminal compatibility.
Carriers must participate in 5G deployment.
 

A New Era of Seamless Wireless Access: Wi-Fi 6 Joint 5G

Wi-Fi 6 and 5G technologies are poised to have profound impacts on all walks of life. Although some of the functions and applications of Wi-Fi 6 and 5G may overlap, all the signs are still pointing to us that taking the advantages of both technologies is wiser and will bring the maximum benefits to the enterprises.

Despite that 5G is growing vigorously and begins to be adopted in some vertical industries now, it still needs a while before being applied to enterprises maturely and fully. But for Wi-Fi 6 technology, there are many applicable solutions for enterprises in various fields at present. That is because adopting Wi-Fi 6 technology in network deployment will help to establish the networks more quickly and reduce the operational expenses, better for the enterprises' customizations at the same time. 5G networking that fits for high roaming and latency requirements focuses more on public networks now. With the development of 5G technology, it will also play an important role in the Wi-Fi network upgradings.

Wi-Fi 6 and 5G each have their respective most applicable scenarios where neither can replace the other. Combining 5G with Wi-Fi 6 is an inevitable trend for public and private networks in the predictable future due to their complementary roles. Selecting the most appropriate technology according to the scenario requirements will help enterprises to improve efficiency with fewer budgets, accelerating the digital transformation eventually.

Tags

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.9k