English

Ethernet Switch Port Types Overview

Updated on Dec 20, 2021 by
42.4k


The forms and data rates of Ethernet switches vary, and the switch port types also do. In this article, some common Ethernet switch port types are briefly introduced in terms of data rates, functions and network architecture to help you better understand their differences and make preparations for your future network plans.

Differentiate Ethernet Switch Port Types by Data Rates

Data rate is a vitally important factor for Ethernet switch interface, and it can usually vary from 1G, 10G, 25G, 40G to 100G and beyond. The following are some mainstream interface types of these different data rates.

RJ45 Port

RJ45 port on 100/1000BASE switch can be used in data centers for server switching, LANs, uplinks from desktop switches or directly to the desktop for broadband application. A standard Ethernet cable (Cat5/5e/6/6a cable) is often used when connecting two RJ45 ports on Gigabit switches.

SFP Port

SFP Port (mini-GBIC port) is a small-sized hot-swappable interface. Typical speeds were 1 Gbit/s for Ethernet SFPs and up to 4 Gbit/s for Fiber Channel SFP modules. SFP port enables a gigabit switch to achieve fiber uplinks over longer distances or short-range copper uplinks by inserting corresponding SFP modules (fiber SFP or copper SFP).

SFP+ Port

SFP+ port (small form-factor pluggable plus) is an enhanced version of SFP port, supporting higher speeds up to 10Gbps. In terms of SFP vs SFP+ compatibility, SFP+ ports often accept SFP optics but at a reduced speed of 1Gbps. However, you cannot plug an SFP+ transceiver into an SFP port because SFP+ does not support speeds less than 1Gbps.

SFP28 Port

SFP28 port is an enhanced version of SFP+ port. SFP28 has the same common form factor as the SFP+, but supports 25Gb/s over a single lane. SFP28 provides a new way for networking upgrade: 10G-25G-100G, which is an energy-efficient solution to meet the growing demands of next-generation data center networks.

QSFP+ Port

QSFP+ port is an evolution of QSFP (quad small form-factor pluggable) port designed to 4x10G lanes to support 40G Ethernet. That’s to say, it has four-channel 10 Gbit/s SFP+ interfaces which can transfer rates up to 40Gbps.

QSFP28 Port

QSFP28 port is designed for 100G applications. It offers high-speed differential signals with data rates ranging from 25 Gbps up to potentially 40 Gbps, and finally meet 100 Gbps Ethernet (4×25 Gbps) and 100 Gbps 4X InfiniBand Enhanced Data Rate (EDR) requirements.

A network switch may support diversified ports. Here take some gigabit switch, 10GB Ethernet switch and 40G/100G Ethernet switches as examples to show the switch port types and numbers that a network switch may have.


Cisco Catalyst 4948 10 Gigabit Switch Dell EMC S6010-ON 40GE Switch FS S3900-24T4S 10/100/1000BASE-T Gigabit Switch FS S5850-48S2Q4C 100GB Ethernet Switch
RJ45 Port 48 / 24 /
SFP Port / / / 48
SFP+ Port / / 4 /
QSFP+ Port / 32 / 2
QSFP28 Port / / / 4

Differentiate Ethernet Switch Port Types by Functions

Functions and applications are also important factors for Ethernet switch connector types as the same port can be used for various purposes. This category may be more complex, but helps us gain insights into Ethernet switch port types configuration.

Combo Port

Combo port is considered as a single interface with dual front ends, i.e. an RJ-45 connector and an SFP module connector. In other words, it is a compound port which can support two different physical, share the same switch fabric and port number. But the two different physical ports can not be used simultaneously. That means if the SFP port is being used, the corresponding copper port is automatically disabled and vice versa. The advantage is to provide different types of connectivity without taking up unused switch fabric, giving users the power and flexibility to configure their switch for their unique application requirements.

FS-S3900-24F4S-24-Port-Gigabit-Switch.jpg

Stack Port

Stack port, a special functional port on the switch, is used to connect with other stackable switches of the same model, brand and software version to operate as a single stackable switch. This group of switches show the characteristics of a single switch but have the port capacity of the sum of the combined switches. Additionally, a stack port can be an uplink port, but some switches may have a dedicated port for stacking. For example, FS S3900 Series stackable switches use uplink port to achieve stacking with DAC, AOC or transceiver modules and fiber patch cables. This solution is very economical with high flexibility and ideal for long distance connection.

FS-S3900-48T4S-Switch-Stacking-Connection.jpg

PoE Port

Power over Ethernet (PoE) allows a single network cable to carry data and power simultaneously. PoE ports deliver power according to two standards – IEEE 802.3af delivers power up to 15.4 Watts on a switch port whereas IEEE 802.3at (also known as PoE+) delivers power up to 30 Watts on a switch port. However, the power would be lost as the distance increasing. The minimum guaranteed power available at the PD is 12.95 watts per port for PoE and 25.5 watts per port for PoE+.

Application-of-FS-S1600-24T4F-24-Port-PoE-Switch.jpg

Differentiate Ethernet Switch Port Types by Network Architecture

Traditional network architecture usually has three layers, including core layer, distribution layer and access layer. Correspondingly, Ethernet switches and ports also have these types.

Access Port

Access port is used for connecting devices such as desktops, laptops, printers etc., only available in access link. A switch port in access modes belongs to one specific VLAN and sends and receives regular Ethernet frames in untagged form. Usually, an access port can only be member of one VLAN, namely the access VLAN, and it discards all frames that are not classified to the access VLAN.

Trunk Port

Trunk port is adopted among switches or between switch and upper-level devices, available in trunk link. A trunk port allows for several VLANs set up on the interface. As a result, it is able to carry traffic for numerous VLANs at the same time. The trunk port is a VLAN aggregation port connected to other switch ports while the access port is the port that the switch connects to the host in the VLAN.

Hybrid Port

Hybrid port can be used to connect network devices, as well as user devices. It supports both untagged VLAN like access port and tagged VLAN like trunk port, and it can receive data from one or more VLANs. The hybrid ports resemble trunk ports in many ways, but they have additional port configuration features.

The following figure shows how the three types of switch ports apply in a same system.

Operation-Process-of-Three-Ports-in-a-System.jpg

Conclusion

Figuring out the differences of Ethernet switch port types helps in choosing more suitable Ethernet switches for your network requirements. When considering the switch port type and switch port number you need, you should think about the current and future business volume and your demands for the functions. The suited is the best.

Related Articles:

What Does Combo Port Mean for Ethernet Switch?

Multi-Gigabit Switch for Growing Enterprise Campus Network

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
390.8k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
369.4k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
339.3k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
423.1k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
298.6k