English

How to Identify the Fiber Color Code?

Updated on Dec 22, 2021 by
159.8k

We have been using different types of fiber optic cable in labs and data centers for years. It is not unusual for a green hand to mix up the 50/125 and 62.5/125 multimode fibers, or the single mode fibers, not to mention the multi-fiber cables that may consist of tens and hundreds of fibers. Fortunately, there are systems made to address these issues, such as the EIA/TIA-598, which is the most recognized system worldwide. It includes fiber color code for different types and numbers of optical fiber cables. These fiber optic cable color codes help us to identify an optical fiber cable from its jacket, buffer, tube, connector, etc.

Colored jackets of multi-fiber cable

Figure 1: Colored jackets of multi-fiber cable.

Outer Jacket Color Code

Colored outer jackets or print may be applied to outside plant and premises fiber cables, such as fiber distribution cables, fiber optic patch cords, etc., for easy identification and distinction. In EIA/TIA-598, the fiber color code defines the jacket color codes for different fiber types. So for optical fiber cable that contains only one type of fiber, we can easily identify it by its jacket color; unless otherwise specified, the outer jacket of premises cable containing more than one fiber type shall use a printed legend to identify the quantities and types of fibers within the cable. For example, "12 Fiber 8 x 50/125, 4 x 62.5/125" indicates the presence of 12 fibers in total, with 8 fibers having a core/cladding size of 50/125μm and 4 fibers having a core/cladding size of 62.5/125μm.

Here are the jacket color codes for different fiber types:

Fiber Type Color Code
  Non-military Applications Military Applications Suggested Print Nomenclature
OM1 62.5/125µm Multimode Orange Slate 62.5/125
OM2 50/125µm Multimode Orange Orange 50/125
OM3 50/125 µm (850 nm Laser-Optimized) Multimode Aqua Undefined 850 LO 50/125
OM4 50/125µm (850 nm Laser-Optimized) Multimode Aqua/Violet Undefined 850 LO 50/125
100/140µm Multimode Orange Green 100/140
OS1/OS2 Single Mode Yellow Yellow SM/NZDS, SM
Polarization Maintaining Single Mode Blue Undefined Undefined

Besides the jacket colors specified in fiber color code standard, other colors may also be used if the print on the outer jacket can tell the fiber classifications. Such colors should be agreed upon between manufacturer and user.

Inner Cable Organizational Fiber Color Code

Inside a multi-fiber cable, individual fibers are compliant to fiber color code as well. They are often distinguished from one another by color-coded jackets, buffers or tubes on each fiber. According to EIA/TIA-598, inner fibers are color coded in a group of 12 fibers and they are counted in a clockwise direction.

fiber color code

Figure 2: Counting direction of a group of 12 fibers.

There are two situations for multi-fiber cables:

When dealing with cables containing multiple buffer tubes, each tube comprising 12 or fewer strands will be labeled or colored according to the same fiber color code. For instance, the 1st tube may be designated as blue, the 2nd as orange, and so on.
In the case of cables with more than 12 strands, the fiber optic cable color code repeats itself. To differentiate each group of 12 fibers, alternative identification methods are implemented. For example, in 24-strand groups, the fiber color code repeats with slight variations. The 1st group of 12 strands may have solid colors, while the 2nd group could have a solid color with a stripe or other distinguishing markings.

The color sequence for inner fibers is as follows:

Fiber Position Jacket Color Fiber Position Jacket Color
1 Blue 13 Blue with black tracer
2 Orange 14 Orange with balck tracer
3 Green 15 Green with black tracer
4 Brown 16 Brown with black tracer
5 Slate 17 Slate with black tracer
6 White 18 White with black tracer
7 Red 19 Red with black tracer
8 Black 20 Black with yellow tracer
9 Yellow 21 Yellow with black tracer
10 Violet 22 Violet with black tracer
11 Rose 23 Rose with black tracer
12 Aqua 24 Aqua with black tracer
Jacket color images are By User: Venge, CC BY-SA 3.0, https://commons.wikimedia.org/w/index.php?curid=64098042

Connector Color Code

Connectors are also a part of the fiber color code. Since there are different polish styles of fiber end-face, the connectors of fiber jumpers and the mating adapters are color coded for identification. However, the advent of metallic connectors like the FC and ST makes connector color coding difficult, so colored strain relief boots are also used. The boot color may vary among manufacturers.

Fiber Types Polish Style Connector Body Strain Relief/Mating Adapter
OM1 62.5/125 UPC Beige/Grey Beige/Grey
OM2 50/125 UPC Black Black
OM3/OM4 50/125 laser optimized UPC Aqua Aqua
Single Mode UPC Blue Blue
Single Mode APC Green Green

Conclusion

Fiber optic cable color code is a system that helps us distinguish fiber types visually from the colored fiber jacket, fiber connector, fiber boot, etc. The optical fiber color coding is also practical for fiber optic engineers during splicing, because the colorful fibers also help ensure the continuity of color codes throughout a cable run. Thus, fiber cable color coding is essential to fiber optic communications like the twisted pair color coding to copper wiring systems.

Related Article: Optimize Network Capacity with Ribbon Fiber Cable

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
382.9k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
366.2k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
332.5k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
418.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
291.9k