English

FS Releases 400G QSFP-DD DACs to Meet Tomorrow's Voracious Bandwidth Demands

Updated on Aug 4, 2020 by
2.6k

Jul. 12th, FS News - FS, a global networking solution provider for data centers, enterprises and Internet access networks, introduced the first batch of its 400G products, responsive to the soaring bandwidth demand and data center traffic. The products include QSFP-DD to QSFP-DD direct attach cables and QSFP-DD to 8x SFP-DD direct attach breakout cables.

QSFP-DD stands for Quad Small Form Factor Pluggable Double Density. As the name suggests, this form factor is similar to current QSFP, but with an additional row of contacts providing for an eight-lane electrical interface. Compared to traditional single or four-lane interface, the new design can increase the bandwidth, channel capacity and port density. Defined by the QSFP-DD MSA Group, this form factor addresses the need for high-density, high-speed networking solutions in a module host that’s backwards compatible with QSFP+, QSFP28 and QSFP56.

The first introduced FS 400G direct attach cables come with multiple choices in length and are compatible with Arista and generic devices, as shown in the table below. QSFP-DD to QSFP-DD direct attach cable, for example, can realize the straight connection between two pieces of 400G equipment. QSFP-DD to 8x SFP-DD direct attach breakout cable allows for 8x 50G breakout interconnection.

Form Factor Length Connector Price (US$) Brands Compatible

 

QSFP-DD to QSFP-DD

 

1m(3ft)

 

400G QSFP-DD to 400G QSFP-DD

 

165.00

Arista, Generic

 

2m(7ft)

210.00

3m(10ft)

304.00

 

QSFP-DD to 8x SFP-DD

 

1m(3ft)

 

400G QSFP-DD to 8x 50G SFP56

 

291.00

 

Arista, Generic

 

2m(7ft)

410.00

2.5m(8ft)

470.00


QSFP-DD, the latest advances in networking technology, is highly favored by the public. It is expected that QSFP-DD will become the de facto standard for 400G just as other QSFP form factors have done so at 40G and 100G, and is promising to lead the pack in 400G applications such as data center interconnects. Online ordering is now available, please contact through sales@fs.com.

About FS

FS has set the goal to provide high quality and cost-effective data centers, enterprise and Internet access networking solutions for global customers. Since then, the company has built up seven oversea branches and warehouses within the United States, Germany, United Kingdom, Australia, Singapore, and Russia. In the future, more branches and warehouses will be set up. This allows FS products to be exported to companies and individuals all around the world. More information is available at www.fs.com.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.4k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.7k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.7k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.9k