English

FS S5800-8TF12S Switch: Key Choice for Hyper-Converged Infrastructure Solution

Updated on May 10, 2018 by
5.2k

Hyper-converged infrastructure (HCI) is a rising star to herald an architectural revolution in data centers over past years. Hyper-convergence brings compute and storage together in one box with the built-in hypervisor, typically mated to a server platform to create an easy-to-use appliance. Hyper-converged appliance requires Ethernet switches with higher capabilities than unmanaged switches. FS S5800-8TF12S hyper-converged infrastructure switch is the key HCI solution that helps optimize costs and improve business efficiency. This post takes a look at why it makes sense to go hyper-converged infrastructure, what makes FS S5800-8TF12S switch the key choice for HCI solution and the most frequently asked questions when buying FS S5800-8TF12S switch.

S5800-8TF12S Hyperconverged Infrastructure Switch

Benefits of Hyper-Converged Infrastructure (HCI)

Hyper-converged infrastructure integrates compute and storage into a single server. This eliminates the bulk of legacy standalone hypervisors and storage complexity, while reducing power and space. As shown in the figure below, with non-converged architecture, physical servers operate a virtualization hypervisor that manages each of the virtual machines including the network switch and the Fibre Channel switch that were created on the server. By contrast, with converged architecture, the link between storage and physical server was built up via the converged network and storage switch. While in hyper-converged infrastructure, a storage controller runs as a service on every node in the cluster and merges the local storage within each server into a VSAN, thus creating a shared and distributed layer of storage.

traditional vs hyper-converged infrastructure

As there are no separate storage requirements to be provisioned in HCI, the deployment is simple and fast. Through the addition of more nodes, scaling becomes easy. Due to the all-in-one configuration, HCI solution allows you to build, scale and protect IT infrastructure more affordably and effectively than any other option available.

Why FS S5800-8TF12S Hyper-Converged Infrastructure Switch?

To cater for the unique demands for hyper-converged appliance, FS.com develops the S5800-8TF12S 10gb switch which is particularly aimed at solving the problems of access to the hyper-converged appliance of small and medium-sized business (SMB). With the abundant benefits below, it is a preferred key solution for the connectivity between hyper-converged appliance and the core switch.

Data Center Grade Hardware Design

FS S5800-8TF12S hyper-converged infrastructure switch provides high availability port with 8-port 1GbE RJ45 combo, 8-port 1GbE SFP combo and 12-port 10GbE uplink in a compact 1RU form factor. With the capability of static link aggregation and integrated high performance smart buffer memory, it is a cost-effective Ethernet access platform to hyper-converged appliance.

S5800-8TF12S switch

Reduced Power Consumption

With two redundant power supply units and four smart built-in cooling fans, FS S5800-8TF12S hyper-converged infrastructure switch provides necessary redundancy for the switching system, which ensures optimal and secure performance. The redundant power supplies can maximize the availability of the switching device. The heat sensors on the fan control PCBA (Printed Circuit Board Assembly) monitor and detect the ambient airs. It converts fans speeds accordingly to adapt to the different temperatures, thus reducing power consumption in proper operating temperatures.

Multiple Smart Management

Instead of being managed by Web interface, the FS S5800-8TF12S hyper-converged infrastructure switch supports multiple smart management with two RJ45 management and console ports. SNMP (Simple Network Management Protocol) is also supported by this switch. Thus when managing several switches in a network, it is possible to make the changes automatically to all switches. What about the common switches managed only by Web interface? It will be a nightmare when an SMB needs to configure multiple switches in the network, because there’s no way to script the push out of changes if not parse the web pages.

Traffic Visibility and Trouble-Shooting

In FS S5800-8TF12S HCI switch, the traffic classification is based on the combination of the MAC address, IPv4/IPv6 address, L2 protocol header, TCP/UDP, outgoing interface, and 802.1p field. The traffic shaping is based on interfaces and queues. Thus the traffic flow which are visible and can be monitored in real time. With the DSCP remarking, the video and voice traffic that is sensitive to network delays can be prioritized over other data traffic, so the smooth video streaming and reliable VoIP calls are ensured. Besides, the FS S5800-8TF12S switch comes with comprehensive functions that can help in trouble-shooting. Some basic functions include Ping, Traceroute, Link Layer Discovery Protocol (LLDP), Syslog, Trap, Online Diagnostics and Debug.

FAQs of FS S5800-8TF12S Hyper-Converged Infrastructure Switch

Does FS S5800-8TF12S Support MLAG or Stacking?

MLAG and stacking are two different concepts. MLAG is the ability of switches to appear as a single switch at layer 2, so that bundles of links in the form of LAGs can be diversely connected to each switch and appear as one. While in stacking, independent keep alive link between the switches. S5800-8TF12S is not stackable, but it supports MLAG. MLAG can achieve the effect of stacking, two devices can achieve cross device port aggregation. MLAG configuration is relatively simple, and it doesn’t need to reboot after the configuration is completed. More information about stackable switch, please kindly visit How to Stack FS 3800 Series Ethernet Switches.

How to Manage Multiple FS S5800-8TF12S Switches?

We are also asked if we have centralized management software to manage multiple switches. Actually we do not have the centralized management software. But the switch can be programmed through an open RPC API (Application Programming Interface) to achieve several switches are managed. The RPC API interface gives applications access to a variety of run-time services and control of multiple switches interactions at run time.

Summary

HCI offers tremendous integrated services including backup, data protection and highly redundant storage capacity which allow seamless management and expansion of various compute, storage and network. It’s apparent that the rapidly growing market for HCI have created the need for 10 Gigabit switch optimized for making these deployments both high performance and efficient. An 8-12 ports 10G SFP+ Ethernet switch is generally enough for hyper-converged appliance expansion, which is rational considering the expenditure for expansion as well. FS.com S5800-8TF12S hyper-converged infrastructure switch meets these needs, making it the perfect switch for HCI and the software-defined storage clusters for 10GbE connectivity.

You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k