English

FS Offers USB Gigabit Ethernet Adapter for High Performance Networking

Updated on Aug 4, 2020 by
2.4k

February 20th, Shenzhen, FS News—FS has introduced two types of USB Gigabit Ethernet network adapters, USB 3.0 and USB 3.1 type-C, which offer the ultimate solution for home and business users in need of high performance networking.

Gigabit Ethernet Network Adapter


USB to Gigabit Ethernet adapter provides users with a simple way to add Gigabit Ethernet-wire networking connectivity to Windows, MAC, Vista, Linux and other commonly used systems with USB ports, exploiting up to 5Gbps and even higher speed interface to deliver full Gigabit speed performance for home and business networking.

FS offers Gigabit Ethernet network adapters with USB 3.0 or USB 3.1 Type-C port. Both of them can extend network interface and add a wired network connection via corresponding USB port without replacing or adding a new networks card. FS always knows the need of customers. Compared with other vendors on the market, we have the most competitive price to help our customers optimize their network performance to the large extent.

Product Picture Product ID Highlights
USB 3.0 Gigabit Ethernet Network Adapter 65938

Gigabit Ethernet connectivity

USB to RJ45 port

Supports up to 5Gbps

Various systems compatibility

USB-C Gigabit Ethernet Network Adapter 65939

Gigabit Ethernet connectivity

USB-C to RJ-45 port

Supports up to 10Gbps

Windows/Vista//Linux/MAC compatibility

The Gigabit Ethernet network adapter allows you to connect seamlessly when the wireless connectivity is inconsistent or overextended. With the speed and reliability of Gigabit Ethernet, even the largest downloads can be possible without fear of interruption. Now both of the adapters are available in FS. Kindly contact us via sales@fs.com or visit www.fs.com for more information.

FS is a leading manufacturer and supplier of fiber optic subsystems, components and solutions. With last four years growing, we have built our strong and professional teams in optical communication product R&D, systematic solution and supply chain management. Nowadays, we are doing business with more and more worldwide well-known corporations like CloudFlare, EXFO, Apple, MRV, JDSU, ADTRAN, Avago, EMC, etc., who have put large volume of our products into production for their Data Center or Cloud Computing application and speak highly of our service and products. We will be working together with our customers, partners and co-workers to benefit them more and contribute more to the global popularity of optical communication.


You might be interested in

Knowledge
Knowledge
Knowledge
See profile for Sheldon.
Sheldon
Decoding OLT, ONU, ONT, and ODN in PON Network
Mar 14, 2023
386.3k
Knowledge
See profile for Irving.
Irving
What's the Difference? Hub vs Switch vs Router
Dec 17, 2021
367.6k
Knowledge
See profile for Sheldon.
Sheldon
What Is SFP Port of Gigabit Switch?
Jan 6, 2023
335.6k
Knowledge
See profile for Migelle.
Migelle
PoE vs PoE+ vs PoE++ Switch: How to Choose?
Mar 16, 2023
420.6k
Knowledge
Knowledge
Knowledge
Knowledge
See profile for Moris.
Moris
How Much Do You Know About Power Cord Types?
Sep 29, 2021
294.8k